BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog Test CAN BUS on BeagleBone
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 29 Sep 2019 11:59 AM Date Created
  • Views 10222 views
  • Likes 6 likes
  • Comments 6 comments
  • can_bus
  • bbb
  • BeagleBone
  • automotive
  • can
Related
Recommended

Test CAN BUS on BeagleBone

Jan Cumps
Jan Cumps
29 Sep 2019

I'm testing the CAN peripheral on a BeagleBone.

I'll be using my homemade generic CAN driver to implement the physical layer and Thomas Wedemeyer's BB specific instructions.

The other device on the CAN BUS, playing the communication partner role, is a Microchip CAN BUS Analyser.

 

image

Like most microcontrollers that have a CAN peripheral on board, the Sitara on the BeagleBone doesn't have a physical bus driver.

That's something that needs to be implemented separately.

The CAN driver breakout board I made for an e14 roadtest uses a TCAN332DTCAN332D driver IC.

The CAN Bus analyser from Microchip uses their own MCP2551MCP2551 (this family is used in several Arduino shields).

Check Thomas' blog to see how the driver connects to the BeagleBone.

 

Test the CAN Bus

 

Take care that everything is wired up before starting the exercise. The driver has to be connected to the BeagleBone and to a functional CAN bus.

If your device isn't connected to a bus, not a lot will happen physically.

My "functional CAN Bus" is a single Microchip CAN Bus analyser. But any physically correct circuit will work, as long as the voltage levels are compatible with the CAN driver you use.

On a BB Black or Green,  the controller side CAN Rx is on P9.24  and CAN Tx on P9.26.

 

Once everything is wired, there are 3 activities:

 

1. Set the BeagleBone pins to CAN function

There are several ways to do that permanently. Thomas' article is very good, check there.

For this exercise, I chose to assign them to CAN function temporary, with the config-pin utility.

 

sudo config-pin p9.24 can
sudo config-pin p9.26 can

 

2. Enable the Linux interface

CAN is implemented as a network in Linux. You use similar utilities as when defining a TCP/IP network.

 

sudo ip link set can1 up type can bitrate 125000
sudo ifconfig can1 up

 

Again, Thomas' instructions describe a way to do this permanently.

 

3. Send and Receive Data

The BeagleBone has Linux CAN utilities installed by default these days.

These can be used to try out the CAN network from the BB side. Both for sending and receiving traffic.

You'll need to have something on the bus to play the other role. In this case I used the Microchip analyser. An Arduino MKR with a MKR CAN shield and example sketches works equally well.

 

cansend can1 5A1#00.01.02.03.04
candump can1

 

 

image

 

The Logic and Physical Layer Signals

 

While doing this exercise, I captured some data on both sides of the BB driver.

The logic level has TX and RX signals separate. Both 3.3V logic signals. The physical layer is differential.

 

CAN data: logic layer - Tx and Rx lineCAN data: physical layer - differential CAN signal
imageimage

 

I probed the HI and LO with a differential probe.

image

 

Related blog
AVNET SmartEdge IIOT Gateway: Use the Isolated CAN
  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 7 years ago +4
    Thank you Jan Cumps , and apparently Thomas Wedemeyer! I was curious about CAN, so I read this item. But more important for me, I had not come across the config-pin command. I was recently trying to get…
  • clem57
    clem57 over 7 years ago

    Thanks Jan Cumps for the review of the CAN bus on Beagle Bone. I am wondering if you can explain the differential signals. In particular why they are use and where...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<