BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Play audio through HDMI on BeagleBone Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 108 subscribers
  • Views 2152 views
  • Users 0 members are here
  • audio
  • hdmi
  • debian;
  • BeagleBone Black
  • linux
Related

Play audio through HDMI on BeagleBone Black

e14 Contributor
e14 Contributor over 10 years ago

After work with a multitouch screen for the BeagleBone Black, now I just want to play audio/sounds through the HDMI connection as the multitouch screen has a speaker.

 

First of all, I just copied an audio sample, and try to reproduce it by 'vlc', but next message is shown:

    "Audio output failed. The audio device "default" could not be used. No such file or directory."

 

Then, I have installed next tools:

    'alsa-base', 'alsa-utils', 'alsa-tools', 'alsamixergui'

 

But, when I tried to launch 'alsamixergui', the next message is shown:

    "alsamixer: function snd_ctl_open failed for default: No such file or directory"

 

And at "/etc/modprobe.d/alsa-base.conf", the content is:

    # autoloader aliases

      install sound-slot-0 /sbin/modprobe snd-card-0

      install sound-slot-1 /sbin/modprobe snd-card-1

      install sound-slot-2 /sbin/modprobe snd-card-2

      install sound-slot-3 /sbin/modprobe snd-card-3

      install sound-slot-4 /sbin/modprobe snd-card-4

      install sound-slot-5 /sbin/modprobe snd-card-5

      install sound-slot-6 /sbin/modprobe snd-card-6

      install sound-slot-7 /sbin/modprobe snd-card-7

    # Cause optional modules to be loaded above generic modules

      install snd /sbin/modprobe --ignore-install snd && { /sbin/modprobe --quiet snd-ioctl32 ; /sbin/modprobe --quiet snd-seq ; : ; }

      install snd-rawmidi /sbin/modprobe --ignore-install snd-rawmidi && { /sbin/modprobe --quiet snd-seq-midi ; : ; }

      install snd-emu10k1 /sbin/modprobe --ignore-install snd-emu10k1 && { /sbin/modprobe --quiet snd-emu10k1-synth ; : ; }

    # Keep snd-pcsp from beeing loaded as first soundcard

      options snd-pcsp index=-2

    # Keep snd-usb-audio from beeing loaded as first soundcard

      options snd-usb-audio index=-2

    # Prevent abnormal drivers from grabbing index 0

      options bt87x index=-2

      options cx88_alsa index=-2

      options snd-atiixp-modem index=-2

      options snd-intel8x0m index=-2

      options snd-via82xx-modem index=-2

 

Moreover, I have try with next commands:

    'alsamixer -c 1 (2, 3... 7)'

Having next output:

    "invalid card index: 1"

 

Is there any way to reproduce any sound (*.midi, *.wav, *.mp3...) through hdmi easily?

 

______________ EDIT ______________

 

'lsmod':

    snd     56846   6   snd_soc_core, snd_timer, snd_pcm, snd_seq, snd_seq_device, snd_comp

 

'modinfo snd':

    filename:     /lib/modules/4.1.16-bone18/kernel/sound/core/snd.kp

    alias:           char-major-116-*

    license:       GPL

    description: Advanced Linux Sound Architecture driver for soundcards.

    author:        Jaroslav Kysela <perex@perex.cz>

    license:       GPL

    description: Jack detection support for ALSA

    author:        Mark Brown <broonie@opensource.wolfsonmicro.com>

    depends:     soundcore

    intree:          Y

    vermagic:     4.1.16-bone18 mod_unload modversions ARMv7 thumb2 p2v8

    parm:           slots:Module names assigned to the slots. (array of charp)

    parm:           major:Major # for sound driver. (int)

    parm:           cards_limit:Count of auto-loadable soundcards. (int)

 

______________ EDIT2 ______________

 

HDMI audio is in patch hell on mainline, if you want to use "4.1.x"

with hdmi audio you need to use the ti branch:

 

cd /opt/scripts/tools/

git pull

sudo ./update_kernel.sh --ti-channel --lts-4_1

 

Kernel is updated to TI's branch: "4.1.15-ti-r40".

 

Now, VLC player does not show any error message and plays the sound sample, but no sound is reproduced.

I have checked the basics, volume, mute option and similar. These are not the failures.

 

Which could the missing part for making the sound audible? Maybe codecs?

 

Testing the sound configuration, next instructions are launched:
ls /dev/snd
ls /proc/asound
cat /proc/asound/cards
cat /proc(asound/devices
aplay -l
cat /proc/asound/card0/pcm0p/sub0/hw_params
With output:
Black  card0  cards  devices  oss  pcm  seq  timers  version
0 [Black          ]: TI_BeagleBone_B - TI BeagleBone Black
                      TI BeagleBone Black
  2: [ 0]   : control
  3: [ 0- 0]: digital audio playback
  4: [ 0- 0]: digital audio capture
33:        : timer
**** List of PLAYBACK Hardware Devices ****
card 0: Black [TI BeagleBone Black], device 0: HDMI hdmi-hifi-0 []
  Subdevices: 0/1
  Subdevice #0: subdevice #0
access: MMAP_INTERLEAVED
format: S32_LE
subformat: STD
channels: 2
rate: 32000 (32000/1)
period_size: 1024
buffer_size: 16384
But there is no sound.

 

Any hint/tip?

Testing the sound configuration, next instructions are launched:
ls /dev/snd
ls /proc/asound
cat /proc/asound/cards
cat /proc(asound/devices
aplay -l
cat /proc/asound/card0/pcm0p/sub0/hw_params
With output:
Black  card0  cards  devices  oss  pcm  seq  timers  version
0 [Black          ]: TI_BeagleBone_B - TI BeagleBone Black
                      TI BeagleBone Black
  2: [ 0]   : control
  3: [ 0- 0]: digital audio playback
  4: [ 0- 0]: digital audio capture
33:        : timer
**** List of PLAYBACK Hardware Devices ****
card 0: Black [TI BeagleBone Black], device 0: HDMI hdmi-hifi-0 []
  Subdevices: 0/1
  Subdevice #0: subdevice #0
access: MMAP_INTERLEAVED
format: S32_LE
subformat: STD
channels: 2
rate: 32000 (32000/1)
period_size: 1024
buffer_size: 16384
But there is no sound.
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57 +1
    Multitouch screen should support audio. It has an internal speaker. But, meanwhile I test another options, I have launched the question to screen's manufacturer. Another test I have done is: - Current…
Parents
  • clem57
    clem57 over 10 years ago

    Did the touchscreen use the HDMI port? Does it support sound? Maybe a USB audio speaker could be used?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Multitouch screen should support audio. It has an internal speaker. But, meanwhile I test another options, I have launched the question to screen's manufacturer.

     

    Another test I have done is:

    - Current kernel: 4.1.18-ti-r56

     

    - aplay -L:

         null

              Discard all samples (playback) or generate zero samples (capture)

         default:CARD=Black

              TI BeagleBone Black,

              Default Audio Device

         sysdefault:CARD=Black

              TI BeagleBone Black,

              Default Audio Device

     

    - speaker-test -D CARD=Black -t song.wav -c 2 -s 1

         speaker-test1.0.25

     

         Playback device is CARD=Black

         Stream parameters are 48000Hz, S16_LE, 2 channels

         ALSA lib pcm.c:2217:(snd_pcm_open_noupdate) Unknown PCM CARD=Black

         Playback open error: -2,No such file or directory

     

    __________________ EDIT __________________

     

    Launching "alsaplayer", 'wav' and 'mp3' files can be played, but no sound is reproduced.

     

    It seems as the BeagleBone's drivers are not pointing to right audio interface.

    How can I checked if the SoC's audio codec and the HDMI's interface are configured and working fine?

     

    By the moment, I can't find a solution for the issue. I would be glad if someone could help me with it.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Multitouch screen should support audio. It has an internal speaker. But, meanwhile I test another options, I have launched the question to screen's manufacturer.

     

    Another test I have done is:

    - Current kernel: 4.1.18-ti-r56

     

    - aplay -L:

         null

              Discard all samples (playback) or generate zero samples (capture)

         default:CARD=Black

              TI BeagleBone Black,

              Default Audio Device

         sysdefault:CARD=Black

              TI BeagleBone Black,

              Default Audio Device

     

    - speaker-test -D CARD=Black -t song.wav -c 2 -s 1

         speaker-test1.0.25

     

         Playback device is CARD=Black

         Stream parameters are 48000Hz, S16_LE, 2 channels

         ALSA lib pcm.c:2217:(snd_pcm_open_noupdate) Unknown PCM CARD=Black

         Playback open error: -2,No such file or directory

     

    __________________ EDIT __________________

     

    Launching "alsaplayer", 'wav' and 'mp3' files can be played, but no sound is reproduced.

     

    It seems as the BeagleBone's drivers are not pointing to right audio interface.

    How can I checked if the SoC's audio codec and the HDMI's interface are configured and working fine?

     

    By the moment, I can't find a solution for the issue. I would be glad if someone could help me with it.