BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BeagleBone command works as root but not with sudo
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 107 subscribers
  • Views 2876 views
  • Users 0 members are here
  • beagle bone black
  • beagle_bone
  • sudo
  • linux
Related

BeagleBone command works as root but not with sudo

Jan Cumps
Jan Cumps over 10 years ago

I'm tryiong to set the direction of a pin to output by streaming to it's character device.

When logging in as the user 'debian' (the account that is creeted by default in the latest debian image for BBB),

and executing the command sudo echo out > /sys/class/gpio/gpio49/direction,

I get Permision denied.

 

When switching to Root, it works.

 

 

debian@beaglebone:~$ sudo echo out > /sys/class/gpio/gpio49/direction
-bash: /sys/class/gpio/gpio49/direction: Permission denied

debian@beaglebone:~$ su root
Password:
root@beaglebone:/home/debian# echo out > /sys/class/gpio/gpio49/direction

 

What am I doing wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 10 years ago in reply to Jan Cumps +2
    If my understanding is correct, the shell environment (sh) needed to be elevated so that the echo command is run within it, because otherwise the redirected output would go via the user (debian) shell…
  • bwelsby
    bwelsby over 10 years ago +1 verified
    Hi Jan, The problem is that even though you run echo with sudo the output is redirected by your command shell which hasn't got the privileges. one way around this would be : sudo sh -c "echo out > /sys…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to bwelsby +1
    or in my case, where I use bash? sudo /bin/bash -c "echo out > /sys/class/gpio/gpio49/direction"
  • bwelsby
    0 bwelsby over 10 years ago

    Hi Jan,

     

    The problem is that even though you run echo with sudo   the output is redirected by your command shell which hasn't got the privileges.

    one way around this would be :

     

    sudo sh -c "echo out > /sys/class/gpio/gpio49/direction"

    hope that makes sense.

    Brian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to bwelsby

    Yes!! that's it. So I was running the echo as root, but accessed the file as "myself", right?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to bwelsby

    or in my case, where I use bash?

     

    sudo /bin/bash -c "echo out > /sys/class/gpio/gpio49/direction"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 10 years ago in reply to Jan Cumps

    If my understanding is correct, the shell environment (sh) needed to be elevated so that the echo command is run within it, because otherwise the redirected output would go via the user (debian) shell which doesn't have privileges to access the destination location, because of how the shell environment works.

     

    So it's as though you needed to elevate the privileges of the standard input/output of the environment so it had permissions to be passed to the destination, because even though echo itself was elevated, the environment wasn't until sh was ran with sudo.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bwelsby
    0 bwelsby over 10 years ago in reply to cstanton

    Christopher Stanton wrote:

     

    If my understanding is correct, the shell environment (sh) needed to be elevated so that the echo command is run within it, because otherwise the redirected output would go via the user (debian) shell which doesn't have privileges to access the destination location, because of how the shell environment works.

     

    So it's as though you needed to elevate the privileges of the standard input/output of the environment so it had permissions to be passed to the destination, because even though echo itself was elevated, the environment wasn't until sh was ran with sudo.

    yes exactly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Jan Cumps

    Jan Cumps - bash or sh - it doesn't matter.  Any command is elevated to user id 0 with sudo.  The redirect has to be part of the command (hence, -c ".....") as opposed to being "owned" by sudo which was executed by an ordinary user.

     

    By the way, if you are going to execute several root commands, just do

     

         sudo -i

     

    once before all of the commands.  For example,

     

         sudo -i

         apt update > log

         apt dist-upgrade >> log

         apt autoclean >> log

     

    Added benefit: No worries about the redirection belonging to the root or the ordinary user who invoked sudo.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer