BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Black Rev C screens shuts off
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 111 subscribers
  • Views 1977 views
  • Users 0 members are here
  • rev c
  • beagle bone black
Related

Beaglebone Black Rev C screens shuts off

ruanknoetze
ruanknoetze over 9 years ago

I recently bought a new Beaglebone Black rev C and started playing around with it by using a standalone setup with HDMI, keyboard and mouse. After a few minutes the screens completely shuts off and does not want to start up again. I thought it might be a OS issue and re flashed my eMMC with an Angstom distribution. After start up it did the exact same thing. I even added code that disables the auto sleep mode of the screen but that does not work.

 

I know the BBB is getting input from my mouse and keyboard because one of the LEDs flashes when I type or click.

 

Has anyone ever experienced this and what can you recommend I do?

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago +2
    could it be a power issue? If the screen goes off when a usb hub, mouse and keyboard are plugged in its a possibility.
  • ruanknoetze
    ruanknoetze over 9 years ago +2 suggested
    Hi All I have flashed Debian 8.6 to another REVC and so far the screen has not turned off. I am also using a more stable power supply. So maybe it is a Angstom problem or a power supply problem. I will…
  • kleykenb
    kleykenb over 9 years ago +2
    Definately sounds like a power related issue. In my setup I've found that powering the BeagleBone via the microUSB port limits current to 500mA (which is the USB standard but not followed by everyone)…
Parents
  • kleykenb
    0 kleykenb over 9 years ago

    Definately sounds like a power related issue.

     

    In my setup I've found that powering the BeagleBone via the microUSB port limits current to 500mA (which is the USB standard but not followed by everyone).

    Using a short USB to microUSB cable might also help but with applications that include an external screen and peripherals the barrel connector is the best (possibly mandatory) way to go.

    So I assume you already use the barrel connector to power this? Might have an unstable power supply then.

    At one point I've replaced all my USB-microUSB cables with cables of type USB to 5.5mm x 2.1mm DC Barrel Jack (5V 2A) which greatly enhanced the kind of power sources I can use.

     

    regards,

    B

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kleykenb
    0 kleykenb over 9 years ago

    Definately sounds like a power related issue.

     

    In my setup I've found that powering the BeagleBone via the microUSB port limits current to 500mA (which is the USB standard but not followed by everyone).

    Using a short USB to microUSB cable might also help but with applications that include an external screen and peripherals the barrel connector is the best (possibly mandatory) way to go.

    So I assume you already use the barrel connector to power this? Might have an unstable power supply then.

    At one point I've replaced all my USB-microUSB cables with cables of type USB to 5.5mm x 2.1mm DC Barrel Jack (5V 2A) which greatly enhanced the kind of power sources I can use.

     

    regards,

    B