BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum how do you connect a TFT LCD (20 pins HDMI to 40 pins TTL)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 108 subscribers
  • Views 2330 views
  • Users 0 members are here
Related

how do you connect a TFT LCD (20 pins HDMI to 40 pins TTL)

digimbyte
digimbyte over 9 years ago

I've been around the tech community for a while, I've watched tutorials and enjoy the ben heck show and I have acquired several parts over the last few years, and I've decided to try and put them together.

 

I have;
BeagleBones Black

Thing-printer's Replicape Replicape rev B - Thing-Printer

ER-TFT050-3 5" display with driver board (RTD2660) http://www.buydisplay.com/default/5-inch-lcd-screen-tft-module-800x480-vga-video-av-driver-board

 

the replicape does consume almost all the pins from the BBB - but what I'm trying to do is connect the LCD IO pins to the TFT screen

the only problem is, the connectors for the driver board don't really encompass IO inputs. that being VGA and AV.

I was thinking I might possibly solder directly onto the RTD2660 or maybe I'm over complicating it.

I have a few other LCD screens procured from junk tablets, second-hand cam's etc if this display isn't ideal

 

 

things like this work fine if you buy kitbashing parts but this has me stumped as how to connect this TFT display with the touch screen to the BBB

  • Sign in to reply
  • Cancel
Parents
  • RParkerE
    0 RParkerE over 9 years ago

    It seems that you can extract a VGA signal from the LCD headers. Here is an article on how it may be done. This is not a direct fix, as it requires some hardware building, but I believe it will be a workaround.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • RParkerE
    0 RParkerE over 9 years ago

    It seems that you can extract a VGA signal from the LCD headers. Here is an article on how it may be done. This is not a direct fix, as it requires some hardware building, but I believe it will be a workaround.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer