BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum 10 projects in 10 days???
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 22 replies
  • Answers 8 answers
  • Subscribers 111 subscribers
  • Views 2998 views
  • Users 0 members are here
Related

10 projects in 10 days???

littleben1
littleben1 over 8 years ago

So my question is When are we going to get a 10 projects in 10 days feature for the Beaglebone series of boards?? Come on Element14, make this happen.

  • Sign in to reply
  • Cancel

Top Replies

  • afmishaq
    afmishaq over 8 years ago in reply to dkibbey +3
    Something using PocketBeagle will be interesting.
  • gsgill112
    gsgill112 over 8 years ago in reply to cstanton +3 suggested
    cstanton I was thinking Starting from Blinking LED Project and ending with LCD Interfacing Project with GUI Should cover the basics and also give ready made software templates for future projects . Regards…
  • afmishaq
    afmishaq over 8 years ago in reply to gsgill112 +3
    Gurinder, Yes, I have the PocketBeagle. I bought it a few months ago and got it going. But I did not get a chance to do much with it. I am tied up developing an undergrad course on Fluid Mechanics, which…
Parents
  • gsgill112
    0 gsgill112 over 8 years ago

    @littleben1 : How will be  we and some community members coming together and make this 10 Projects in 10 Days happen ?

     

    Regards,

    GS Gill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 8 years ago in reply to gsgill112

    gsgill112 Do you have some content to start blogging with?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 8 years ago in reply to cstanton

    cstanton I was thinking Starting from Blinking LED Project and ending with LCD Interfacing Project with GUI image

     

    Should cover the basics and also give ready made software templates for future projects .

     

    Regards,

    GS Gill

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • abrain
    0 abrain over 8 years ago in reply to gsgill112

    We probably need to work out which common capes and add ons we’re going to use or include too? I was lucky enough to get a wireless cape and my first BBB as part of a Sub-1 GHz Sensor to Cloud IoT Gateway - Review.

     

    A

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • afmishaq
    0 afmishaq over 8 years ago in reply to abrain

    That is a good idea.

     

    Here are my thoughts. The PocketBeagle is very easy to get started with and program. You really need no setup. Connect it to the usb port and it makes an ip network connection. Really seamless, I have tried it with both Windows and Linux.  You connect to the onboard webserver, and off you go. Plenty of ways to program. It has sufficient power to make a decent IoT device. The problem is that you cut the umbilical cord and it does not have much connectivity. So, my idea for the first project would be to build inexpensive wifi connectivity using ESP8266 or nRF2401 modules.

     

    Faiz Ishaq

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • abrain
    0 abrain over 8 years ago in reply to afmishaq

    One option could be to use a MikroElektronika clock board to add on the connectivity? They’re not that cheap, but are a simple way to add features, and there are many of them, so maybe it would be good to introduce one or more of the range, since the PocketBeagle can support two of them.

     

    i like the idea of something IoT like as a target to aim for, so we need to get agreed on some kind of progression from flashing a LED in hello world style to an IoT connected device, basically in 10 steps....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mp2100
    0 mp2100 over 8 years ago in reply to afmishaq

    I bought some adafruit micro usb connectors just to add connectivity to my pocket beagle.

    https://www.adafruit.com/product/1833

     

    It solders directly into the pins on the PB, so I’d add Ethernet or a wifi dongle there. (Still working through the correct combination of debian and wpasupplicant.conf to get it working consistently)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mp2100
    0 mp2100 over 8 years ago in reply to afmishaq

    I bought some adafruit micro usb connectors just to add connectivity to my pocket beagle.

    https://www.adafruit.com/product/1833

     

    It solders directly into the pins on the PB, so I’d add Ethernet or a wifi dongle there. (Still working through the correct combination of debian and wpasupplicant.conf to get it working consistently)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • afmishaq
    0 afmishaq over 8 years ago in reply to mp2100

    This looks good. May require an OTG cable to connect a USB WiFi dongle. Should work.