BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum New Python project using a BeagleBone Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 5 answers
  • Subscribers 108 subscribers
  • Views 2666 views
  • Users 0 members are here
  • pi-visa
  • python
  • beaglebone_black
  • test instrumentation
  • BeagleBone
  • vna
  • bb_black
  • instrument
Related

New Python project using a BeagleBone Black

angellxp
angellxp over 7 years ago

I'm looking for directions/guidance for the best direction to take with this new project.

 

I have a VNA that is controllable via Python/Pi-Visa and a network cable.  I also constructed a custom relay switching board so that I can test up to 32 connection points(using 16 relays) without reconnecting my VNA. The attached image is the 8Ch version I made.

My question is if anyone has had experience with instrument control via Python and/or the BB Black, what direction should I take?

 

Thanks

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • jomoenginer
    jomoenginer over 7 years ago in reply to angellxp +3 suggested
    Derek Molloy has some good examples of how to interface the GPIOs of the BB Black. Some of the example may be dated but they should still point you in the right direction. His source code that can be downloaded…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz +1 suggested
    My code i not hard to adapt to another relay board - even your home-grown - or a BBB. There's a limited piece of code that talks to the hardware. Where-ever you see a SPI call, replace it by the code to…
  • shabaz
    shabaz over 7 years ago in reply to angellxp +1 suggested
    Hi Jon, I think all of this can be achieved easily. First step would be to wire up the relay board to the BBB (using the GPIO API link earlier to see which pins are allowed - not all GPIO pins on the BBB…
Parents
  • jomoenginer
    0 jomoenginer over 7 years ago

    Some instruments also have a serial interface and even a RESTful interface (although this does require a network connection) all of which can be controlled from Python. Some of new devices from Keysight require a Windows COM object to remotely control the instrument making it a bit interesting to using a non Windows system for connection.

     

    What interface does your Relay board use?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jomoenginer
    0 jomoenginer over 7 years ago

    Some instruments also have a serial interface and even a RESTful interface (although this does require a network connection) all of which can be controlled from Python. Some of new devices from Keysight require a Windows COM object to remotely control the instrument making it a bit interesting to using a non Windows system for connection.

     

    What interface does your Relay board use?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • angellxp
    0 angellxp over 7 years ago in reply to jomoenginer

    My Relay board has an on board relay driver per relay so all I need is logic H/L from the BB.  That part is easy enough.  Im just trying to figure out the Python side of things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 7 years ago in reply to angellxp

    Derek Molloy has some good examples of how to interface the GPIOs of the BB Black.  Some of the example may be dated but they should still point you in the right direction.  His source code that can be downloaded has some Python examples that might be of interest to you.

    http://exploringbeaglebone.com/chapter8/

     

    The Adafruit examples that were referenced previously are another good source of examples.

     

    What relay driver does the board use?  It is possible that you may find examples already created for the driver it uses.

     

    For a Python GUI, you could use wxPython or tkinter which would run directly on the BBB.  Or you could use something like Flask and Javascript and Python to publish a browser based application for remote control of the Relay board.  Then there is the whole NodeRed thing. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to jomoenginer

    jomoenginer  wrote:

     

    Derek Molloy has some good examples of how to interface the GPIOs of the BB Black.  Some of the example may be dated but they should still point you in the right direction. ...

    His newly released Second Edition of the BB book should be up to date ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mp2100
    0 mp2100 over 7 years ago in reply to angellxp

    I just installed the adafruit_BBIO on a beaglebone black, the debian instructions work well.  The examples in that tutorial are very useful to get the python working.

     

    I'm also using raspberry pi examples, those are much easier to find, --> substituting BBB pin names of course (eg "P9_39").  It's working quite well.