BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Changing Static Ip adderess.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 4 answers
  • Subscribers 108 subscribers
  • Views 4435 views
  • Users 0 members are here
Related

Changing Static Ip adderess.

daniel689
daniel689 over 7 years ago

I am trying to change the IP address of my Beagle.   My google attemps have lead me to modifying the interfaces file using a nano editor.   

 

 

 

I have edited the file to

 

# The primary network interface

auto eth0

iface eth0 inet static

address 192.168.1.80

netmask 255.255.255.0

gateway 192.168.1.1

…

# Ethernet/RNDIS gadget (g_ether)

iface usb0 inet static

address 192.168.7.4

netmask 255.255.255.0

network 192.168.7.0

gateway 192.168.7.1

 

 

I was expecting it to change when saved but it is clearly not.   It still says 192.168.7.2.

 

 

 

I was ex

  • Sign in to reply
  • Cancel

Top Replies

  • mp2100
    mp2100 over 7 years ago +1 suggested
    Daniel, do you want to change both the USB address and the Ethernet address? Normally I leave the USB at the default (192.168.7.2). For the Ethernet (your example is 192.168.1.80) you can try a reboot…
  • shabaz
    shabaz over 7 years ago +1 suggested
    Hi Daniel, I don't know the answer, but I'm guessing it is because that's a special interface, it may restrict itself to only certain addresses (despite being configured as a /24 network in the file you…
  • shabaz
    shabaz over 7 years ago in reply to clem57 +1 suggested
    Hi Clem, I'm not sure this will work. There's an earlier link pasted above, that suggest connman is not used for USB network configuration. Text from there: OK, figured it out. The usb0 interface is not…
Parents
  • mp2100
    0 mp2100 over 7 years ago

    Daniel, do you want to change both the USB address and the Ethernet address?  Normally I leave the USB at the default (192.168.7.2).  For the Ethernet (your example is 192.168.1.80) you can try a reboot to get the beaglebone to read the interfaces file.  Or, I forget exact syntax, but you can do  $ sudo ifdown and  $ sudo ifup commands  (the command stands for "interface up")

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mp2100
    0 mp2100 over 7 years ago

    Daniel, do you want to change both the USB address and the Ethernet address?  Normally I leave the USB at the default (192.168.7.2).  For the Ethernet (your example is 192.168.1.80) you can try a reboot to get the beaglebone to read the interfaces file.  Or, I forget exact syntax, but you can do  $ sudo ifdown and  $ sudo ifup commands  (the command stands for "interface up")

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer