BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum No expected output in console window with printk
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 107 subscribers
  • Views 1932 views
  • Users 0 members are here
Related

No expected output in console window with printk

elem2018
elem2018 over 6 years ago

Hello,

 

SDK: ti-processor-sdk-linux-am335x-evm-05.03.00.07.

I want to have more debug ouputs in the console window during the Linux kernel booting so that I can trace for example MMC driver loading process.

Added some printk() into the kernel, for example printk("this function is called \n"). After successful compiling and loading the kernel unfortunately I can't see the

exptected output message "this function is called" in the console window.

I also tried

     echo 8 > /proc/sys/kernel/printk

     dmesg

after login but the same results.

Is there any configuration missing in .config file?

I also see brcmf_dbg() in kernel files, how can I activate it?

Thanks

 

Xi

  • Sign in to reply
  • Cancel
  • marisol
    0 marisol over 6 years ago

    Hi Xi Fan,

     

    Please see my answers in bold image Hope that helps!

     

    I want to have more debug ouputs in the console window during the Linux kernel booting so that I can trace for example MMC driver loading process.

    Added some printk() into the kernel, for example printk("this function is called \n"). After successful compiling and loading the kernel unfortunately I can't see the exptected output message "this function is called" in the console window.

     

    It is generally easier to use the "pr_" helper functions:

    https://elinux.org/Debugging_by_printing

     

    pr_err() uses KERN_ERR level should always print regardless of the

    printk log level.  KERN_ERR is not a good practice for debug output,

    but it does eliminate the chance that the log level is filtering out

    your print statements.

     

    Try adding this:

    pr_err("DEBUG: start name_of_function()");

     

    If you don't see that in dmesg, then it is likely that the function

    you put that in is never actually called.

     

    I also tried

         echo 8 > /proc/sys/kernel/printk

         dmesg

    after login but the same results.

    Is there any configuration missing in .config file?

     

    level 8 should be sufficient but it is easier if you just set the

    level in the .config before you compile your kernel.

     

    CONFIG_PRINTK_TIME=y

    CONFIG_CONSOLE_LOGLEVEL_DEFAULT=7

    CONFIG_CONSOLE_LOGLEVEL_QUIET=7

    CONFIG_MESSAGE_LOGLEVEL_DEFAULT=7

     

    You probably also want to make sure dynamic debugging is enabled:

    CONFIG_DYNAMIC_DEBUG=y

     

    Dynamic debugging is a neat feature where you can chose to see more

    debug information for a particular source code file:

    https://linux-kernel-labs.github.io/refs/heads/master/labs/kernel_modules.html?highlight=config_dynamic_debug#dynamic-debugging

     

    Sometimes you don't even need to add in your own debug print

    statements, you just need to enable the dynamic debug output that is

    already built-in to a driver or subsystem.

     

    I also see brcmf_dbg() in kernel files, how can I activate it?

     

    Are you trying to debug a Broadcom wifi driver?

     

    Taking a look at Elixir to search the kernel code:

    https://elixir.bootlin.com/linux/latest/ident/brcmf_dbg

     

    It looks like CONFIG_BRCM_TRACING will enable debug output:

    https://elixir.bootlin.com/linux/latest/source/drivers/net/wireless/broadcom/brcm80211/brcmfmac/debug.h#L63

     

    Try setting that in your .config:

    https://cateee.net/lkddb/web-lkddb/BRCM_TRACING.html

     

    While it is technically to enable function tracing for the driver, it

    looks like it will cause brcmf_dbg() to be defined.

     

    Now the individual invocations of brcmf_dbg() will have a log level

    associated with them.  It appears that level can be set as kernel

    module parameter:

    https://elixir.bootlin.com/linux/latest/source/drivers/net/wireless/broadcom/brcm80211/brcmfmac/common.c#L42

     

    This forum post has more information:

    https://forum.openwrt.org/t/getting-output-of-brcmf-dbg/31094/4

     

    It indicates this can be set while the module is loaded via:

    echo 6 > /sys/module/brcmfmac/parameters/debug

     

    Best Regards,

    Marisol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer