BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BBB can not access Internet via USB to Win-10
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 108 subscribers
  • Views 4081 views
  • Users 0 members are here
Related

BBB can not access Internet via USB to Win-10

kenunix
kenunix over 6 years ago

I can SSH to 192.168.7.2 OK.

I can connect to virtual USB COM port OK.

I can connect to virtual serial COM port to JTAG OK.

Above using putty

 

I can Firefox to 192.168.7.2 OK

 

I can not ping off the BBB to an external address. I.E.  ping 23.194.117.73 ping to 192.168.7.1 OK.

 

Destination Gateway     Genmask     Flags Metric RefUse Iface
default     192.168.7.1 0.0.0.0     UG0  0    0 usb0
192.168.6.0 0.0.0.0     255.255.255.252 U 0  0    0 usb1
192.168.7.0 0.0.0.0     255.255.255.252 U 0  0    0 usb0

 

 

Is the Win-10 set up to forward packets? I need some help here. Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • kenunix
    kenunix over 6 years ago +1 verified
    Actually what I had to do follows for Internet access. Took some trial and error. Out of the box the IP addresses 192.168.7.x are only good between two devices. Example a Laptop and the BBB. If you want…
Parents
  • kenunix
    0 kenunix over 6 years ago

    Actually what I had to do follows for Internet access. Took some trial and error.

     

    Out of the box the IP addresses 192.168.7.x are only good between two devices.

    Example a Laptop and the BBB.

     

    If you want Internet access to do updates or whatever do the following

     

    In /etc/network/interfaces make the following changes

     

    iface usb0 inet static

        address 192.168.137.2    <=== 137 was used because Windows insisted on it to do WiFi sharing 7 no go

        netmask 255.255.0.0

        network 192.168.137.0    <=== 137 was 7 originally

        gateway 192.168.137.1    <=== What Windows assigned to the adapter in Windows-10 19.09 64-bit home

        dns-nameservers 8.8.8.8  <=== Point to nameserver

        post-up route add default gw 192.168.137.1  <== Add default gateway. Auto up.

     

    debian@beaglebone:~$ route

    Kernel IP routing table

    Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

    default         192.168.137.1   0.0.0.0         UG    0      0        0 usb0  <== Updated automatic entry

    192.168.0.0     0.0.0.0         255.255.0.0     U     0      0        0 usb0

    192.168.6.0     0.0.0.0         255.255.255.252 U     0      0        0 usb1

    debian@beaglebone:~$

     

    On the Windows side make sure the Network connection for the BBB or Ethernet 2

    that the TCP/IP V4 setting is set to the 137 address from above. Save it then bring

    up the WiFi  settings / Properties / Sharing and allow sharing and choose either BBB

    or Ethernet 2. Whichever is the new one added. Save it and exit.

     

    Do a clean startup of the P.C. and the BBB.

     

    It should work fine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kenunix
    0 kenunix over 6 years ago

    Actually what I had to do follows for Internet access. Took some trial and error.

     

    Out of the box the IP addresses 192.168.7.x are only good between two devices.

    Example a Laptop and the BBB.

     

    If you want Internet access to do updates or whatever do the following

     

    In /etc/network/interfaces make the following changes

     

    iface usb0 inet static

        address 192.168.137.2    <=== 137 was used because Windows insisted on it to do WiFi sharing 7 no go

        netmask 255.255.0.0

        network 192.168.137.0    <=== 137 was 7 originally

        gateway 192.168.137.1    <=== What Windows assigned to the adapter in Windows-10 19.09 64-bit home

        dns-nameservers 8.8.8.8  <=== Point to nameserver

        post-up route add default gw 192.168.137.1  <== Add default gateway. Auto up.

     

    debian@beaglebone:~$ route

    Kernel IP routing table

    Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

    default         192.168.137.1   0.0.0.0         UG    0      0        0 usb0  <== Updated automatic entry

    192.168.0.0     0.0.0.0         255.255.0.0     U     0      0        0 usb0

    192.168.6.0     0.0.0.0         255.255.255.252 U     0      0        0 usb1

    debian@beaglebone:~$

     

    On the Windows side make sure the Network connection for the BBB or Ethernet 2

    that the TCP/IP V4 setting is set to the 137 address from above. Save it then bring

    up the WiFi  settings / Properties / Sharing and allow sharing and choose either BBB

    or Ethernet 2. Whichever is the new one added. Save it and exit.

     

    Do a clean startup of the P.C. and the BBB.

     

    It should work fine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer