BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum USB 3.0 support for beagle bone AI.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 27 replies
  • Answers 11 answers
  • Subscribers 104 subscribers
  • Views 4724 views
  • Users 0 members are here
  • beagleboard_ai
Related

USB 3.0 support for beagle bone AI.

prathamesh12
prathamesh12 over 5 years ago

I want to use basler ace camera (acA1300-200um) with beagle bone AI board. It requires usb 3.0 host controller. As BB AI board provides only usb 2.0 , camera isn't working. Is there any way we can add usb 3.0 support to board? Like an external module with 3.0 support which can be further connected to AI board via UART....

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 5 years ago in reply to prathamesh12 +3 verified
    The answer is simply hidden. sudo /opt/scripts/boot/bbai_usb_host.sh This executes: echo "host" > /sys/kernel/debug/48890000.usb/mode Which puts the USB-C 3.0 hub on the BeagleBone AI into 'USB Host Mode…
  • gdstew
    gdstew over 5 years ago +2 suggested
    The USB C connector used to power the AI is also connected to a USB 3 data interface on the SoC. The problem I've seen is that none of the power supplies for the AI make these signals available to use…
  • cstanton
    cstanton over 5 years ago in reply to gdstew +2 suggested
    Maybe a USB-C USB hub would work? If it allows backpowering. I may be able to test this.
Parents
  • clem57
    0 clem57 over 5 years ago

    Hah! You need to supply higher current for the camera... The data can be USB 2.0 at a slower frame rate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 5 years ago

    Hah! You need to supply higher current for the camera... The data can be USB 2.0 at a slower frame rate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • prathamesh12
    0 prathamesh12 over 5 years ago in reply to clem57

    That would have been an option. But the camera which I am using (basler acA1300-200um) will be detected but can't be used on any other interface than USB 3 according to the manufacturers. It's an industrial grade camera which requires high frame rate.