BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum USB 3.0 support for beagle bone AI.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 27 replies
  • Answers 11 answers
  • Subscribers 104 subscribers
  • Views 4735 views
  • Users 0 members are here
  • beagleboard_ai
Related

USB 3.0 support for beagle bone AI.

prathamesh12
prathamesh12 over 5 years ago

I want to use basler ace camera (acA1300-200um) with beagle bone AI board. It requires usb 3.0 host controller. As BB AI board provides only usb 2.0 , camera isn't working. Is there any way we can add usb 3.0 support to board? Like an external module with 3.0 support which can be further connected to AI board via UART....

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 5 years ago in reply to prathamesh12 +3 verified
    The answer is simply hidden. sudo /opt/scripts/boot/bbai_usb_host.sh This executes: echo "host" > /sys/kernel/debug/48890000.usb/mode Which puts the USB-C 3.0 hub on the BeagleBone AI into 'USB Host Mode…
  • gdstew
    gdstew over 5 years ago +2 suggested
    The USB C connector used to power the AI is also connected to a USB 3 data interface on the SoC. The problem I've seen is that none of the power supplies for the AI make these signals available to use…
  • cstanton
    cstanton over 5 years ago in reply to gdstew +2 suggested
    Maybe a USB-C USB hub would work? If it allows backpowering. I may be able to test this.
Parents
  • prathamesh12
    0 prathamesh12 over 5 years ago

    Hello,

    I have tried with a powered usb 3.0 hub (link). But Beagle-Bone can't detect it. Hub is working fine. I have checked it on my PC with c type connector.

    Now there may be this issue. As gdstew said back-powering is not possible. Kernel suspends usb if there is no enough power supply from host. This autosuspend functionality is default enabled on Debian image provided for BB-AI. It can be disabled but I could only find it out using Grub, which is not available for the kernel I m using.So any other way this can be disabled? Any other issue you guys can think of, other than this??

     

    --Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cstanton
    0 cstanton over 5 years ago in reply to prathamesh12

    Disabling auto suspend should be possible. The kernels are available online.

    I still need to find my beaglebone AI, it's in a box...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • cstanton
    0 cstanton over 5 years ago in reply to prathamesh12

    Disabling auto suspend should be possible. The kernels are available online.

    I still need to find my beaglebone AI, it's in a box...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer