BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BBONE-BLACK-WIRELESS and BB-CAPE-DISP-CT43
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 107 subscribers
  • Views 1273 views
  • Users 0 members are here
Related

BBONE-BLACK-WIRELESS and BB-CAPE-DISP-CT43

teddytronix
teddytronix over 6 years ago

Hello,

I am trying to figure out if the two products in the subject line are compatible without having to jump through those proverbial hoops: the element14 BeagleBone Black Wireless with WiFi & Bluetooth, and the Beaglebone Black Touchscreen Display.

 

Both are currently available at CPC under order codes, respectively, SC14310 and SC14039.

 

I have been reading through a variety of documents, but I am still struggling to come up with a definitive answer. On the CPC site it says, for the touch screen, "connects directly to your BeagleBone" and "plug-and-play functionality with the default Debian operating system". On element14 it states "*PLEASE read the folowing notice regarding product compatibility with BeagleBone Black." which then reveals that firmware updates are required as the element14 B'Bone is different to a standard one. There is then a comment stating that after the firmware upgrade the wireless and bluetooth will not work any longer. Confusing :-)

 

Some documents appear several years old, but I cannot find any notice if they have been superseeded. Or, indeed, found any more recent versions.

 

So, can I just connect SC14310 and SC14039, i.e. element14 BeagleBone Black Wireless with WiFi & Bluetooth and Beaglebone Black Touchscreen Display, to work out-of-the-box(es), or are mods like firmware updates required?

 

After any updates, will all subsystems be functional?

 

Many thanks, for your time,

Teddy

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 6 years ago +3 suggested
    The 'problem' is that you'll have to set this up manually for it to work, basically you need the code / device tree overlay from the image available at 4.3 LCD Display Cape for Beaglebone Board (White…
  • teddytronix
    teddytronix over 6 years ago in reply to cstanton +2 suggested
    Hi Christopher, thanks for the pointers and especially the link to the overlay. Good to see that there is lots of info, too. I have just bought both after realising that they are on very special offer…
  • shabaz
    shabaz over 6 years ago +1 suggested
    Hi Teddy, I don't have these so I'm slightly speculating (and hopefully anyone who owns these and with better information can step in), but I think it's best to assume that it will not be plug-and-play…
Parents
  • cstanton
    0 cstanton over 6 years ago

    The 'problem' is that you'll have to set this up manually for it to work, basically you need the code / device tree overlay from the image available at 4.3 LCD Display Cape for Beaglebone Board (White, Black, or Wireless) to then apply it to the latest Debian image to run on the BeagleBone Wireless. The 'image' or 'OS Image' that was produced and available to download on the link here is assuming you only have the BeagleBone Black, so it won't contain the firmware, device tree, or drivers for the WiFi and Bluetooth.

     

    The overlay for this board is available https://github.com/beagleboard/bb.org-overlays/blob/master/src/arm/BB-CAPE-DISP-CT4-00A0.dts  which should help show what pins, etc are needed.

     

    Hopefully rramesh1992 can step in and provide further guidance or files for supporting the display cape.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • teddytronix
    0 teddytronix over 6 years ago in reply to cstanton

    Hi Christopher,

     

    thanks for the pointers and especially the link to the overlay. Good to see that there is lots of info, too.

     

    I have just bought both after realising that they are on very special offer at cpc.co.uk and

     

    ** cost less than GBP20 for both **

     

    ... less than six for the beagle, hard to beat that price I would imagine. Should anyone be interested: SC1431069 and SC1403969 (as above but with 69's added ... important as that is the offer code). Both are in a quickly changing section of the site so prices won't last for long.

     

    Any other pointers, info, comments very welcome,

     

    many thanks,

    Teddy

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • teddytronix
    0 teddytronix over 6 years ago in reply to cstanton

    Hi Christopher,

     

    thanks for the pointers and especially the link to the overlay. Good to see that there is lots of info, too.

     

    I have just bought both after realising that they are on very special offer at cpc.co.uk and

     

    ** cost less than GBP20 for both **

     

    ... less than six for the beagle, hard to beat that price I would imagine. Should anyone be interested: SC1431069 and SC1403969 (as above but with 69's added ... important as that is the offer code). Both are in a quickly changing section of the site so prices won't last for long.

     

    Any other pointers, info, comments very welcome,

     

    many thanks,

    Teddy

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer