BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Odd PRU interrupt behavior
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 107 subscribers
  • Views 1147 views
  • Users 0 members are here
Related

Odd PRU interrupt behavior

ivangalysh
ivangalysh over 6 years ago

I want to determine if I can use the PRUs to interact with an instrument for a satellite payload. I am able to get rpmsg-proc working and can move blocks of data quickly enough. I added the IEP timer and want to set it up to generate a 1 second interrupt so I can set a flag in the data indicating end of 1 second integration. My test code is supposed to send a message once a second triggered by the timer. Instead I am getting two messages every two seconds. I modified resource_table1.h to map event 7, IEP compare event, to host 1 which is R31 bit 31. I am using PRU1. Attached is the code. Any help would be appreciated.

 

I'm hoping to use the BBB industrial version in two space missions.

 

Ivan

Attachments:
main.c.zip
resource_table_1.h.zip
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +1 suggested
    Hi Ivan, I didn't check all the code, but at first glance this looks incorrect: CT_IEP.TMR_CMP0 = 0x20000000; // set compare to 1 second at 200 MHz At 200 MHz clocking, this would be a delay of just over…
  • ivangalysh
    ivangalysh over 6 years ago +1 verified
    I finally figured it out. I needed to set CT_INTC.SICR = 7 to clear out the event. After line 117, CT_INTC.SECR0 = 0x80; I added CT_INTC.SICR_bit.STS_CLR_IDX = 7; This took care of it. I have my code working…
  • ivangalysh
    ivangalysh over 6 years ago in reply to shabaz +1 suggested
    I caught that too. It's the interrupt process that was not well described anywhere. I finally muddled through it.
  • shabaz
    0 shabaz over 6 years ago

    Hi Ivan,

     

    I didn't check all the code, but at first glance this looks incorrect:

    CT_IEP.TMR_CMP0 = 0x20000000; // set compare to 1 second at 200 MHz

     

    At 200 MHz clocking, this would be a delay of just over 2 seconds (2.68 seconds). If you wish it to be 1 second then this is not the right value.

    It should be 200000000 (or just type (int)2E8 it is easier to follow or (int)200E6), not 0x20000000

    Also, for space stuff (or any coding), these constants should be defined elsewhere, not in the function, and someone can then check each one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ivangalysh
    0 ivangalysh over 6 years ago

    I finally figured it out. I needed to set CT_INTC.SICR = 7 to clear out the event.

    After line 117,

    CT_INTC.SECR0 = 0x80; I added

    CT_INTC.SICR_bit.STS_CLR_IDX = 7;

     

    This took care of it.

     

    I have my code working. Now to work on the physical interface.


    Ivan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ivangalysh
    0 ivangalysh over 6 years ago in reply to shabaz

    I caught that too.

     

    It's the interrupt process that was not well described anywhere. I finally muddled through it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer