BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BB-VIEW 7" touchscreen display blank
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 108 subscribers
  • Views 1658 views
  • Users 0 members are here
Related

BB-VIEW 7" touchscreen display blank

e14 Contributor
e14 Contributor over 12 years ago

I seem to be having difficulty getting a just purchased BeagleBone Black and BB 7" Touchscreen display to work. I wonder if someone could give some help.

 

Followed the hardware installation instructions in the manual, which are easy enough. After fiddling around with Debian, in which I could get HDMI OK and all else seemed to work fine, Went looking for the TI Angstrom demo. After working through the Element14 links I dug BBB-eMMC-flasher-2013.09.04.img out from BeagleBoard.org - latest-images. I am still presented with a blank screen.  Is this the correct image?

 

It shows the cape not being recognised.

# more /sys/devices/bone_capemgr.*/slots

0: 54:PF---

1: 55:PF---

2: 56:PF---

3: 57:PF---

4: ff:P-O-L Bone-LT-eMMC-2G,00A0,Texas Instrument,BB-BONE-EMMC-2G

5: ff:P-O-L Bone-Black-HDMI,00A0,Texas Instrument,BB-BONELT-HDMI

 

Followed instructions in the BB-View Cape user manual with  no effect (the images suggested are actually a later date than the latest images from beagleboard.org, but cannot find them on Element14's site).

 

Back to Debian. After updating the kernel as suggested in the Debian Howto, and setting in uEnv.txt:

optargs=capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN capemgr.enable_partno=BB-VIEW-LCD7-01

 

got the same result - cape not recognised, similar to here BB View + BeagleBone Board.

 

That seems to be the end of my competence. Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to timcnc +1 suggested
    That's more or less what I was seeing a few times except that there was some text on the LCD screen, but if you haven't changes uEnv.txt then it will probably not use the LCD (though it should have used…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, excellent instructions and I appreciate it very much. I do have a question though. My BB works well with the Ti SDK image so I know the hardware works. My confusion, and before I try it, is the SCP part of the process you describe. Where do you SCP to? Would it be possible to provide a sample of the command? I presume you are SCPing to the root in the BB but I want to be sure.

     

    thanks in advance

     

    jim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, excellent instructions and I appreciate it very much. I do have a question though. My BB works well with the Ti SDK image so I know the hardware works. My confusion, and before I try it, is the SCP part of the process you describe. Where do you SCP to? Would it be possible to provide a sample of the command? I presume you are SCPing to the root in the BB but I want to be sure.

     

    thanks in advance

     

    jim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    No worries, I just moved them there and then followed your instructions. image duh!

    My BB works very well with the screen now.

    Thank you very much for the instructions.