BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BB VIEW_43 Hardware Question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 108 subscribers
  • Views 566 views
  • Users 0 members are here
  • lcd
  • bb
  • beaglebone-black
  • view
Related

BB VIEW_43 Hardware Question

e14 Contributor
e14 Contributor over 12 years ago

I am looking at the BB View as a possible LCD for my project.  My project uses 3 GPIOs for its custom functions on an existing cape that I will need to be plugged into J1 and J2 of the BB View.  They are P9 pins 23, 27 and 42.   In the BB View manual it says J2 (I assume this corresponds to P9 on the BBB)   pins 27 and 42 are NC (No Connect). 

 

Does this mean I need to chose another IO and that those IO are not available at all on J2?  

 

Is pin 23 on J2 the same as Pin 23 on J9 of the BBB or GPIO1_17?

 

Are the no connects just not connected to J1 & J2 and so those IOs are lost and can't be used? 

 

If they are lost I can use other IOs but I really need to know if those other IOs correspond to the same pins on the BBB. 

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 verified
    I figured it out by reading the manual a little closer. All the No Connect pins are available for use in my design, the pins with functions on them are used by BB-VIEW for the LCD and the USER buttons…
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I figured it out by reading the manual a little closer.  All the No Connect pins are available for use in my design,  the pins with functions on them are used by BB-VIEW for the LCD and the USER buttons. 

     

    Sorry for the wasted post.    

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • markvenn
    0 markvenn over 11 years ago in reply to e14 Contributor

    Not sure it is a wasted post, I am looking at the possibility of using a view_43 in one of my projects! image