BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BeagleBone boards discussion
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 105 subscribers
  • Views 3354 views
  • Users 0 members are here
  • BeagleBone
Related

BeagleBone boards discussion

koudelad
koudelad over 2 years ago

Hello,

do you use BeagleBone boards personally or professionally?

I have a few boards in my electronics box, but haven't used them for a few years (or ever).

Looking at the beagleboard.org website, it somehow got more confusing than it used to be. It is hard to find software images and later I realized why - the OS is not compatible with all boards they way Raspberry Pi OS is.

BeagleBone Blue (ready to be used with various motors), Green, White, XM disappeared. BeagleBone Black has more than a year old OS images (Debian Buster), only newer boards have Debian Bookworm.

It is great that the boards are open-source, but with uncertain SW support, I wouldn't used them professionally. I do use Raspberry Pi professionally, because the compatibility and OS support is excellent.

What do you think?

David

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 2 years ago +2
    I've used BeagleBones and Raspberry Pis both personally and professinally. The last time I used a BeagleBone (Black) professionally was to allow the hole marshalls to switch video sources at the Ryder…
  • flyingbean
    flyingbean over 2 years ago +2
    BBB is better for learning Linux flow, especially for deeper knowledge about kernels. I joined a seminar hosted by bootlin this year. They used BBB as one of two platforms for the training platforms. I…
  • cstanton
    cstanton over 2 years ago +2
    I keep thinking about the beagleboard - Arduino collaboration that almost came to be, the Arduino Tre . Hands on with the Arduino Tre : Developer Edition
Parents
  • battlecoder
    battlecoder over 2 years ago

    I also have a couple of BeagleBone boards that I never used for anything. I always considered them more "industrial" than the Raspberry Pi (leaner distros, less multimedia/entertainment/educational packages by default, so a lot less bloat). So in my mind they are perfect for advanced robots and industrial applications. I even remember running a camera capture + OpenCV example on one of them).

    But I never got to build a project that required a board like that. None of my "robots" ever required anything fancier than a Wemos (this could change soon, though).

    A couple of RPI boards I had also had the same fate, they sit in a drawer; although one of them is working as a local FTP/Git/NodeRED server.

    I still think BB boards is what I would use for a professional project since they boot from on-board memory instead of an SD card, and that already makes them faster and more reliable (the SD card of a Pi, for example, would be prone to failure due to vibration if mounted on a robot, or in any machine in a vibration-rich environment).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 2 years ago in reply to battlecoder

    I almost forgot about the eMMC storage, which should be much more reliable than a micro SD card in a slot.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • koudelad
    koudelad over 2 years ago in reply to battlecoder

    I almost forgot about the eMMC storage, which should be much more reliable than a micro SD card in a slot.