BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum How to copy file from PC to BeagleBone with SSH
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 108 subscribers
  • Views 7574 views
  • Users 0 members are here
Related

How to copy file from PC to BeagleBone with SSH

ninjatrent
ninjatrent over 8 years ago

Hello everyone,

 

My question is, how can I copy a file from a Windows PC to a BeagleBone?

 

I have tried PSFTP for Windows but I get permission denied when I try to copy the file over.

I am logged in as "debian" with default password "temppwd".

Anyone know a solution? I tried logging in as root but I don't know the default password.

 

Thanks for your time and help.

 

Trent

  • Sign in to reply
  • Cancel

Top Replies

  • mp2100
    mp2100 over 8 years ago +6
    And I feel compelled to admit I usually do "sneakernet", for one-time copies. Copy files to USB flash drive, walk it over to beaglebone, copy files.
  • gecoz
    gecoz over 8 years ago in reply to ninjatrent +3
    Hi Trent, Yes, it does. Make sure that the system path includes the path to the pscp.exe file (or you can just cd into the directory containing the executable before executing the command) From your earlier…
  • shabaz
    shabaz over 8 years ago +3
    Hi Trent, Hopefully you've solved it with all the excellent solutions above, otherwise for some examples of the syntax for the method Fabio mentions, see here in the "Transferring Files" section: Accessing…
Parents
  • gecoz
    gecoz over 8 years ago

    Hi Trent,

     

    To copy a file via SSH I usually use scp (PSCP on WIndows). The command syntax is straighforward:

     

    pscp <path_to_the_source_file_to_copy>  <user>@<destination_host>:<absolute_path_to_the_destination>

     

    In your case,  the user is debian, and the absolute path to the destination should point to a directory that the user debian has write permission  for (somewhere inside the user home directory /home/debian is safe).

     

    I hope this helps,

     

    Fabio

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago in reply to gecoz

    Hi Fabio,

     

    Does this need to be typed in Windows Command Prompt?

    pscp <path_to_the_source_file_to_copy>  <user>@<destination_host>:<absolute_path_to_the_destination>

     

    Trent

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gecoz
    gecoz over 8 years ago in reply to ninjatrent

    Hi Trent,

     

    Yes, it does. Make sure that the system path includes the path to the pscp.exe file (or you can just cd into the directory containing the executable before executing the command)

     

    From your earlier reply to Allen, I suspect it is a file permission problem. To copy or move anything in the /usr/bin and /boot/dtbs directories you need root privileges. Perhaps you can try copying the files in the debian user home directory first, then log into the BeagleBone and copy the files to their final destination using sudo.

     

    Fabio

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago in reply to gecoz

    Hi Fabio,

     

    This is correct. Thank you for the help. The files required sudo sed permission to be moved. I've made so many mistakes on this image.

    I am going to start over with a fresh image on the microSD.

     

    Trent

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ninjatrent
    ninjatrent over 8 years ago in reply to gecoz

    Hi Fabio,

     

    This is correct. Thank you for the help. The files required sudo sed permission to be moved. I've made so many mistakes on this image.

    I am going to start over with a fresh image on the microSD.

     

    Trent