BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Black (rev. C) booting from Ethernet (RJ45)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 110 subscribers
  • Views 4049 views
  • Users 0 members are here
Related

Beaglebone Black (rev. C) booting from Ethernet (RJ45)

elem2018
elem2018 over 7 years ago

Hello,

 

I have a BBB rev. C, trying to boot it from ethernet (RJ45) in the sequence of MLO ---> u-boot.img  ---> zImage.bin.  MLO, u-boot.img and zImage.bin are located in the same folder /tftpboot

Following configurations are done in /etc/dhcp/dhcpd.conf

------------------------------------------------------

subnet 192.168.0.0 netmask 255.255.255.0 {

  range 192.168.0.2 192.168.0.100;

  if substring (option vendor-class-identifier, 0, 10) = "AM335x ROM"

  {

    filename "MLO";

  }

  elsif substring (option vendor-class-identifier, 0, 10) = "DM814x ROM"

  {

    filename "MLO";

  }

  elsif substring (option vendor-class-identifier, 0, 17) = "AM335x U-Boot SPL"

  {

    filename "u-boot.img";

  }

  else

  {

    filename "zImage.bin";

  }

}

------------------------------------------------------

I confirm that either tftp and dhcp server works fine, because I tested them in u-boot from a bootable SD card.

Then I removed the SD card, cleaned emmc (writing zeros into emmc) and reset BBB.  I expected that the rom loader in BBB

will read the configration from the dhcpd.conf via ethernet and boot first MLO, then u-boot.img and finally the zImage.bin.

 

But what I see are only CCCCCCC...

Am I missing something in configuration? Would you please help me to make the BBB bootable (MLO, u-boot.img and zImag.bin) from Ethernet?

 

Thanks

Xi

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 7 years ago +1
    According to TI documentation: General Boot Sequence (Linux system) Boot sequence (in order) Boot ROM X-loader U-boot Linux At power-up an OMAP3 device begins booting from internal Boot ROM. This code…
Parents
  • gdstew
    gdstew over 7 years ago

    According to TI documentation:

     

    General Boot Sequence (Linux system)

    Boot sequence (in order)

    • Boot ROM
    • X-loader
    • U-boot
    • Linux


    At power-up an OMAP3 device begins booting from internal Boot ROM.  This code is fixed during the manufacturing process and cannot be altered.  The Boot ROM reads boot configuration pins (SW4 on the OMAP3 EVM) which tell the Boot ROM where to look for the first external bootloader.  The choices include NAND, UART, and SD/MMC Card.  Control is then passed to this first external bootloader called x-loader.  The x-loader application is included in the Linux PSP provided by TI and can be modified by the end user.  The x-loader application passes control to u-boot.  U-boot is also a bootloader and is considered the second external bootloader in this case.


    U-boot is the application which passes control to the Linux system.  The main goal of u-boot is to retrieve the Linux kernel and provide the kernel with information about the location of the Linux filesystem.  U-boot can be configured to retrieve the kernel from NAND, SD/MMC Card, UART or Ethernet (via TFTP).  U-boot can also specify a root filesystem that is located in NAND (jffs2), SRAM (ramdisk), SD/MMC card (ext3 partition) or mounted over IP (NFS).


    U-boot then boots the Linux kernel.  The Linux kernel mounts the Linux root filesystem.

     

     

    So the internal boot ROM will not look for any DHCP configuration information over Ethernet at least, I'm not sure what it is looking for over the UART (an  x-loader?). Your only choices look to be a modified x-loader or U-boot. I know U-boot can boot over

    tftp or nfs so that looks like the easiest path.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 7 years ago

    According to TI documentation:

     

    General Boot Sequence (Linux system)

    Boot sequence (in order)

    • Boot ROM
    • X-loader
    • U-boot
    • Linux


    At power-up an OMAP3 device begins booting from internal Boot ROM.  This code is fixed during the manufacturing process and cannot be altered.  The Boot ROM reads boot configuration pins (SW4 on the OMAP3 EVM) which tell the Boot ROM where to look for the first external bootloader.  The choices include NAND, UART, and SD/MMC Card.  Control is then passed to this first external bootloader called x-loader.  The x-loader application is included in the Linux PSP provided by TI and can be modified by the end user.  The x-loader application passes control to u-boot.  U-boot is also a bootloader and is considered the second external bootloader in this case.


    U-boot is the application which passes control to the Linux system.  The main goal of u-boot is to retrieve the Linux kernel and provide the kernel with information about the location of the Linux filesystem.  U-boot can be configured to retrieve the kernel from NAND, SD/MMC Card, UART or Ethernet (via TFTP).  U-boot can also specify a root filesystem that is located in NAND (jffs2), SRAM (ramdisk), SD/MMC card (ext3 partition) or mounted over IP (NFS).


    U-boot then boots the Linux kernel.  The Linux kernel mounts the Linux root filesystem.

     

     

    So the internal boot ROM will not look for any DHCP configuration information over Ethernet at least, I'm not sure what it is looking for over the UART (an  x-loader?). Your only choices look to be a modified x-loader or U-boot. I know U-boot can boot over

    tftp or nfs so that looks like the easiest path.