BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone functioning
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 106 subscribers
  • Views 907 views
  • Users 0 members are here
Related

Beaglebone functioning

teja2711
teja2711 over 7 years ago

My beaglebone black is not responding after connecting to a power a source. User led's are numb and they dont respond after a long time too.I could not understand the problem.

  • Sign in to reply
  • Cancel

Top Replies

  • mp2100
    mp2100 over 7 years ago +1
    Did it work before, and now it stopped working? Or is this the first time you used it? The user LEDs are the 4 above the mini-USB port. Does the "PWR" LED light up, the one right next to the 5 volt barrel…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi,

     

    Perhaps it is not booting (this can happen if some board is plugged on top). Have you tried powering it up without any cape plugged on?

    It could also be a faulty or corrupted micro SD card, if you're booting off that. Or corrupted on-board Flash. To fix that, you may need a replacement microSD card and reinstall.

    Also, it's highly recommended to connect to the serial pins (e.g. use a 3.3V UART-USB adaptor) to see how far in the boot process it has got.

    To do that, see the section "Using a serial cable" here: Some quick-start things to do for developing on the BBB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago

    Hi,

     

    Perhaps it is not booting (this can happen if some board is plugged on top). Have you tried powering it up without any cape plugged on?

    It could also be a faulty or corrupted micro SD card, if you're booting off that. Or corrupted on-board Flash. To fix that, you may need a replacement microSD card and reinstall.

    Also, it's highly recommended to connect to the serial pins (e.g. use a 3.3V UART-USB adaptor) to see how far in the boot process it has got.

    To do that, see the section "Using a serial cable" here: Some quick-start things to do for developing on the BBB