RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog RIoT Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mconners
  • Date Created: 7 Sep 2014 2:21 PM Date Created
  • Views 4444 views
  • Likes 2 likes
  • Comments 31 comments
Related
Recommended

RIoT Board

mconners
mconners
7 Sep 2014

Recently Element 14 was kind enough to provide me with a RIoT board to evaluate and eventually share my thoughts on the device here on the site.

 

 

Out of the box it looks like most other development boards that I have encountered. A little larger form factor than the Beagle Bone or Raspberry Pi, so you're not going to fit it in an Altoids tin.

 

image

 

The core of the RIoT Board is the Freescale Semiconductor i.MX 6Solo, a ARM Cortex-A9 running at 1 GHz. It features a wide array of peripherals that are available to the user, such as :

1GB DDR3 RAM

10/100/Gb Ethernet

HDMI

LVDS

Headphone jack

Microphone jack

SD card interface

uSD card interface

4 USB ports

4 Serial (TTL) ports

JTAG

2 Camera interfaces

Expansion port featuring I2C, SPI, GPIO

2 user defined LEDs

 

This is already more capable than desktop computers I have owned in my lifetime.

 

Out of the box the RIoT Board is configured with Android 4.3 (Jelly Bean). For initial checkout I connected my monitor to the HDMI port and booted the system into the supplied Android OS. I spent a few minutes playing around in there and noted the capabiilities. It immediately recognized my Logitech wireless keyboard an mouse combo that I had plugged into the USB port. This made navigation a breeze. As expected the RJ45 network connection was recognized an I was able to do a few typical things I might do on a tablet, such as browse the web and run a few applications. I disconnected the wired ethernet connection and tried to connect to the network via a wireless dongle plugged into a USB port but was unsuccessful. My guess is that it is the lack of a driver for the particular device I had selected, but I wasn't really interested in pursuing it much further.

 

 

My real interest in this board was as a computer running Linux. I was able to look around the web as well as the Element 14 site and find some good information on running Linux on this board. I was able to find some instructions on booting Debian Linux directly from the uSD without having to modify the supplied firmware, this seemed like I good option so that was where I started.

 

I found some source to a bootloader, built it and copied it to the SD card. I didn't have a uSD card available, so I went with the full size. Followed some instructions to build a 3.15 kernel, installed a Debian release on the SD card and was off and running. But I wasn't satisfied. I was able to modify the instructions slightly and find a version of Ubuntu that was compatible with the ARM A9 and get that running with minimal effort. Here it is after logging in to the Unity interface

 

image

 

That is running Ubuntu 12.04 LTS. Logging into the system this morning I am seeing a notice that 14.04.1 LTS is currently available. I may have to try that.

 

I was able to hook a 500 GB USB drive to the board so I can see this device becoming a NAS, or a media streamer or finding another purpose around my home as a Thing on the Internet. I had written a device driver years ago for a USB temperature probe and was able to easily move the source to the RIoT Board and recompile with little effort, so it's possible this little device could become a temperature monitor for a critical system in my home (the beer cooler). With the full power of a modern operating system behind it there are few limitations on this device. It can serve web pages, maintain a DB, tweet status, send me emails, the list goes on. With little effort I could have it flash a light or sound a klaxon alerting me that the beer in my cooler is reaching dangerous temperatures.

 

Bottom line, I haven't decided what role this device will play in my life. I can think of many applications. Some temperature related as I have described, or perhaps as a modern BBQ aid. Perhaps in a role to conserve electricity or water by monitoring other less critical systems in my home.  Taking advantage of the camera interface to monitor activity around my front door or the rest of my property. At $79 US, there are a multitude of tasks that can be inexpensively completed, monitored, and reported with minimal effort. The device is probably more limited by my imagination than by its physical capabilities.

 

Once again I thank Element 14 for giving me the opportunity to try out this board.

  • Sign in to reply

Top Comments

  • mconners
    mconners over 12 years ago in reply to johnbeetem +1
    Thanks John. Honestly I don't really think it is adequate as a desktop replacement. It was still a little laggy. TBH, I generally run most of these boards headless. That pic was just for demonstration…
  • tusharp
    tusharp over 12 years ago in reply to mconners +1
    But there is documentation on other sites I posted a glossary with all content till date .
  • mconners
    mconners over 12 years ago in reply to mconners +1
    You know John, one other thought I had on this, I find the Ubuntu Unity interface laggy on even my desktop machines. I always end up installing gnome instead. Perhaps with something light weight like chrome…
  • shabaz
    shabaz over 12 years ago in reply to mconners

    Hi Mike,

     

    Oh! I see it now. You're right, the size difference is virtually nothing - especially when you factor in all the Raspberry Pi protrusions.In fact the RIoTboard would probably take up less real estate due to all that!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 12 years ago in reply to shabaz

    Hey Shabaz, You know I didn't realize it at first, but in my pic of the board it is actually sitting on top of a Raspberry Pi that is in a clear case. You can kid of make it out and see the minimal size difference.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 12 years ago in reply to kylemills

    seemed like the stuff you had was ok. Try that first

     

    mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kylemills
    kylemills over 12 years ago in reply to mconners

    thanks for instructions.

    any instructions on kernel and arm compatible linux file system i can use  ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 12 years ago in reply to mconners

    Also, if you dl the  mainline u-boot type:


    make riotboard_config

    make -j 4

     

    dd if=/dev/zero of=/dev/mmcblk0 bs=1M count=100

    dd if=u-boot.imx of=/dev/mmcblk0 bs=1k seek=1

     

    and that should get you the uboot that works with the bootscript I provided

     

    you will then have to remake your fs and copy everything back on your card

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>