RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Have a RIoTboard question?  Ask the expert, John McLellan
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 33 subscribers
  • Views 9025 views
  • Users 0 members are here
  • the
  • have
  • expert
  • question?
  • john
  • riotboard
  • mclellan
  • ask
  • a
Related

Have a RIoTboard question?  Ask the expert, John McLellan

e14 Contributor
e14 Contributor over 12 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about RIoTboard in the element14 Community RIoTboard group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

 

 

 

 

 

John McLellanJohn McLellan
John McLellan is a hardware hacker, maker, and embedded systems guy with more than 10 years semiconductor experience at Freescale.
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +2
    Hello Selsinork (a great name, by the way) Thanks for the response. I guess others share my frustration. You are correct - it definitely needs an easy-to-install SD image for those who like me don't have…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz +2
    Other than http://www.element14.com/community/message/102310/l/where-does-riot-fit no, not really. At the point I wrote that I wasn't convinced the RIoT had a niche to call it's own. What caused me to…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    kas671 wrote: ... and if there will be an actual linux kernel: will we have an SD Card Image total boot from? there appears to be a non-e14 effort to get mainline u-boot support, see mainline u-boot…
  • denisc1
    denisc1 over 12 years ago

    Hi John

    Just got my RIOT board but so far not impressed.

    The documentation is poor (no actual operation or user guide - lots about the hardware and changing the operating system).

    I can't get a display.

    On one monitor with a DVI to HDMI adapter - nothing.

    On a 42 Panasonic TV with HDMI - Nothing.

    On a Dell monitor with the DVI cable I get the ANDROID appear for a few seconds then a black screen.

    If I hot plug the HDMI cable it shows the booted android screen but the screen asks to plug in the charger (no charger fitted) and then the screen goes black.

    I have checked the power supply and I also have 5V and 3.3V on pins on the DIO port so power is good.

    For something that is supposed to work out of the box it fails badly.

    I am an electronics tech with 20+ years of experience and had no such problems with the dozen or so boards I have used in the past (Arduino, Olimex, PIC ).

    Am I just unlucky or was this released before it was tested properly?

    Regards

    Denis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to denisc1

    It is a shame, but I have to agree with previous post.

     

    I expected to have to do some poking about and troubleshooting but not at the stage of bringing up the pre-loaded OS.


    I plugged in 5V and a Dell HDMI monitor, USB mouse and keyboard and expected the Riot-board to, well,  to work...

    It kind of works, but I can't see the bottom of the screen so can't get HOME.

    It needs a "getting started guide"

    What display will work? (i.e show me the whole screen)I am happy to go and buy one

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello John McLellan,

     

    I have recently used Ubuntu in RIoTBoard and was good but:

     

    Do you have image of Debian for RIoTBoard?

    Also do you have alsa sound driver for "Debian RIoT"?

     

    Best regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hello, you can use these two links to build your Debian rootfs. I didn't try the audio output so I can't help you with second question.

     

    This link will help you create Debian rootfs using debootstrap. It is pretty straightforward so you shouldn't have any problem to achieve that.

    Hard Float on RIoTboard

     

    This link will help you dealing with kernel issue causing segmentation fault after reboot. This require recompiling kernel which is described in RiotBoard manual.

    Reboot of the Linux OS run into segmentation fault

     

    Hope it will help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to e14 Contributor

    @peter

    What display will work? (i.e show me the whole screen)I am happy to go and buy one

     

    There is a LCD8000-97CLCD8000-97C available and its supported by RIoT board .

    It comes with a setup manual .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to denisc1

    @Denis

     

    Thanks for the feedback, you had lots of points so let me address them..

    For actual usage and operation of the operating system, refer to the O/S site.  Here is the Google Developer site which has tons of information about the usage and operation of Android.


    Out of the Box HDMI to HDMI video is currently the best option.  If it's not displaying properly you can try to adjust the screen resolution as described in this post.  I am looking into why the DVI to HDMI conversion. 


    Regarding the screen saying charger not connected disregard that.  There is no charger circuit as you pointed out but the operating system expects one.

    If you are booting up, you are good to go!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    @Peter - Try a few other HDMI enabled monitors or TV's.  My samsung TV did not like it, but LG TV and Acer HDMI monitor gave me no issues.  You can try to adjust the screen resolution as described here.  This issue has made the bug list so we are looking into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Any plans to upstream decent linux support via Shawn Guo @ linaro - the linux imx6 maintainer ? 

     

    Or should we write the board off as Android only ?  I think it'd be a shame to have to do that, especially when it seems that the BeagleBone Black will soon increase to a price very similar to the RIoT.  The RIoTboard could take advantage of the BBB's price increase, but unlikely to do so if the focus stays with Android or increasingly out of date 3.0.35 linux kernels.

    A lot of the other i.MX6 boards like wandboard, Sabre-Lite, etc. are already represented upstream so it's puzzling why the RIoT isn't.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    ... and if there will be an actual linux kernel: will we have an SD Card Image total boot from?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    kas671 wrote:

     

    ... and if there will be an actual linux kernel: will we have an SD Card Image total boot from?

    there appears to be a non-e14 effort to get mainline u-boot support, see mainline u-boot which is a good sign.  An up to date version of u-Boot that supports the board gives us options. Probably it makes creating a linux bootable sd card quite easy to do.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>