RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Ubuntu 14.04
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 27 subscribers
  • Views 4103 views
  • Users 0 members are here
Related

Ubuntu 14.04

e14 Contributor
e14 Contributor over 12 years ago

How can I install an the actual Ubuntu 14.04 or at least how can i fix the reboot problem at ubuntu 12.04.

Has anybody a finished image available for download, in order to use with the riotboard.?

  • Sign in to reply
  • Cancel

Top Replies

  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor +1
    Just came home but selsinork did help already. I´m glad it´s working now.
Parents
  • radiatortwo
    radiatortwo over 12 years ago

    Only alternative right now is compiling the Kernel yourself.

    There is a branch of the original Kernel in which the reboot error is corrected.

     

    I described here how to compile the Kernel.

    Re: Linux : Where is UART's

     

    You then just have to replace the Kernel image file when flashing Ubuntu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    Hallo Mr. Römer sadly copy and paste didn't work at all.

    I always receive following error

    linaro@linaro-ubuntu-desktop:~/linux-imx$ sudo make ARCH=arm CROS_COMPILE=arm-linux-gnueabihf- uImage

    make: arm-fsl-linux-gnueabi-gcc: Command not found

    scripts/kconfig/conf --silentoldconfig Kconfig

    make: arm-fsl-linux-gnueabi-gcc: Command not found

      CHK     include/linux/version.h

      CHK     include/generated/utsrelease.h

    make[1]: `include/generated/mach-types.h' is up to date.

      CC      kernel/bounds.s

    /bin/sh: 1: arm-fsl-linux-gnueabi-gcc: not found

    make[1]: *** [kernel/bounds.s] Error 127

    make: *** [prepare0] Error 2

    linaro@linaro-ubuntu-desktop:~/linux-imx$

     

     

    I tried to do i tby manual and replaced u-boot and linux to embest_imx_3.0.35_4.1.0. and also downloaded the compiler from toochain.

    Make u-boot worked fine, but creating kernel image delivered still the same error.

    I tried on ubuntu 11. now on 12.11 but still the same problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    It appears that Ottos working version is Linux-3.0.35-03023-ga0660f4

     

    Unfortunately, the file in the boot directory is never used.

    Assuming you're using the MFG_Tool, you'd need to replace the uimage in the correct subdirectory and reflash completely. (I don't have a windows machine, so really can't help with MFG_Tool)

     

    The reason it doesn't use the file in the boot directory can be found in the embedded script in u-boot which does this:

     

    bootdelay=3
    baudrate=115200
    ipaddr=192.168.1.103
    serverip=192.168.1.101
    netmask=255.255.255.0
    loadaddr=0x10800000
    rd_loadaddr=(0x10800000 + 0x300000)
    netdev=eth0
    ethprime=FEC0
    uboot=u-boot.bin
    kernel=uImage
    nfsroot=/opt/eldk/arm
    bootargs=console=ttymxc1,115200 nosmp video=mxcfb0:dev=hdmi,1280x720M@60,bpp=32 video=mxcfb1:off
    bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
    bootcmd_net=run bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
    bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait
    bootcmd_mmc=run bootargs_mmc; mmc dev 3; mmc read ${loadaddr} 0x800 0x2000; bootm
    bootcmd=run bootcmd_mmc

    the bit in bold is what loads the kernel and what it's doing is reading raw data directly from the mmc card starting at  1,048,576 bytes into the card, and a length of 4,194,304 bytes.

     

    Theoretically you could use dd to write the new uimage to the card in the correct location with something like:

    dd if=/boot/uImage of=/dev/mmcblk0 bs=1M seek=1

    However, I've never done that and can't guarantee it'll work, so you should be prepared to have to reflash using the MFG_Tool

     

    Note that there's an implicit problem with the u-boot setup that's being used - if you recompile a kernel and it ends up being bigger than 4MB then it won't be able to boot since u-boot will only partially load the kernel image.  I'm sure it's obvious why the way this is currently being done is a bad idea.  The worst part is that there's no need to do this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    well done. dd worked fine.

    Now reboot works.

    why no need to this? "The worst part is that there's no need to do this."

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    basically because u-boot can be setup in such a way that it will read the uImage from the file in /boot which eliminates an extra step and removes any confusion people have with the file being there.  From a technical point of view, reading the file from the filesystem also means the kernel can grow outside the current hard limit of 4MB without requiring any changes.

     

    There are several typical u-boot usage patterns that are not necessary today, probably they still happen due to historic reasons.  I think it's good to drop those things that are not needed, it removes confusion and means nobody has to answer the 'why am I doing this unnecessary step?' type of question image

     

    Anyway, glad the dd command worked!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    Just came home but selsinork did help already.
    I´m glad it´s working now.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • GregC
    GregC over 12 years ago in reply to e14 Contributor

    Eugen

    As suggested by Otto, can you please share your stable Linux Ubuntu 12.04 image with the community ?

    I have limited Linux experience and a slow computer but I would like test it on my RiOT board image

    Thanks in advance
    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to GregC

    You can use the official Linux download and just replace the kernel image in the files folder with mine.

    Then flash it normally with mfgtools.

     

    You then have the same image as Eugen.

    I don't think we need a whole system image for this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    I agree, however mfgtool is a difficulty for a lot of people. Especially with the file in the current download needing renamed before it will work!

     

    In a lot of ways, I think it could be preferable to have simple img files that can be written to SD card, or a BBB style 'flasher' SD card image. Most people can handle win32diskimager by now as it's a common thing to use for most boards. RIoT being different by using mfgtool just adds an obstacle that could easily be removed..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    Jup that´s right. But the only problem is you can´t flash an image directly on the internal eMMC. You´d have to manually copy the image from the sdcard onto the internal flash.

    And I think a lot of people like me want to use the riotboard without extra sdcards.

     

    By the way. I tried putting the board into bootloader mode (the mode when MFGTool writes it´s data onto the board.) and then copy the image onto the flash drive you get then. But no luck. It just crashes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to radiatortwo

    i guess greg is asking for ubuntu 12.04 which Eugen got working

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to e14 Contributor

    mfgtool is a difficulty for a lot of people

    almost every MFG newbie hits the .txt to .xml roadblock, will notify vendor on this image.

    RIoT being different by using mfgtool just adds an obstacle that could easily be removed

    thats a standard set by freescale , RIoT being a i.MX bundle just carries it,  however flashing images in linux is not at all a constraint for linux users.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tusharp
    tusharp over 12 years ago in reply to e14 Contributor

    mfgtool is a difficulty for a lot of people

    almost every MFG newbie hits the .txt to .xml roadblock, will notify vendor on this image.

    RIoT being different by using mfgtool just adds an obstacle that could easily be removed

    thats a standard set by freescale , RIoT being a i.MX bundle just carries it,  however flashing images in linux is not at all a constraint for linux users.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to tusharp

    tushar panda wrote:

    almost every MFG newbie hits the .txt to .xml roadblock, will notify vendor on this .

    I saw you specifically added instructions for that to http://www.element14.com/community/docs/DOC-68063/l/riotboard-updating-os-images-in-windows-environment

    So we can point people to that now image

     

    thats a standard set by freescale , RIoT being a i.MX bundle just carries it,  however flashing images in linux is not at all a constraint for linux users.

    Having several other i.MX6 based boards, I've never come across MFGTool before..  Have used the Linux imx_usb (https://github.com/boundarydevices/imx_usb_loader) variant to update u-boot in spi on both Sabre-Lite and MarS, but that's much more straightforward.

    Other SoC vendors have similar ideas - FEL mode on AllWinner devices for example, where it's a pain as well. Olimex IIRC were at one point charging an extra 10 euros for boards with NAND/Android specifically due to the difficulty of using it (think production line where you're testing lots of boards but can only do one board per Windows PC and it needs manual touch time as the windows util can't easily be automated).

     

    The BBB took the opposite route of using a bootable SD card that when booted automatically formats the eMMC and unpacks a tar.gz file onto it..  This is much the same as what mfgtool does, just less complex from the perspective of the users image

     

    The method described in that blog post is good for linux users, but it's fairly clear from the people asking questions here that most of them are using windows.  The BBB method wins simply because it's useable, and almost identical in operation, whether you're using Mac/Windows/Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to e14 Contributor

    but it's fairly clear from the people asking questions here that most of them are using windows

        will try to layout some thing simple for windows users image.