RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum eMMC Image
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 25 subscribers
  • Views 733 views
  • Users 0 members are here
Related

eMMC Image

omeier
omeier over 12 years ago

Hello,

 

is it possible to create an image of the eMMC that can be easily restored with the MFGTool?

I currently have 3 RIoTboards and it take some time to Upgrade/Install/Configure all needed Packeges.

-> If the Project goes well it can be 100+ boards...

 

Regards,

Oliver

  • Sign in to reply
  • Cancel
Parents
  • radiatortwo
    radiatortwo over 12 years ago

    It´s not possible to create an image and then flash it on the emmc of the board with MFGTool.

     

    What´s possible is, that you create an image, flash it onto an sd card (or dd the image directly on the sd card with the riotboard) and then put it into the next board, boot from it and then dd it onto the emmc.

    You then only have to create one sd card and you can reuse it to flash those 100+ boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • radiatortwo
    radiatortwo over 12 years ago

    It´s not possible to create an image and then flash it on the emmc of the board with MFGTool.

     

    What´s possible is, that you create an image, flash it onto an sd card (or dd the image directly on the sd card with the riotboard) and then put it into the next board, boot from it and then dd it onto the emmc.

    You then only have to create one sd card and you can reuse it to flash those 100+ boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • omeier
    omeier over 12 years ago in reply to radiatortwo

    Yes, this would be an option, and can easyly be done by script.

    -> Does the eMMC holds any data (e.g the serial bootmode or recovery data) that must be preserved or can the eMMC be overwritten from flash 1:1 (starting with addr 0)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to omeier

    The eMMC is simply nothing else but an sdcard.

    The bootcode from u-boot is written at the beginning of the card. So you can copy the whole thing 1:1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to omeier

    check this : Re: How can i create an image of my linux configuration and flash it into emcc

    its like  booting from sdcard & copying the nand mmcblk0.