RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum debug/repair riotboard powerup
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 23 subscribers
  • Views 1229 views
  • Users 0 members are here
Related

debug/repair riotboard powerup

farsi
farsi over 9 years ago

Hello,

 

I haven't been using the riotboard for a while, and now it does not power up anymore (the green LEDs are on, but there is no boot signal on the screen).

 

Is it possible to repair the board, e.g. exchanging the power management IC ?

 

Otherwise, where can I send the board to to have it repaired?

 

Thanks a lot!

  • Sign in to reply
  • Cancel

Top Replies

  • stmorgan
    stmorgan over 9 years ago +1 suggested
    If you are using one of the Linux images, then it is possible that there is nothing wrong with your RIoTboard. Some users (including me) have a problem using the HDMI output with the provided Linux images…
  • stmorgan
    0 stmorgan over 9 years ago

    If you are using one of the Linux images, then it is possible that there is nothing wrong with your RIoTboard.  Some users (including me) have a problem using the HDMI output with the provided Linux images, particularly when an HDMI-to-DVI cable is used to connect to a DVI-D display.  The problem is evident if you use a serial cable connected to the J18 connector to view console output during boot time as noted by this user:

     

    https://www.element14.com/community/thread/37656/l/linux-freezes-when-connected-to-hdmi#174912

     

    Note that the boot process halts after the "Starting kernel ..." message appears.

     

    So you might want to get a serial cable and see what the console output is telling you before making any arrangements for repair, particularly if you have changed anything in your equipment setup since you last used the RIoTboard successfully.  I posted some links on serial cable use in this thread a while back:

     

    https://www.element14.com/community/thread/59383/l/yocto-image-on-riotboard-with-no-keyboard-detection#219067

     

    Also, I would imagine that the cost of repair would equal or exceed buying a new (or used) board, if you are obliged to ship any sub-$100.00US single-board computer (not just RIoTboard) internationally.  Although there are not many RIoTboard sources anymore, there are still a few left:

     

    MCIMX6 SOLO - RIOTBOARD - Development Platform, High-performance Multimedia Processing, RIOT Board, IOT, Cortex-A9 | New…

    RIOT BOARD STARTER KIT - ELEMENT14 - Development Board, RIoT, Enclosure, 1GHz Multimedia Application Processor, Open Sou…

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer