RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum How can i flash using Linux?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 32 replies
  • Subscribers 24 subscribers
  • Views 4024 views
  • Users 0 members are here
  • flash
  • linux
Related

How can i flash using Linux?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

there is no method described in the manual. I guess many (most?) people interested in an open

hardware development device are using linux.

 

I hope there are any tools available and the documentation can be extended.

 

Thanks

 

Steffen

  • Sign in to reply
  • Cancel

Top Replies

  • vandana
    vandana over 12 years ago in reply to e14 Contributor +2
    We will be uploading the actual gerbers very soon - and it will be truly open source. Based on some of the community feedback, we are also looking into CAD library support with other tools. Thanks
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    community.element14.com/.../contentimage_5F00_176409.html It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Though maybe that means eventually it'll have an SD option…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    anthony_h wrote: It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Unfortunately that's so vague as to be pointless.. From a Linux point of view eMMC and SD are…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

     

    to get back to topic ...

     

    At the end i used an old windows notebook for uploading open source to open hardware.

    The result is nothing i would safely call open any more.

     

    Still looking for a linux solution. Of course linux as sd-card image would be perfect ;-)

     

    I had a look on imx_usb_loader, but i didn't got how to use it with the riotboard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Steffen Reinecke wrote:

     

    I had a look on imx_usb_loader, but i didn't got how to use it with the riotboard.

    imx_usb_loader essentially allows you to download some code to the board via a usb connection, in much the same way as the mfg tools.

    Normally you'd use it to download a version of U-Boot which can then subsequently boot linux, android or whatever you choose from any device the version of U-Boot you load supports

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Steffen Reinecke wrote:

     

    I had a look on imx_usb_loader, but i didn't got how to use it with the riotboard.

    imx_usb_loader essentially allows you to download some code to the board via a usb connection, in much the same way as the mfg tools.

    Normally you'd use it to download a version of U-Boot which can then subsequently boot linux, android or whatever you choose from any device the version of U-Boot you load supports