RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum How can i flash using Linux?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 32 replies
  • Subscribers 24 subscribers
  • Views 4003 views
  • Users 0 members are here
  • flash
  • linux
Related

How can i flash using Linux?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

there is no method described in the manual. I guess many (most?) people interested in an open

hardware development device are using linux.

 

I hope there are any tools available and the documentation can be extended.

 

Thanks

 

Steffen

  • Sign in to reply
  • Cancel

Top Replies

  • vandana
    vandana over 12 years ago in reply to e14 Contributor +2
    We will be uploading the actual gerbers very soon - and it will be truly open source. Based on some of the community feedback, we are also looking into CAD library support with other tools. Thanks
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    community.element14.com/.../contentimage_5F00_176409.html It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Though maybe that means eventually it'll have an SD option…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    anthony_h wrote: It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Unfortunately that's so vague as to be pointless.. From a Linux point of view eMMC and SD are…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Remember that the RIoT board is targeted specifically for Android development, not mainline linux.

     

    It's also not a truly open hardware design as the actual CAD files are not provided. There are Gerbers available now which allow you to produce an exact copy, but the Mentor/KiCad/Eagle/whatever source files are not available so you can't easily modify it.

    There are better choices if you want an open hardware board, for eaxmple the Olimex OLinuXino boards.

     

    However, the user manual has section 5 on how to build linux kernel images and you'll find a linux download on this page RIoTboard

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for the reply. You are right - it's maybe not that open.

     

    I have seen the linux image. My problem is, that i don't see a way to upload it to the riotboards eMMc. The mfg tool is not

    running on my linux desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    anthony_h wrote:

     

    It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC.

    My board arrived at the weekend, so I can now refute the claim made in the UM for certain. Exactly what the manual is referring to in that section on p44 isn't clear, what is clear is that it's either misleading or just plain wrong.

     

    I setup a uSD card today with mainline u-boot (0b2da7e209f4110b7c81d578336a10330e4a4404 from 28th March with the patches mentioned here http://www.element14.com/community/thread/32560/l/mainline-u-boot ) and a 3.14 kernel with madewish patches from http://www.element14.com/community/thread/31675?start=16&tstart=0 and have it booting directly from uSD without problem.

     

    The user manual is also particularly unhelpful, Table 4-3 on page 46 shows "Boot Switch Configuration - SD", technically correct but useless information... The SoC has four SD interfaces, the table shows the config to boot from the full-size SD slot at J6 on the underside of the board. To boot from the uSD (J7 on the top of the board) you have to set D7 On, D8 Off. You'll want to grab IMX6SDLRM from Documentation to work out exactly what the switches do. Start with Chapter 8..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I tried the same way, using the mainstream git sources of u-boot, added the riot patches and uploaded with the MfgTool2.exe. But I'm getting no u-boot message on the serial debug console like with the original version. Do I have to use the u-boot.bin or u-boot.imx file?

     

    git clone git://git.denx.e/u-boot.git

    <apply patch>

    make riotboard_config

    CROSS_COMPILE=armv7a-hardfloat-linux-gnueabi- make

    <install u-boot.bin with MfgTool2.exe>

     

    Could you post or upload your corresponding file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    You want u-boot.imx.  I didn't try to upload it using the tool, I just wrote it to a uSD card and then set the switches appropriately

    Fullscreen contentimage_176410.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

    Fullscreen contentimage_176411.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

    the card should have the first partition start at sector 2048, not sector 63.

     

    You then write u-boot.imx to the card starting at 1K with a command something like

     

    dd if=u-boot.imx of=/dev/sdX bs=1024 seek=1

     

    The attached version will look for a file called /bootscript in the first partition..  unfortunately my only copy of that file is on the uSD card that's currently at home, I'll post a copy of it later today.  Even without this, you should still get the u-boot console on the serial port.

     

    However if you have the switches set incorrectly you get nothing.

    Attachments:
    u-boot.imx.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Not really sure if that attachment will work or not, I uploaded a 319KB u-boot.imx and seem to have ended up with a zip file that's a different size image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I think the attachment is ok u-boot.imx has 326656 bytes, here is the situation:

     

    • Original u-Boot console on internal eMMC from RIoT-tools: working, with original ubuntu kernel, but I get CRC error when using my own Gentoo kernel.
      Message from u-Boot (with or without uSD put in):
      Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]
      *** Warning - bad CRC or MMC, using default environment
      MMC read: dev # 3, block #2048, count 8192 ... 8192 blocks read: OK
      ## Booting kernel from Legacy Image at 1080000000 ...
           Image Name:   Linux-3.0.35-02871-ga35ffe
           Image Type:     ARM Linux Kernel Image (uncompressed)
           Date Size:        3901664 Bytes = 3.7 MB
           Load Address: 10008000
           Entry Point:      10008000
           Verifying Checksum ... OK
           Loading Kernel Image ... OK
      OK
      Starting Kernel ...
      Linux version 3.0.35...
    • Your u-boot.imx on external uSD card: no message at all
      Booted ubuntu from eMMC cleared the uSD with dd if=/dev/zero of=/dev/mmcblk1
      Created 4 partitions on uSD with fdisk starting from sector 2048 (uSD hast 4 heads, 16 sectors, 486192 cylinders)
      Installed u-boot.imx with dd if=u-boot.imx of=/dev/mmcblk1 bs=1024 seek=1
      Powered down the system and set the DIP switch for booting from uSD
      Reboot and no reaction on serial console
    • Your u-boot.imx on internal eMMC: no message at all, same as above but used /dev/mmcblk0 instead /dev/mmcblk1
    • Original u-boot-mx6solo-riot.bin on external uSD card: no message at all like above
    • Reflash original u-boot-mx6solo-riot.bin on internal eMMC: works
    • Reflash Android on external SD card: works I can switch between eMMC ubuntu and SD android via DIP switches
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hmm... like I said, I don't have the board here, so it's difficult to check switch settings. I'll do so later this afternoon and let you know. 

     

    file size looks correct, and the exact command I used to write it from the history was dd if=u-boot.imx of=/dev/sdb bs=1024 seek=1 using a usb SD adapter.

     

    Unfortunately uploads here seem to be limited to 50MB, but maybe we just need to find a way to get you a straight copy of my uSD image to try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I found this log in my terminals history showing what you should see, you should at least get the u-boot part with probably an error about missing /bootscript

     

    U-Boot 2014.04-rc2-00094-g7d72f06-dirty (Mar 30 2014 - 18:20:25)

     

    CPU:  Freescale i.MX6SOLO rev1.1 at 792 MHz
    Reset cause: POR
    Board: RIoTboard
    I2C:   ready
    DRAM:  1 GiB
    MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
    No panel detected: default to HDMI
    Display: HDMI (1024x768)
    In:   serial
    Out:  serial
    Err:  serial
    Net:  FEC [PRIME]
    Warning: Your board does not use generic board. Please read
    doc/README.generic-board and take action. Boards not
    upgraded by the late 2014 may break or be removed.
    Hit any key to stop autoboot:  0
    start
    MMC: no card present
    mmc0(part 0) is current device
    load..
    MMC: no card present
    ** Bad device mmc 0 **
    mmc1 is current device
    load..
    473 bytes read in 29 ms (15.6 KiB/s)
    import...
    executing
    2836792 bytes read in 192 ms (14.1 MiB/s)
    kernel_loaded
    33044 bytes read in 76 ms (423.8 KiB/s)
    fdt_loaded
    Kernel image @ 0x12000000 [ 0x000000 - 0x2b4938 ]
    ## Flattened Device Tree blob at 11000000
      Booting using the fdt blob at 0x11000000
      Using Device Tree in place at 11000000, end 1100b113

     

    Starting kernel ...

     

    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 3.14.0-imx (root@sl1) (gcc version 4.8.2 (GCC) ) #9 SMP Tue Apr 1 14:04:31 UTC 2014
    [    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine model: RIoTboard i.MX6SDL
    [    0.000000] cma: CMA: reserved 16 MiB at 3e800000
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] PERCPU: Embedded 8 pages/cpu @edfce000 s8320 r8192 d16256 u32768
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260624
    [    0.000000] Kernel command line: console=ttymxc1,115200n8 rootwait root=/dev/mmcblk0p1 enable_wait_mode=off
    [    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Memory: 1017160K/1048576K available (3802K kernel code, 169K rwdata, 1280K rodata, 196K init, 353K bss, 31416K reserved, 270336K highme)
    [    0.000000] Virtual kernel memory layout:

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Matthias Schwartz wrote:

     

    I think the attachment is ok u-boot.imx has 326656 bytes, here is the situation:

     

    root@fubar01:~/riotboard# ls -l u-boot.imx
    -rw-r--r-- 1 root root 326656 Mar 30 19:23 u-boot.imx
    root@fubar01:~/riotboard# sha256sum u-boot.imx
    36c4d61fa46203b8c4297c94ce5833739674a4bea92ea5766b631b5ab4a5b4ab  u-boot.imx

     

    Hopefully that can confirm the file you have is the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Yes the sha256sum is correct. I think the problem is not the u-boot.imx image. Either the dd call failed or the system needs additional information on the boot device, perhaps the u-boot parameters or some checksum. Or something on my board is corrupt.

     

    I tried dd to /dev/mmcblk0 and /dev/mmcblk1 directly from ubuntu on the RIoT-board and dd to /dev/sda from an x86 linux system with USB to SD converter. Same effect with both. I checked the dip switches multiple times. Are there different board revisions with different switch settings?

     

    When I'm using your u-boot in the serial download mode for BootStrap your UBoot-2014.04-rc2...dirty starts, first success image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    as far as I know, the only requirement is that the u-boot.imx file is written at 1K into the card..  it's obviously important that you don't create a filesystem at sector 63 as that would overwrite u-boot. Hence you create the first partition at 2048 blocks (1MByte) into the card.

    The very same method works on the Wandboard and I've used it sucessfully there too.

     

    Likewise, I've not seen anything to suggest there's more than one revision of the board.  I suppose it's possible that one of the boot settings resistors from p18 of the schematics is missing, but it seems less likely if you're able to get the original images to boot.

     

    If the serial download mode gets you something on the console then it seems it's likely to be switch settings, wrong SD card slot, failed write to the card, or maybe the boot rom is doing something your sd card doesn't like while trying to load u-boot..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    as far as I know, the only requirement is that the u-boot.imx file is written at 1K into the card..  it's obviously important that you don't create a filesystem at sector 63 as that would overwrite u-boot. Hence you create the first partition at 2048 blocks (1MByte) into the card.

    The very same method works on the Wandboard and I've used it sucessfully there too.

     

    Likewise, I've not seen anything to suggest there's more than one revision of the board.  I suppose it's possible that one of the boot settings resistors from p18 of the schematics is missing, but it seems less likely if you're able to get the original images to boot.

     

    If the serial download mode gets you something on the console then it seems it's likely to be switch settings, wrong SD card slot, failed write to the card, or maybe the boot rom is doing something your sd card doesn't like while trying to load u-boot..