RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Getting Ubuntu on Riotboard with a Mac
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 1454 views
  • Users 0 members are here
  • Ubuntu
  • image
Related

Getting Ubuntu on Riotboard with a Mac

e14 Contributor
e14 Contributor over 12 years ago

Can someone point me to a credible link on getting my riotboard setup with Ubuntu. I'm using my macbook pro running OSX mavericks. I just got my board in today and it has been a mess trying to find instructions on getting the board setup with ubuntu. I'm fairly good with terminal on my mac and would like to get this ubuntu install out of the way. Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • lmcelhiney
    lmcelhiney over 10 years ago +1 suggested
    Hi Shane, I use a Macintosh Powerbook to create SD-based versions of Linux OS for my Raspberry PI, Banana PI and Orange PI and Riotboard boards on a regular basis. I always use the current version of OSX…
Parents
  • lmcelhiney
    0 lmcelhiney over 10 years ago

    Hi Shane,

     

    I use a Macintosh Powerbook to create SD-based versions of Linux OS for my Raspberry PI, Banana PI and Orange PI and Riotboard boards on a regular basis. I always use the current version of OSX.  (Also use a 2014 MacMini for the same purpose.)  I realize that this does not provide a link, hence, it might not be of direct use, but want to encourage your experimentation. 

     

    (I have tried to create SD cards from a Windows 7 PC with internal SD card writer and three different external USB SD card writers and the same with Mint running on a 2-year old laptop.  Neither of those machines had success.)

     

    With the Macintosh, it was as easy as:

    • Download a ZIP image file of the desired file for the hardware
    • Use UnArchiver to create the image file.
    • Move image file to my home directory and rename (ex: ubuntu.img to make dd string simpler)
    • Install an SD or microSD (in holder) into card slot
    • Erase card when prompted (use defaults in Disk Utilities app,  as dd will redo it anyway)
    • Unmount the formatted card from Terminal - diskutil unmountDisk disk2
    • Use dd to write image.  sudo dd if=ubuntu.img of=/dev/disk2 bs=4m && diskutil eject disk2
      • Internal slot is disk2
      • Macintosh can handle 4m speed
      • Add the eject to simplify end process
    • Card should now be ready for your single board computer.
    • I created and evaluated 8 different SD cards for a current Banana PI board in one evening.
    • There is a working version of Ubuntu for Riotboard on Element14:  RIoTboard BSP Images and Tools Download - Android and Linux
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tusharp
    0 tusharp over 10 years ago in reply to lmcelhiney

    thanks larry for the instructions,

     

    can you post a small blog on this  ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tusharp
    0 tusharp over 10 years ago in reply to lmcelhiney

    thanks larry for the instructions,

     

    can you post a small blog on this  ??