RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Problem in installing eMMC with Linux from Windows 7 64bit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 1580 views
  • Users 0 members are here
  • riotboard
  • linux
Related

Problem in installing eMMC with Linux from Windows 7 64bit

bose
bose over 12 years ago

Hello,

 

I have just received my RIoT board and wish to change the existing Android OS to Ubuntu.

I downloaded updater tool for Linux Image: http://downloads.element14.com/linux/Linux.zip?ICID=knode-riotboard-quick&COM=RIoTboard

 

However the updater tool would not start up.

The OS on my laptop is Windows 7 64bit.

 

Here are the steps I followed:

1. Set the boot jumpers to Serial Download as stated in the RIoT board User Manual

2. Extract the Linux.zip to a folder

3. Copy the files from 'image_SVN2487' directory to 'tools\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\files' directory.

4. Power up the board using 5V DC jack with 3A power adapter

5. Connect the USB-OTG cable to PC and it recognised as USB HID Input device

6. Run the Updater MfgTool2.exe - However this fails with the below Error

image

I have tried using Admin Mode but does not work and shows the same error.

 

I wish to know if any one has faced this problem or has a solution for this.

Kindly point out if there are any mistakes in my configuration steps.

 

Warm Regards,

Abhijit

  • Sign in to reply
  • Cancel
Parents
  • radiatortwo
    0 radiatortwo over 12 years ago

    You missed a little step.

     

    There´s a little file called ucl2.txt that has to be renamed to ucl2.xml.

     

    It should be here:

    Linux\tools\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\ucl2.txt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • radiatortwo
    0 radiatortwo over 12 years ago

    You missed a little step.

     

    There´s a little file called ucl2.txt that has to be renamed to ucl2.xml.

     

    It should be here:

    Linux\tools\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\ucl2.txt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • bose
    0 bose over 12 years ago in reply to radiatortwo

    Hi,

     

    Thanks for the quick reply.

    I am changing this name and trying out right now.

     

    I will update on my status.

     

    Thanks,

     

    Warm Regards,

    Abhijit