RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Problem in installing eMMC with Linux from Windows 7 64bit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 1580 views
  • Users 0 members are here
  • riotboard
  • linux
Related

Problem in installing eMMC with Linux from Windows 7 64bit

bose
bose over 12 years ago

Hello,

 

I have just received my RIoT board and wish to change the existing Android OS to Ubuntu.

I downloaded updater tool for Linux Image: http://downloads.element14.com/linux/Linux.zip?ICID=knode-riotboard-quick&COM=RIoTboard

 

However the updater tool would not start up.

The OS on my laptop is Windows 7 64bit.

 

Here are the steps I followed:

1. Set the boot jumpers to Serial Download as stated in the RIoT board User Manual

2. Extract the Linux.zip to a folder

3. Copy the files from 'image_SVN2487' directory to 'tools\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\files' directory.

4. Power up the board using 5V DC jack with 3A power adapter

5. Connect the USB-OTG cable to PC and it recognised as USB HID Input device

6. Run the Updater MfgTool2.exe - However this fails with the below Error

image

I have tried using Admin Mode but does not work and shows the same error.

 

I wish to know if any one has faced this problem or has a solution for this.

Kindly point out if there are any mistakes in my configuration steps.

 

Warm Regards,

Abhijit

  • Sign in to reply
  • Cancel
Parents
  • ansmp
    0 ansmp over 12 years ago

    Somebody knows how many cycles of rewriting supports emmc ( MTFC4GMDEA)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • radiatortwo
    0 radiatortwo over 12 years ago in reply to ansmp

    Can´t tell you specific things about this eMMC chip. Only found out that it´s a MCP. (Multi Chip Package)

     

    But since it´s just a normal NAND Flash: With SLC you have about 100k or more cycles. With MLC Chips it´s about 10k or more.

    I can´t find info if the chip is SLC or MLC. But I think it´s one with MLC because SLC chips are pretty expensive.

     

    FYI:

    SLC = Single Level Cell

    MLC = Multi Level Cell

     

    With SLC only one bit per cell is saved.

    With MLC two bit per cell is saved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • radiatortwo
    0 radiatortwo over 12 years ago in reply to ansmp

    Can´t tell you specific things about this eMMC chip. Only found out that it´s a MCP. (Multi Chip Package)

     

    But since it´s just a normal NAND Flash: With SLC you have about 100k or more cycles. With MLC Chips it´s about 10k or more.

    I can´t find info if the chip is SLC or MLC. But I think it´s one with MLC because SLC chips are pretty expensive.

     

    FYI:

    SLC = Single Level Cell

    MLC = Multi Level Cell

     

    With SLC only one bit per cell is saved.

    With MLC two bit per cell is saved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ansmp
    0 ansmp over 12 years ago in reply to radiatortwo

    Thanks, but i found a wide spacing in data - 3 к - 10 к.