RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum RIOT board booting problem
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 23 subscribers
  • Views 525 views
  • Users 0 members are here
  • embedded
  • arm
Related

RIOT board booting problem

e14 Contributor
e14 Contributor over 12 years ago

HI,

 

                     This is pushpa associated with J-tech India .we are working with RIOT board for one of my project . I was trying to boot the board by taking demo image i was trying to load Linux by using MFG tool . i kept the board to eMMC mode according to the user manual i loaded images and seen output in putty i was getting the error .like this

 

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:00:00:00:00:00

----enet_board_init: phy reset

FEC0 [PRIME]

Hit any key to stop autoboot:  0

booti: bad boot image magic

fastboot is in init......flash target is MMC:3

Bad partition index:2 for partition:recovery

Bad partition index:5 for partition:system

USB Mini b cable Connected!

fastboot initialized

USB_SUSPEND

 

 

RIOT board cannot boot Linux through SD card i contacted em beast people he told me to try from another PC i did as per his instructions but error not solved .then i loaded u boot through MFG and i i tried to load u Image and root file system by using NFS but struck with the new error

 

Loading : T T T T T T T T T T T T

 

of above please can help me with your valuable guidance

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Pushpa,

    I got my RiotBoard last week and haven't observed your problems. I've completed the following;

     

    1- Boot up the default Android. This is a good basic test.

        I actually had an issue where it didn't like my HDMI to VGA converter. I actually had to plug it into a proper VGA monitor. That was an important learning step for me.

     

    2- Download and burn the Ubuntu SD image. I used Win32DiskImager (used to burn Raspberry Pi images), burnt the image. Powered off the board, changed the switches on the board, inserted the SD and powered on. After a minute or so it booted up healthy. This was a great troubleshooting step.

     

    3- I then used the MFG tool to burn the Ubuntu kit to the board. I downloaded the kit and tool. I powered off the board, set the switches as per the instructions. Plugged in the USB cable that came with the board, you connect it from your PC to the little uUSB port near the SD card. Powered up the board. Waited for Win7 to recognize the device and load the driver. Then followed the instructions for the MFG tool from the manual. It took about an hour (not sure I was doing something else) to complete. Once done I selected "Stop" then "Exit" as per the manual. And then I unplugged the USB cable, powered off the board, changed the switches (as per the manual) and powered the board back on. After a minute it booted into the Ubuntu desktop.

     

    The documentation was a bit daunting. However it all just worked without any major issues.

     

    My suggestion is to try each of the above to help build your confidence with the board, documentation and process. If you have issues re-read the document and double check you have the switches set correctly. And ensure you follow the documentation.

     

    Regards,

    Dave