RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Problem in using the Linux BSP from element14
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 24 subscribers
  • Views 1250 views
  • Users 0 members are here
  • riotboard
Related

Problem in using the Linux BSP from element14

Nitin_Bhaskar
Nitin_Bhaskar over 12 years ago

Hi all,

 

I tried booting RiotBoard from SD card as described in this document. I used Linux.zip BSP. But I faced kernel panic issue,

 

sgtl5000 0-000a: Failed to get supply 'VDDD': -19

print_constraints: 0-000a: 850 <--> 1600 mV at 1200 mV normal

sgtl5000 0-000a: sgtl5000 revision 17

mmc0: new high speed DDR MMC card at address 0001

mmcblk0: mmc0:0001 MMC04G 3.57 GiB

mmcblk0boot0: mmc0:0001 MMC04G partition 1 2.00 MiB

mmcblk0boot1: mmc0:0001 MMC04G partition 2 2.00 MiB

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk0: p4 size 5324800 extends beyond EOD, truncated

mmcblk0boot1: unknown partition table

mmcblk0boot0: unknown partition table

asoc: sgtl5000 <-> imx-ssi.1 mapping ok

imx_3stack asoc driver

asoc: mxc-hdmi-soc <-> imx-hdmi-soc-dai.0 mapping ok

ALSA device list:

  #0: sgtl5000-audio

  #1: imx-hdmi-soc

NET: Registered protocol family 26

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

mmc1: new high speed SDHC card at address 1234

mmcblk1: mmc1:1234 SA04G 3.63 GiB

mmcblk1: p1

List of all partitions:

b300         3751936 mmcblk0  driver: mmcblk

  b301            8192 mmcblk0p1 00000000-0000-0000-0000-000000000000

  b302            8192 mmcblk0p2 00000000-0000-0000-0000-000000000000

  b303               1 mmcblk0p3 00000000-0000-0000-0000-000000000000

  b304         2621440 mmcblk0p4 00000000-0000-0000-0000-000000000000

  b305          524287 mmcblk0p5 00000000-0000-0000-0000-000000000000

  b306          524287 mmcblk0p6 00000000-0000-0000-0000-000000000000

  b307            8191 mmcblk0p7 00000000-0000-0000-0000-000000000000

  103:00000       8191 mmcblk0p8 00000000-0000-0000-0000-000000000000

b310            2048 mmcblk0boot1  (driver?)

b308            2048 mmcblk0boot0  (driver?)

b318         3813376 mmcblk1  driver: mmcblk

  b319         3805184 mmcblk1p1 00000000-0000-0000-0000-000000000000

No filesystem could mount root, tried:  ext3 ext2 ext4 cramfs vfat msdos

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,1)

[<80048834>] (unwind_backtrace+0x0/0xf8) from [<80514554>] (panic+0x74/0x18c)

[<80514554>] (panic+0x74/0x18c) from [<80008d58>] (mount_block_root+0x1e0/0x224)

[<80008d58>] (mount_block_root+0x1e0/0x224) from [<80008e84>] (mount_root+0xe8/0x108)

[<80008e84>] (mount_root+0xe8/0x108) from [<80008fc4>] (prepare_namespace+0x120/0x178)

[<80008fc4>] (prepare_namespace+0x120/0x178) from [<800089b0>] (kernel_init+0x108/0x13c)

[<800089b0>] (kernel_init+0x108/0x13c) from [<80042aa4>] (kernel_thread_exit+0x0/0x8)

 

Did anyone face similar issue?

  • Sign in to reply
  • Cancel
Parents
  • Nitin_Bhaskar
    0 Nitin_Bhaskar over 12 years ago

    Well it looks like the issue is with the kernel. I compiled kernel from embest and re-flashed only kernel. It worked!!!

     

    Following are the steps I followed for kernel compilation.

     

    git clone git://github.com/embest-tech/linux-imx.git -b embest_imx_3.0.35_4.0.0
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- imx6_defconfig
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- uImage

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Nitin_Bhaskar
    0 Nitin_Bhaskar over 12 years ago

    Well it looks like the issue is with the kernel. I compiled kernel from embest and re-flashed only kernel. It worked!!!

     

    Following are the steps I followed for kernel compilation.

     

    git clone git://github.com/embest-tech/linux-imx.git -b embest_imx_3.0.35_4.0.0
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- imx6_defconfig
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- uImage

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer