RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Linux freezes when connected to HDMI
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 5407 views
  • Users 0 members are here
  • hdmi
  • riotboard
Related

Linux freezes when connected to HDMI

e14 Contributor
e14 Contributor over 12 years ago

I have loaded the Linux image SVN2652 on Riotboard, but it only boots if HDMI is not connected.

If I connect the HDMI after Linux starts running it also freezes.

The kernel is: Linux version 3.10.17_1.0.0_RIoTboard+g9ba99b4 (luofc@embest-tech) (gcc version 4.8.1 (GCC) ) #1 SMP PREEMPT Thu Jun 19 09:46:07 CST 2014.

I have tried it on two other boards with the same result. If I stop the boot it displays the Freescale logo, so the hardware seems to work.

Could it be a driver problem?

Is there a fix for this?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • tusharp
    0 tusharp over 12 years ago

    hi cristian,

     

    I guess you have downloaded from here : https://www.dropbox.com/sh/nuhzba8uqpijenb/AAAt8l9g6u6T6-DOqJHozyKca/fsl-image-fb-riotboard.sdcard?dl=1

     

    If I connect the HDMI after Linux starts running it also freezes.

    The HDMI screen freezes or Riotboard booting ??

     

    it only boots if HDMI is not connected.

    The HDMI GUI support is not yet enabled in kernel.

    on display devices it will show a terminal with Yocto signature as shown below.

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to tusharp

    If I stop the boot it displays the Freescale logo

     

    if possible, plz share a snapsort  .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    Hi,

    Just to clarify, I don't want a GUI, my application uses GStreamer to output straight to the framebuffer.

    I have tried both the downloaded file and also one that I build with Yocto (fsl-image-fb),  with the same result.

     

    If I have the HDMI cable connected the kernel would not start. Here is the console output:

    ---------------------------------------------------------------------------------------------------------

    U-Boot 2013.04-04988-gd2e8066-dirty (Jul 04 2014 - 09:18:53)

     

     

    CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz

    CPU:   Temperature 35 C, calibration data: 0x5915165f

    Reset cause: POR

    Board: MX6SOLO RIoTboard

    I2C:   ready

    DRAM:  1 GiB

    MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

    *** Warning - bad CRC, using default environment

     

     

    No panel detected: default to HDMI

    Display: HDMI (640x480)

    In:    serial

    Out:   serial

    Err:   serial

    mmc2(part 0) is current device

    Net:   FEC [PRIME]

    Warning: failed to set MAC address

     

     

    Normal Boot

    Hit any key to stop autoboot:  0

    mmc2(part 0) is current device

    reading boot.scr

    ** Unable to read file boot.scr **

    reading uImage

    5275824 bytes read in 274 ms (18.4 MiB/s)

    Booting from mmc ...

    reading imx6solo_RIoTboard.dtb

    43553 bytes read in 21 ms (2 MiB/s)

    ## Booting kernel from Legacy Image at 12000000 ...

       Image Name:   Linux-3.10.17_1.0.0_RIoTboard+g9

       Image Type:   ARM Linux Kernel Image (uncompressed)

       Data Size:    5275760 Bytes = 5 MiB

       Load Address: 10008000

       Entry Point:  10008000

       Verifying Checksum ... OK

    ## Flattened Device Tree blob at 18000000

       Booting using the fdt blob at 0x18000000

       Loading Kernel Image ... OK

    OK

       Using Device Tree in place at 18000000, end 1800da20

     

     

    Starting kernel ...

    --------------------------------------------------------------------------------------------

     

    If I have the cable initially disconnected it works OK. As soon as I connect the cable Linux freezes. No serial console and the LED stops blinking.

     

    The strange thing is that I have a board that works with no problems at all and another four that behave like I described.

    I currently don't have the working board with me to see if there is a hardware difference (however unlikely that is). I should get it back next week.

    The software is exactly the same on all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I have the same problem.  I have 6 boards all flashed with the same u-boot, 3.10 kernel and ubuntu 14.04.

     

    4 of them work great.  Both the serial console and the hdmi work well.

     

    On 1 the serial console does not display anything but the hdmi works.

     

    The last 1 has the same problem described here.  If I plug the hdmi cable it freezes.  From the serial console I am able to see u-boot go but it gets stuck at "Starting kernel ..." just like yours:

     

    U-Boot 2013.04-04992-g002bd44 (Oct 10 2014 - 16:41:48)

     

    CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz

    CPU:   Temperature 41 C, calibration data: 0x5935125f

    Reset cause: POR

    Board: MX6SOLO RIoTboard

    I2C:   ready

    DRAM:  1 GiB

    MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

    *** Warning - bad CRC, using default environment

     

    No panel detected: default to HDMI

    Display: HDMI (640x480)

    In:    serial

    Out:   serial

    Err:   serial

    mmc2(part 0) is current device

    Net:   FEC [PRIME]

    Warning: failed to set MAC address

     

    Normal Boot

    Hit any key to stop autoboot:  0

    mmc2(part 0) is current device

    reading boot.scr

    ** Unable to read file boot.scr **

    reading uImage

    5580480 bytes read in 352 ms (15.1 MiB/s)

    Booting from mmc ...

    reading imx6solo_RIoTboard.dtb

    46379 bytes read in 20 ms (2.2 MiB/s)

    ## Booting kernel from Legacy Image at 12000000 ...

       Image Name:   Linux-3.10.17_1.0.0_RIoTboard-80

       Image Type:   ARM Linux Kernel Image (uncompressed)

       Data Size:    5580416 Bytes = 5.3 MiB

       Load Address: 10008000

       Entry Point:  10008000

       Verifying Checksum ... OK

    ## Flattened Device Tree blob at 18000000

       Booting using the fdt blob at 0x18000000

       Loading Kernel Image ... OK

    OK

       Using Device Tree in place at 18000000, end 1800e52a

     

    Starting kernel ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    About the time I posted my first message I have also contacted Embest via their web site. I got a couple of replies asking for more info, but I haven't heard from them since. I can only assume they don't have an answer or simply don't care.

    Since I am developing a commercial product and have no time to muck around  I had to go back to kernel 3.0.35 (using the good old LTIB).

    So far, so good. All my boards seem to work OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    About the time I posted my first message I have also contacted Embest via their web site. I got a couple of replies asking for more info, but I haven't heard from them since. I can only assume they don't have an answer or simply don't care.

    Since I am developing a commercial product and have no time to muck around  I had to go back to kernel 3.0.35 (using the good old LTIB).

    So far, so good. All my boards seem to work OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tusharp
    0 tusharp over 12 years ago in reply to e14 Contributor

    I had to go back to kernel 3.0.35 (using the good old LTIB).

    So far, so good. All my boards seem to work OK.

    I am unable to generate the HDMI freeze issue.

    does this occur after any changes made to bsp or its a custom bsp .

     

    which BSP version you are using ??