RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Accessing SPDIF input pins
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 24 subscribers
  • Views 751 views
  • Users 0 members are here
  • spdif
Related

Accessing SPDIF input pins

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

we have two RIoT boards in our test setups now, along with other imx6 boards, and they are working great! We are able to use SPI, I2C, UART and other connections. On other boards we now also acitivated the SPDIF input of the imx. Sadly, there is no pin available for this on the RIoT's expansion port.

 

The possible pins for SPDIF input are:

EIM_DATA_21

ENET_RX_ER

GPIO_16

KEY_COL3

 

The question is now: How to access one these pins most comfortably?

Does anybody now if GPIO_16 is available on the bottom of the board, so we could solder a wire to it?

Does any of the other pins have an easily accessible contact spot?

 

Thanks,

 

Jonas.

  • Sign in to reply
  • Cancel
  • tusharp
    0 tusharp over 12 years ago

    Not sure if its possible.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In the meantime I was able to access one of the pins. ENET_RX_ER is connected to the USB OTG socket, as pin nr. 4. Using the instructions from the Udoo forums (Forum | UDOO) one can enable the SPDIF input and then either solder a new wire at the back of the USB connector, or make a custom cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to e14 Contributor

    talking about alternatives:

     

    EIM_D21 & EIM_D22 can be used as SPDIF IN & OUT but at the cost of USB OTG pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    Those two pins have the problem that they are not directly wired to the USB connector, but to U20, the USB IC. The only one directly connected from the CPU to the USB is ENET_RX_ER. Note that I am talking only about SPDIF input. Output is not required in our project, so I haven't done any research regarding the other pins.