RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Inserting USB Thumb Drive Causes The Riotboard to reboot
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 25 subscribers
  • Views 734 views
  • Users 0 members are here
  • reboots
  • causing
  • port
  • usb
  • riotboard
Related

Inserting USB Thumb Drive Causes The Riotboard to reboot

rshuler
rshuler over 11 years ago

Hi,

 

Has anyone seen an issue when inserting a USB Thumb into the Riotboard USB Port?  I'm finding that the Riotboard will reset / reboot as soon as the USB Thumb Drive touches the outside of the USB Port shield.  I have been able to reproduce this issue many times, and with different USB Thumb Drives.  All you need to do is wait until the Riotboard has finished booting, and setting at the desktop.  Then take a USB Thumb Drive and insert it in the Riotboard USB port or touch the outside of the Riotboard USB Port ( you may have to touch the thumb to the outside of the USB port a few times before) it will reboot, and it seems to always reboots.  The longer the Riotboard is powered up, the sooner it will reboot when the USB Thumb drive is touched to the USB port or inserted into the USB port.

 

OS: Android 4.3

 

Any recommendation for resolving this failure would be helpful.

 

Thanks,

Robert

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Robert,

    I've got a RiotBoard, received last week. Just loaded linaro-ubuntu the last few days. I've been putting in a couple of different USB keys to install java kits, etc. and I haven't seen your problem. Just now as a test I've been trying repeatedly to reproduce your problem and no issues. Though I doubt the OS has anything to do with it when it's just touching the outside metal of the USB connector.

     

    Off the top of my head - it's most likely static electricity. Low humidity is the biggest cause, especially if you are in hemisphere and it's winter. If so try increasing the humidity a bit. Clothing/carpet etc. can be a cause too (wool and nylon together are a bad mix). But again all of this can be exacerbated by low humidity.

     

    Also do you have it in a case? or is it sitting on the bench? Mine is just sitting on a piece of paper on the book shelf, no case. However depending how you have it set up you could be shorting it etc.

     

    One final thought, power the board off, and examine it under a magnifying glass and bright light to see if there are any mechanical defects to the USB connection soldering to the board, if the solder joints are cracked or something looks bad, then it may also be the culprit. However looking at mine it seems well constructed with no mechanical issues.

     

    I hope you get it sorted.

     

    Regards,

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • radiatortwo
    0 radiatortwo over 11 years ago

    This can happen if the power supply you are using is too weak.
    When putting a USB device in you get a peak in the current drawn from the board.
    Which can lead to a voltage drop if the power supply can´t handle it, forcing the board to reset.

     

    If the tips from Dave R didn´t help try a stronger power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rshuler
    0 rshuler over 11 years ago in reply to e14 Contributor

    Hi Dave,

     

    Thanks for the suggestions.  We grounded the Riotboard to the chassis and this has so far seemed to help.  This was really odd.  All you had to do was touch the USB port housing shield with anything metallic (pins, usb cables tips, etc) and the Riotboard would reset.

     

    Thanks for the help,

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rshuler
    0 rshuler over 11 years ago in reply to radiatortwo

    Hi Otto,

     

    Thanks for the response to my question.  We never had to actually plug in a USB device to get the Riotboard to reset.  All we had to was touch the USB Housing with something metallic like a pen, or the end of an unconnected used be cable to generate the reset. 

     

    Our power supply was 5V/4A.

     

    We ended up grounding the Riotboard  by moving it to the embedded housing that we use for our embedded products and making sure it was grounded to the chassis.  So far, this has appeared to help.  I want call it fix yet.

     

    Thanks,

    Robert