WaRP7
  • Products
  • Dev Tools
  • Single-Board Computers
  • WaRP7
  • More
  • Cancel
WaRP7
Blog Warp7 Yocto : Part1 : setup, configure and generate Warp7 binaries
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WaRP7 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tusharp
  • Date Created: 16 Sep 2016 7:30 AM Date Created
  • Views 9913 views
  • Likes 4 likes
  • Comments 89 comments
  • tusharp
  • imx7
  • yocto
  • image
  • bitbake
  • warp7
  • embedded
  • yocto-bsp
  • linux
Related
Recommended

Warp7 Yocto : Part1 : setup, configure and generate Warp7 binaries

tusharp
tusharp
16 Sep 2016

Contents

1. Warp7 Yocto Part1 <-- You are here

2. Warp7 Yocto Part2

3. Warp7 Sensors demo - mpl3115a2

4. Warp7 Sensors demo - fxos8700cq

5. Warp7 IoT demo

 

The Warp7 is a next generation Wearable and IoT development platform.

plz refer  NXP and element14 website for more platform related information.

 

Warp7 Board

fd53fb.jpg

CPU Board

34nmm39.jpg

IO Board

2dkfsao.jpg

 

In this blog we will

1. Download warp7 yocto sources.

2. Setup required environment.

3. add/customise warp7 machine configs.

4. Compile and generate binaries.

 

 

A bit on yocto before we start :

oq9937.jpg

 

If you are new to yocto , plz make sure to check the yocto project before proceeding.

 

Platform Setup:

I am using Ubuntu 14.04 x86_64 for the build process. you can use do this from a Virtual Machine (vmware, virtualbox) also.

 

We need to install some packages on which yocto depends for the build process.

sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev \
xterm sed cvs subversion coreutils texi2html python-pysqlite2 help2man make gcc g++ desktop-file-utils libgl1-mesa-dev \
libglu1-mesa-dev mercurial autoconf automake groff curl lzop u-boot-tools

 

vr90kz.jpg

 

Download repo:

We need to have a repo tool to pull yocto sources.

 

mkdir ~/bin
curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
chmod a+x ~/bin/repo
export PATH=~/bin:$PATH

 

Download Yocto:

following steps will help download yocto sources from NXP(Freescale) official repository:

 

mkdir warp7_yocto
cd warp7_yocto
repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b krogoth
repo sync

 

Before building the yocto bsp we need to update the yocto build with warp7 config.

To configure we need to pass the proper MACHINE name as a macro.

 

Determine machine name:

echo; ls sources/*/conf/machine/*.conf | sed s/\.conf//g | sed -r 's/^.+\///' | xargs -I% echo -e "\t%" | grep imx

 

1444o6p.jpg

 

The Warp7 machine name is imx7s-warp .

 

 

Setting up the environment:

 

MACHINE=imx7s-warp source setup-environment build

 

2useno7.jpg

 

Select "Y" to accept the EULA license and complete the machine config setup.

 

9bi39u.jpg

 

Now a build directory is created under ~/warp7_yocto directory.

It contains the build system settings for warp7 machine(i.e local.conf) and yocto bitbake layers path information (i.e bblayers.conf).

 

local.conf

1z4a4vn.jpg

 

bblayers.conf

141tfeq.jpg

 

 

Customise warp7 machine config:

Now edit the kernel source in warp7 machine configuration file.

 

in ~/warp7_yocto/sources/meta-fsl-arm-extra/conf/machine/imx7s-warp.conf file, edit as below.

Replace

PREFERRED_PROVIDER_virtual/kernel ?= "linux-fslc-imx"

with

PREFERRED_PROVIDER_virtual/kernel ?= "linux-warp"

 

Now the kernel source will be pulled from the linux-warp%%  bitbake recipe.

Create a directory named "linux-warp7-4.1" and recipe named "linux-warp7_4.1.bb" in below path.

~/warp7_yocto/sources/meta-fsl-arm-extra/recipes-kernel/linux/

 

mkdir ~/warp7_yocto/sources/meta-fsl-arm-extra/recipes-kernel/linux/linux-warp7-4.1
touch ~/warp7_yocto/sources/meta-fsl-arm-extra/recipes-kernel/linux/linux-warp7_4.1.bb

 

 

Populating warp7 recipe:

populate the recipe "linux-warp7_4.1.bb" with below contents.

# Released under the MIT license (see COPYING.MIT for the terms)

 

include recipes-kernel/linux/linux-imx.inc

include recipes-kernel/linux/linux-dtb.inc

 

DEPENDS += "lzop-native bc-native"

 

SRCBRANCH = "4.1-1.0.x-imx"

SRCREV = "fa571312b4271e368ca99ffcdf7992247d534e55"

 

SRC_URI = "git://github.com/WaRP7/linux-fslc.git;branch=${SRCBRANCH} \

           file://defconfig"

 

COMPATIBLE_MACHINE = "(imx7s-warp)"

 

In above recipe we setup 4.1-1.0.x-imx as source branch for our kernel and file defconfig will be the default kernel config file.

Next copy the defconfig file (in attachment) into the linux-warp7-4.1 directory.

 

 

Downloading yocto packages:

If you want to build images offline, its a good idea to download the packages first.

bitbake core-image-minimal -c fetchall

 

 

Build:

bitbake core-image-minimal

 

Now build, it will take several hours to complete depending on your PC configuration.

 

While kernel build is in process you might encounter an error wrt imx7s-warp.dtb.

This will happen is there is no imx7s-warp.dts file in below directory.

~/warp7_yocto/build/tmp/work/imx7s_warp-poky-linux-gnueabi/linux-warp7/4.1-r0/git/arch/arm/boot/dts

 

below is a snapshot from the log file that captured the above  error.

90avr7.jpg

 

In that case copy the imx7s-warp.dts from the attachments to the below directory:

~/warp7_yocto/build/tmp/work/imx7s_warp-poky-linux-gnueabi/linux-warp7/4.1-r0/git/arch/arm/boot/dts

 

2s7dqv4.jpg

 

Now hit build again.

 

After build completed, the images build are found in ~/warp7_yocto/build/tmp/deploy/images/imx7s-warp

noajk7.jpg

 

 

Let us know any challenges faced during build procedure through comments.

 

Next time we will flash the generated images.

 

Happy Warping.

Attachments:
warp7_attachments.zip
  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 9 years ago in reply to Jan Cumps +1
    Jan Cumps wrote: bitbake -fetch finished successful (14 hours on the raspberry pi to complete all 189 jobs. it used 4 job threads to allocate tasks on this board), now up to the next step: build That's…
  • bheemarao
    bheemarao over 9 years ago +1
    I tried building the same as shown steps below bheema@Bheema:~/warp7_yocto$ MACHINE=imx7s-warp source setup-environment build-warp7 then by default the kernel will fetch from "include recipes-kernel/linux…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps +1
    Installing the dependencies. Once I'm at the bitbake line, I'll switch to bheemarao 's steps...
  • texierp
    texierp over 8 years ago in reply to ba243

    Hello,

     

    Have you tried with : bitbake core-image-minimal ?

     

    BR

     

    PJ

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ba243
    ba243 over 8 years ago

    image

    Hello, I followed step by step for the configuration but to generate the image with the bitbake command iot-qt-image I have errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • griff0417
    griff0417 over 8 years ago in reply to marcocavallini

    Hi Marco,

     

    After taking a look at lsusb output with switch 2 on the base board in upper position, this is what I found.  The vid and pid which shows in lsusb (15a2:0076) matches whats in the imx_usb.conf.

     

    I am using vmware with open-vm-tools

     

    My lsusb output:

    :~$ lsusb
    Bus 004 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
    Bus 003 Device 004: ID 0e0f:0002 VMware, Inc. Virtual USB Hub
    Bus 003 Device 003: ID 0e0f:0002 VMware, Inc. Virtual USB Hub
    Bus 003 Device 005: ID 15a2:0076 Freescale Semiconductor, Inc. 
    Bus 003 Device 002: ID 0e0f:0003 VMware, Inc. Virtual Mouse
    Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
    Bus 002 Device 002: ID 0e0f:0002 VMware, Inc. Virtual USB Hub
    Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub

     

    imx_usb.conf from https://github.com/boundarydevices/imx_usb_loader

    #vid:pid, config_file
    0x066f:0x3780, mx23_usb_work.conf
    0x15a2:0x004f, mx28_usb_work.conf
    0x15a2:0x0052, mx50_usb_work.conf
    0x15a2:0x0054, mx6_usb_work.conf
    0x15a2:0x0061, mx6_usb_work.conf
    0x15a2:0x0063, mx6_usb_work.conf
    0x15a2:0x0071, mx6_usb_work.conf
    0x15a2:0x007d, mx6_usb_work.conf
    0x15a2:0x0080, mx6_usb_work.conf
    0x15a2:0x0076, mx7_usb_work.conf
    0x15a2:0x0041, mx51_usb_work.conf
    0x15a2:0x004e, mx53_usb_work.conf
    0x15a2:0x006a, vybrid_usb_work.conf
    0x066f:0x37ff, linux_gadget.conf

     

    I see now that your post is updated and you got it working with vmware but I figured I'd just post this anyways. Glad to hear you were able to get things working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • marcocavallini
    marcocavallini over 8 years ago in reply to griff0417

    Hi Jason,

    I am using Virtual Box at the moment and the load u-boot via USB procedure fails:

     

    $ sudo ./imx_usb ../u-boot-imx7s-warp.imx 
    [sudo] password for tux: 
    config file <.//imx_usb.conf>
    vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf
    vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf
    vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf
    vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf
    vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf
    vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf
    vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf
    vid=0x15a2 pid=0x007d file_name=mx6_usb_work.conf
    vid=0x15a2 pid=0x0080 file_name=mx6_usb_work.conf
    vid=0x15a2 pid=0x0076 file_name=mx7_usb_work.conf
    vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf
    vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf
    vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf
    vid=0x066f pid=0x37ff file_name=linux_gadget.conf
    no matching USB device found

     

    in fact

    $ dmesg
    [   29.100155] ftdi_sio 2-3:1.0: FTDI USB Serial Device converter detected
    [   29.100249] usb 2-3: Detected FT2232C
    [   29.111951] usb 2-3: FTDI USB Serial Device converter now attached to ttyUSB0

     

    and

    $ lsusb
    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
    Bus 002 Device 004: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
    Bus 002 Device 003: ID 058f:9540 Alcor Micro Corp. 
    Bus 002 Device 002: ID 80ee:0021 VirtualBox USB Tablet
    Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub

     

    (updated)

    But... using VmWare it works!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • griff0417
    griff0417 over 8 years ago in reply to marcocavallini

    I am using vmware and I have had to do this twice. Each time I had no issues. Have you tried following the steps listed here (https://github.com/WaRP7/WaRP7-User-Guide/blob/master/04-Chapter/U-boot.adoc )?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>