STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum STM32F4 Discovery open-source development software
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 7 subscribers
  • Views 2015 views
  • Users 0 members are here
  • gcc
  • stm32-discovery
  • stm32f4dis_software_examples
Related

STM32F4 Discovery open-source development software

e14 Contributor
e14 Contributor over 13 years ago

I don't know if ST are planning to offer support for the open source GNU toolchain for STM32 (as used by Raisonance RIDE7), as they do for other products.  But it can be made to work if you are prepared to hack your own makefiles and linker scripts.  I just got the LCD, Touchscreen and Ethernet examples running, built on my Ubuntu Linux workstation with the arm-none-eabi-gcc toolchain and the openocd debugger (yes, openocd does support SWD, and they are even available on Windows).  I won't say it was instant, it took a week or so of learning curve, but I didn't have to part with any hard-earned cash. I even got the Discovery board set 'free' under the Power Circuit rewards scheme after my last project.

 

Once I'd found all the files and got the typos out of the scripts, it did what it says on the tin ( and no crippleware size limits to worry about).

 

It would be a shame if such a wonderfully low-cost development system lost its potential to lower the entry bar for designers by restricting it to $1000-plus software systems.  Allright for those that already have them: a few years ago I coughed up for a development system for the uPSD series, only to find their FS USB was seriously buggy, and to have ST pull the plug the following year.  So I'm naturally cautious.

 

Me, I'm looking forward to designing some ethernet-enabled instruments.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi Tim,

    I'm interested in what you have done here with the open source toolchain.

    I'll be working on getting it all going with CoIDE and gcc-arm-none-eabi-4_7 (as soon as I get some free time) so any pointers you may have would be very helpfull.

    I've got an application in mind for driving Variable Message Signs and need to get the ethernet interface working along with the GLCD and touch screen.

    Regards,

    Dean.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Well there was a lot of learning curve because I never worte makefiles before, although I've used Linux a lot. 

     

    Obviously you need to collect a list of all the source files you need in your project, you can use $wildcard, but sometimes that gets conflicting alternates etc.  For gcc working bare-metal you need a .specs file that adds libnosys.a to the lib variable so that system calls from within libc (eg _sbrk) get satisfied. 

     

    You need gcc options -mthumb and -mcpu=cortex-M4 (or what have you), plus the options for floating point if you use it, that selects which library gets used.  Beware that the default is ARM assembler, which the cortex-M series can't read, and attempting to interwork will get you a hard-fault exception.  Make sure everything is compiled for thumb code, and that all functions in the map have odd-numbered addresses (bit 0 set identifies thumb code). Add "-D USE_STDPERIPH_DRIVER" unless you are talking direct to registers.

     

    Don't call ld directly, always use the gcc wrapper, it adds the core libraries.  Then you need a startup file and an ld script that martch each other, i.e. the startup uses the same section names that the script defines, and of course you need to put the right memory definitions in the ld script, the examples come with mem.lc and sections.ld separately.  I used the default startup then found the gcc/ride .ld didn't match it, and modified it to fit.   Probably you could use either of the supplied toochain option versions instead with little effort, it should only be a matter of what labels they use for start and end of initialised RAM etc.

     

    Most of the examples don't include a stm32f4xx_conf.h file, which selects which standard preipheral headers to include, but it's pretty harmless to use the default one that includes everything.

     

    For some reason discovery_lcd.c #includes fonts.c rather than fonts.h, which means wildcard compilation gets fonts.o twice, either exlude fonts.o or fix the code.

     

    The debug and lcd-log (printf/stdio output to UART or LCD respectively) functions don't work out of the box, the "PUTCHAR" function they actually need to supply for newlib is "int _write( FILE*fd, char*pc, int len){}", and not either of the options they give (and note that needs to output the whole buffer, not just a char).  Obviously you can only include one or the other of the above in your link.

     

    Debugging: you need to build openocd with config options --enable-hla and --enable-stlink, install it, then plug in the Discovery board and run it  with a config file (./openocd.cfg) as follows:

    interface hla

    hla_layout stlink

    hla_vid_pid 0x0483 0x3748

    stlink_api 2

    source [find target/stm32f4x_stlink.cfg]

     

    If you run it in a terminal it's easier to evict if it crashes, but it can be run as a daemon.

    Download the manual separately from sourceforge, the one in the distro is out of date and doesn't mention SWD.

     

    Then to talk to it run (in a separate termnal)

    arm-none-eabi-gdb -ex 'target remote :3333' filename

    and start typing commands like

    load filename

    monitor reset halt

    cont

    or whatever.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Well there was a lot of learning curve because I never worte makefiles before, although I've used Linux a lot. 

     

    Obviously you need to collect a list of all the source files you need in your project, you can use $wildcard, but sometimes that gets conflicting alternates etc.  For gcc working bare-metal you need a .specs file that adds libnosys.a to the lib variable so that system calls from within libc (eg _sbrk) get satisfied. 

     

    You need gcc options -mthumb and -mcpu=cortex-M4 (or what have you), plus the options for floating point if you use it, that selects which library gets used.  Beware that the default is ARM assembler, which the cortex-M series can't read, and attempting to interwork will get you a hard-fault exception.  Make sure everything is compiled for thumb code, and that all functions in the map have odd-numbered addresses (bit 0 set identifies thumb code). Add "-D USE_STDPERIPH_DRIVER" unless you are talking direct to registers.

     

    Don't call ld directly, always use the gcc wrapper, it adds the core libraries.  Then you need a startup file and an ld script that martch each other, i.e. the startup uses the same section names that the script defines, and of course you need to put the right memory definitions in the ld script, the examples come with mem.lc and sections.ld separately.  I used the default startup then found the gcc/ride .ld didn't match it, and modified it to fit.   Probably you could use either of the supplied toochain option versions instead with little effort, it should only be a matter of what labels they use for start and end of initialised RAM etc.

     

    Most of the examples don't include a stm32f4xx_conf.h file, which selects which standard preipheral headers to include, but it's pretty harmless to use the default one that includes everything.

     

    For some reason discovery_lcd.c #includes fonts.c rather than fonts.h, which means wildcard compilation gets fonts.o twice, either exlude fonts.o or fix the code.

     

    The debug and lcd-log (printf/stdio output to UART or LCD respectively) functions don't work out of the box, the "PUTCHAR" function they actually need to supply for newlib is "int _write( FILE*fd, char*pc, int len){}", and not either of the options they give (and note that needs to output the whole buffer, not just a char).  Obviously you can only include one or the other of the above in your link.

     

    Debugging: you need to build openocd with config options --enable-hla and --enable-stlink, install it, then plug in the Discovery board and run it  with a config file (./openocd.cfg) as follows:

    interface hla

    hla_layout stlink

    hla_vid_pid 0x0483 0x3748

    stlink_api 2

    source [find target/stm32f4x_stlink.cfg]

     

    If you run it in a terminal it's easier to evict if it crashes, but it can be run as a daemon.

    Download the manual separately from sourceforge, the one in the distro is out of date and doesn't mention SWD.

     

    Then to talk to it run (in a separate termnal)

    arm-none-eabi-gdb -ex 'target remote :3333' filename

    and start typing commands like

    load filename

    monitor reset halt

    cont

    or whatever.