STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Problem with "official" LCD software example on STM32F4 Discovery Expansion Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 8 subscribers
  • Views 4717 views
  • Users 0 members are here
  • discovery
  • stm32f4-lcd
  • stm32
  • stm32f4dis-bb
  • stm32f4dis_software_examples
  • stm32f4discovery
Related

Problem with "official" LCD software example on STM32F4 Discovery Expansion Board

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I've just started to use my STM32F4 discovery expansion board (discovery board, base board, LCD and camera) and as a first shot I want to try out the software examples found here:

 

http://www.element14.com/community/docs/DOC-51670/l/stm32f4dis-bb-discover-more-software-examples

 

I've tried to run the LCD example called "LCD_35T" located in the folder "STM32F4xx_LCD_Example" but ran into some problems...

 

I'm using IAR Embedded Workbench for ARM as my IDE and have performed the following steps:

 

  • Open the project file located in "LCD_35T/EWARM" folder
  • Rebuild all --> Results in a successful build without errors/warnings
  • Download and debug --> Code is flashed and debugger started (using ST-LINK)
  • Running program (Go) --> Expecting LCD to show color bars according to the example but the screen is just white...


Does anyone have an idea what I'm doing wrong?

 

Thanks in advance for all response!

  • Sign in to reply
  • Cancel

Top Replies

  • Kilohercas
    Kilohercas over 13 years ago +1
    do you have LCD with same controller/pinout ? Right code with wrong init ( set registers for refresh rate, color type, bus type and so on) will produce white screen Check if RESET is high. Disable opt…
  • Kilohercas
    Kilohercas over 13 years ago in reply to e14 Contributor +1
    IF LCD reset Line is LOW, you never get LCD working. some one mentioned bad contacts, also make RESET High after power up at if not by default code, than yourself. #define LCD_RST_PIN (GPIO_Pin_3) #define…
  • ChuckMcM
    ChuckMcM over 13 years ago +1
    So I too was having issues with the code provided by Embest so I wrote some of my own. You can pull a copy from Github here: https://github.com/ChuckM/bb-lcd This puts up a simple display on the LCD with…
Parents
  • Kilohercas
    0 Kilohercas over 13 years ago

    do you have LCD with same controller/pinout ?
    Right code with wrong init ( set registers for refresh rate, color type, bus type and so on) will produce white screen

    Check if RESET is high.
    Disable optimization

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Kilohercas
    0 Kilohercas over 13 years ago

    do you have LCD with same controller/pinout ?
    Right code with wrong init ( set registers for refresh rate, color type, bus type and so on) will produce white screen

    Check if RESET is high.
    Disable optimization

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Kilohercas

    Hi,

     

    First of all, thanks for your reply, Linas!

     

    I have the STM32F4DIS-LCD which I believe is the one considered for this project so i don't think it should be any problems with the controller/pinout.

    I checked that RESET is not high and turned off all optimization but I still have the same behavior from the LCD.

     

    Let me know if you have any additional thoughts to this problem.

     

    Thanks again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to e14 Contributor

    IF LCD reset Line is LOW, you never get LCD working. some one mentioned bad contacts, also make RESET High after power up at if not by default code, than yourself.

    #define LCD_RST_PIN                     (GPIO_Pin_3)

    #define LCD_RST_PORT                 (GPIOD)


    (and you can't use that for your one usage, just for lcd )

     

    Set this pin yourself high before init, and delete same code from lcd init, i don't know why it's not High, it must be. , where is no point to look any further if you have lcd in reset at all time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Kilohercas

    Hi again,

     

    Never mind, I also had bad contact! Reconnected everything after you mentioned that, and now it all works just fine image

     

    Sorry for taking your time with such a silly problem, but I really appreciate your help!