STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Learning the STM32F4Discovery
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 3 answers
  • Subscribers 7 subscribers
  • Views 2462 views
  • Users 0 members are here
Related

Learning the STM32F4Discovery

philip-1992
philip-1992 over 13 years ago

Hi everyone,

 

I have an upcoming project for my finals as electrical engineer and the project consists of a design of a touch screen interface for micro controller. As I am not that familiar programming I bought the STM discovery, extention and LCD boards in order to get more familiar with the programming. I am using IAR embedded software and downloaded the examples available on this forum. I started with an example that regards the LCD the project's name is LCD_35T. Currently I am struggling understanding a few things mainly the GPIO configuration found under the stm32f4_discovery_lcd.c. I have downloaded the manual of the STM board and read the sections of GPIO (page 185-203 from the manual). However I cannot understand what each instruction is doing to each pin. Is there an explaination like a tutorial of this example?

 

Thank you in advance.

  • Sign in to reply
  • Cancel
  • mconners
    0 mconners over 13 years ago

    This is one of my favorite resources. There is quite a bit of good info in here. http://www.cs.indiana.edu/~geobrown/book.pdf

     

    If you dowload the software he mentions all of the solution code is in one of the lib directories. Good luck.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to mconners

    Wow just the resource I needed. At a quick glance it looks much more user friendly than the manual especially due to the fact that there are exercises in it. Thank you alot very much appreciated image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 13 years ago in reply to philip-1992

    Not a problem.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 13 years ago in reply to mconners

    While the document is actually on the STM32F1 series you should find enough similarities to answer questions.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago

    As I am debugging the program mentioned earlier I noticed a coloured line on the screen (as shown on the attatched photo). I made a break point at: void LCD_DisplayOff (void) {} just to show it to you clearer. Is this some sort of a damage that occured to the screen??? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 13 years ago in reply to philip-1992

    It looks like it could be some sort of defect, but it is hard to tell without having hands on :-)

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to mconners

    Atleast it is not permanent only at certain times. So I hope it won't come as a problem at a later stage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to mconners

    I was wondering about the book you gave me last time, as I read the required hardware chapter I found out that the boards are not the same (he uses STM32 VL and I am using the STM32f4Discovery) and also there are other hardware required. Are all those necessary? Or I can manage to do some examples from the book without the mentioned hardware?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 13 years ago in reply to philip-1992

    Hey Phillip,

     

    Yeah, I had mentioned the processors were different in a follow up post. The code won't change much between the two boards, but you will probably need a different linker script. Google around for that, Folks have made them an posted them to various forums. No you don't have to do all the exercises in the book, pick one or two you are interested in and complete those. I don't know if there is an electronics store (like a radio shack) that may have some of that hardware, but if nothing else, just simulate output by making leds blink.

     

    Also, remember, Google (or bing, or whatever) is your friend, search around for examples for the STM34F4Discovery, I'm sure you'll find more.

     

    Either that or buy the STM32VLDISCOVERY, it's like $12, and buy the hardware in the book, $40-$60, and do all the exercises, you'll learn alot. Everytime you touch either of those boards its an education.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to mconners

    Hi there I found a program which basicly an analogue input is given to PC0 via a potentiometer and through a variable named "ConvertedValue" the user can monitor the actual value of resistance applied by the pot. owever as I tried to Download the code to the board I am getting this error: Error[Li005]: no definition for "SystemInit" [referenced from C:\Users\Philip\Desktop\Potentiometer Read\Project\LCD_35T\EWARM\Discover-More\Obj\startup_stm32f4xx.o]. I checked the whole code and that function isn't referenced anywhere. So my guess is that is has to do with some sort of start up file.. Any guess on how to solve this problem?? The code is below Thank you in advance.

     

    #include "stm32f4_discovery.h"

    #include "stm32f4_discovery_lcd.h"

    #include "stm32f4xx_adc.h"

    #include "stm32f4xx_gpio.h"

    #include "stm32f4xx_rcc.h"

     

     

    int ConvertedValue = 0; //Converted value readed from ADC

     

     

    void adc_configure(){

    ADC_InitTypeDef ADC_init_structure; //Structure for adc confguration

    GPIO_InitTypeDef GPIO_initStructre; //Structure for analog input pin

    //Clock configuration

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1,ENABLE);//The ADC1 is connected the APB2 peripheral bus thus we will use its clock source

    RCC_AHB1PeriphClockCmd(RCC_AHB1ENR_GPIOCEN,ENABLE);//Clock for the ADC port!! Do not forget about this one image

    //Analog pin configuration

    GPIO_initStructre.GPIO_Pin = GPIO_Pin_0;//The channel 10 is connected to PC0

    GPIO_initStructre.GPIO_Mode = GPIO_Mode_AN; //The PC0 pin is configured in analog mode

    GPIO_initStructre.GPIO_PuPd = GPIO_PuPd_NOPULL; //We don't need any pull up or pull down

    GPIO_Init(GPIOC,&GPIO_initStructre);//Affecting the port with the initialization structure configuration

    //ADC structure configuration

    ADC_DeInit();

    ADC_init_structure.ADC_DataAlign = ADC_DataAlign_Right;//data converted will be shifted to right

    ADC_init_structure.ADC_Resolution = ADC_Resolution_12b;//Input voltage is converted into a 12bit number giving a maximum value of 4096

    ADC_init_structure.ADC_ContinuousConvMode = ENABLE; //the conversion is continuous, the input data is converted more than once

    ADC_init_structure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;// conversion is synchronous with TIM1 and CC1 (actually I'm not sure about this one :/)

    ADC_init_structure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;//no trigger for conversion

    ADC_init_structure.ADC_NbrOfConversion = 1;//I think this one is clear image

    ADC_init_structure.ADC_ScanConvMode = DISABLE;//The scan is configured in one channel

    ADC_Init(ADC1,&ADC_init_structure);//Initialize ADC with the previous configuration

    //Enable ADC conversion

    ADC_Cmd(ADC1,ENABLE);

    //Select the channel to be read from

    ADC_RegularChannelConfig(ADC1,ADC_Channel_10,1,ADC_SampleTime_144Cycles);

    }

    int adc_convert(){

    ADC_SoftwareStartConv(ADC1);//Start the conversion

    while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC));//Processing the conversion

    return ADC_GetConversionValue(ADC1); //Return the converted data

    }

    int main(void){

    adc_configure();//Start configuration

        while(1){//loop while the board is working

         ConvertedValue = adc_convert();//Read the ADC converted value

        }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>