STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Stm32f4 loading image
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Subscribers 8 subscribers
  • Views 4245 views
  • Users 0 members are here
Related

Stm32f4 loading image

philip-1992
philip-1992 over 13 years ago

Hi all,

 

I am still on the experimenting phase of the stm32f4 Discovery. I am trying to load an image on the touch screen (DM-LCD35RT) but I cannot find any examples in order to guide me. Is there anyone that has an available example in which I can understand the process and thus write my own program? Any help would be greatly appreciated. Thank you

  • Sign in to reply
  • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to philip-1992

    void LCD_BMP(uint8_t *bitmap)

    {

      uint32_t size = 320 * 240;

      uint32_t *bitmap_ptr = (u16 *)bitmap;

      LCD_SetCursor(0x00, 0x00);

      LCD_WriteRAM_Prepare(); /* Prepare to write GRAM */

     

      for(uint32_t index=0;index<(size);index++)

      {

        LCD_Data = *bitmap_ptr++;

      }

     

    }

     

    just past this code to your project (in the bottom of library of lcd), and use 320x240 picture (convert without header)

    LCD_BMP((uint8_t*) ImageBuffer);

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to Kilohercas

    I have tried the last solution that you gave me but now I have to deal with the size limit :/ I will get back to you as soon as I discover on how to save the image from SD card and load it from there

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to philip-1992

    I am strugling with the same problems as you are. Probably you can save also the picture in FLASH, but you have to "tell" the compiler not to copy it to RAM. Unfortuantely I have not figured it yet how to do it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago

    All you have to do, is to write windowfunction for lcd, and you can edit LCD_CLear function to paint picture. I could do that, but i don't have right LCD

    void LCD_SetDisplayWindow(uint8_t Xpos, uint16_t Ypos, uint8_t Height, uint16_t Width)

    {

      if(Xpos >= Height)

      {

        LCD_WriteReg(0x0044, (Xpos - Height +1));

      }

      else

      {

        LCD_WriteReg(0x0044, 0x0000);

      }

      if(Ypos >= Width)

      {

        LCD_WriteReg(0x0045, (Ypos - Width +1));

      } 

      else

      {

        LCD_WriteReg(0x0045, 0x0000);

      }

      LCD_WriteReg(0x0046, Ypos);

      LCD_SetCursor(Xpos, Ypos);

     

    }

     

    And with internal flash, it is possibe to save up to 7 pictures at 320x240 resolution

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to Kilohercas

    Yes but I still have the 32K size limit of IAR that is the problem. Hopefully by storing the pictures on the SD card it will not exceed the 32K

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to philip-1992

    no, because you could use 50x50 pictures, not 320x240.
    so you can still develope code under size limit, or go for another trial of compiler, but time, not size limited

     

    Ok, writed simple program, to paint using paint pixel function (you must use paint pixel function with x, y, and colour parameters to make it work, i don't know ST library function name for that)

     

     

    void Slow_paint(int x_start,int y_start,int size_x, int size_y,uint8_t *bitmap)

    {

      uint16_t *bitmap_ptr = (uint16_t *)bitmap;

      int i=0,j=0;

      while(i<size_y)

      {

        while(j<size_x)

        {

         Pixel(j+x_start,i+y_start,*bitmap_ptr++);

          j++;

        }

        i++;

        j=0;

      }

    }

     

    call it like this:
    Slow_paint(10,10,60,60,(u8*)ImageBuffer);

    10 is offset, and 60x60 is my picture size, change to mach your own

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 13 years ago

    Hi. I too am struggling with this. I (mistakingly) though that buying the official kits (Baseboard + Discovery-LCD) would improve the interoperability.

     

    So far I have a distorted image being displayed through use of the 'LCD_BMP' function provided above, though the official 'LCD_WriteBMP' results in no image at all. Does anybody have any sample code that I can work through to solve this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    https://www.youtube.com/watch?v=tDG1unD_GPw

    Using BMPDATA (BMP DATA - Download - 4shared).

    For LCD, ID 8989;

    ...

    #define LOWBYTE(v)   ((unsigned char) (v))

    #define HIGHBYTE(v)  ((unsigned char) (((unsigned int) (v)) >> 8))

    ...

    void Region_Set(u16 H_E_S ,u16 y,u16 y_end)

    {

    LCD_WriteReg(R44,H_E_S); //HORIZONTAL [END] [START]     (R44 = 0x44h)

    LCD_WriteReg(R45,y);     //VERTICAL START                         (R45 = 0x45h)

    LCD_WriteReg(R46,y_end); //VERTICAL END;                        (R45 = 0x46h)

    ili9320_SetCursor(LOWBYTE(H_E_S),y); //

    LCD_WriteRAM_Prepare();

    ClrCs;

    SetRs;

    }

    Region_Set(0xEF00,0,319);     //320x240

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<