STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Discover Wi-Fi Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 4 subscribers
  • Views 356 views
  • Users 0 members are here
  • discover_wi-fi_board
Related

Discover Wi-Fi Board

e14 Contributor
e14 Contributor over 13 years ago

Hi,

I Have just bought the Discover Wi-Fi board and also downloaded the software. In the first instance I wanted to port the stm32f40x software to my Mbed. I have completed this task, but now have a number of questions.

 

I noticed while porting the software that there is a copyright notice /******************** (C) COPYRIGHT 2009 Embest Info&Tech Co.,LTD. ************.

 

(1). Will the Embest software ever be released as OpenSource?

(2). Is my port an infringement of the Embest copyright?

(3). Can I publicly release my Mbed port of the Embest copyrighted software?

 

While running the software and joining a network I cannot get access to the internet, I assumed that this is due to using a different subnet. I also found that when accessing sn8200.com (The sn8200 sever.) the pages were different to the ones shown in Discover Wi_Fi UserManual_V4.pdf.

 

(4). Should I be able to access the internet using the sn8200 as an AP?

(5). Should I be seeing the same content as shown in Discover Wi_Fi UserManual_V4.pdf?

(6). Is the sn8200 M3 firmware Embest, MuRata or Broadcom copyright?

(7). Will there be a release of the source code for the M3.

 

Are the software bound to NDA's so that nobody from the open source development community can use it?

 

Regards,

 

Dave.