STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum STM32F4DIS-WIFI - no output from the wifi module
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Subscribers 10 subscribers
  • Views 4189 views
  • Users 0 members are here
  • stm32f4dis_wifi
  • stm32f4discovery
Related

STM32F4DIS-WIFI - no output from the wifi module

roli
roli over 12 years ago

I have just bought the STM32F4DIS-WIFI today and I have some problems getting it to work on my STM32F4 discovery board. The included example is for the MDK-ARM only and I had some trouble building parts of it (mainly the sn8200_core and sn8200_api files) with IAR. I fixed the problem by commenting out the #include <rtl.h> (I believe it's part of the MDK-ARM) and replacing it with this code:

 

#define INADDR_ANY ((unsigned long int) 0x00000000)
#define INADDR_NONE ((unsigned long int) 0xffffffff)
#define    htonl(l) lswap(l)
#define    htons(s) ((unsigned int)(((unsigned int)(s) >> 8) | ((unsigned int)(s) << 8)))
#define    ntohl(l) lswap(l)
#define    ntohs(s) htons(s)

 

I got the code to compile by doing this but it doesn't appear to be working. This is my main function:

void main() {
  //wifi init
  SN8200_API_Init(921600);
  WifiOn(seqNo++);
  GetStatus(seqNo++);
  WifiScan(seqNo++);
  WifiDisconn(seqNo++);
  WifiJoin(seqNo++);
  SnicInit(seqNo++);
  SnicIPConfig(seqNo++);

  while(1) {}
}

 

I didn't use any DBGBU and other functions (and I don't have anything connected to the USART3). IAR provides printf/scanf functions that work with the included debug console so I didn't see any need for that part of the code.

 

The problem that I am having is this: I get no input from the module. For instance the GetStatus function - I get the -GetStatus but not the actual status. The same goes for wifi scan. I never get the actual list of available SSIDs. I can actually disconnect and join the network though. If I enter my SSID, security mode and password then the module connects to the wifi network as expected. So apparently it is geting the data from the board. But I am not sure why I am not getting anything from the module.

  • Sign in to reply
  • Cancel

Top Replies

  • roli
    roli over 12 years ago in reply to roli +1 verified
    Got it. F*** IAR. It was their printf redirect that was making things not work as they should. I redirected that stream to a simple character array instead and what do you know... everything showed up…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, I'm also developing a project using this kind of module together with my F4.

     

    The problem I'm having is that the POST Req, and Get req isn't working. Any clues so as to why this is happening? I bought mine last year, so it came with the "Discover-wifi v2.rar".

     

    Do you have a user's manual for this? I mean like I've been trying the WIFI capabilities of this module together with my webserver in my PC but it doesn't seem to work. I even tried to just monitor port 80 using socket listener but to no avail, the POST or GET req can't be received. :<

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, I'm also developing a project using this kind of module together with my F4.

     

    The problem I'm having is that the POST Req, and Get req isn't working. Any clues so as to why this is happening? I bought mine last year, so it came with the "Discover-wifi v2.rar".

     

    Do you have a user's manual for this? I mean like I've been trying the WIFI capabilities of this module together with my webserver in my PC but it doesn't seem to work. I even tried to just monitor port 80 using socket listener but to no avail, the POST or GET req can't be received. :<