STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum STM32F4DIS-WIFI - no output from the wifi module
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Subscribers 10 subscribers
  • Views 4189 views
  • Users 0 members are here
  • stm32f4dis_wifi
  • stm32f4discovery
Related

STM32F4DIS-WIFI - no output from the wifi module

roli
roli over 12 years ago

I have just bought the STM32F4DIS-WIFI today and I have some problems getting it to work on my STM32F4 discovery board. The included example is for the MDK-ARM only and I had some trouble building parts of it (mainly the sn8200_core and sn8200_api files) with IAR. I fixed the problem by commenting out the #include <rtl.h> (I believe it's part of the MDK-ARM) and replacing it with this code:

 

#define INADDR_ANY ((unsigned long int) 0x00000000)
#define INADDR_NONE ((unsigned long int) 0xffffffff)
#define    htonl(l) lswap(l)
#define    htons(s) ((unsigned int)(((unsigned int)(s) >> 8) | ((unsigned int)(s) << 8)))
#define    ntohl(l) lswap(l)
#define    ntohs(s) htons(s)

 

I got the code to compile by doing this but it doesn't appear to be working. This is my main function:

void main() {
  //wifi init
  SN8200_API_Init(921600);
  WifiOn(seqNo++);
  GetStatus(seqNo++);
  WifiScan(seqNo++);
  WifiDisconn(seqNo++);
  WifiJoin(seqNo++);
  SnicInit(seqNo++);
  SnicIPConfig(seqNo++);

  while(1) {}
}

 

I didn't use any DBGBU and other functions (and I don't have anything connected to the USART3). IAR provides printf/scanf functions that work with the included debug console so I didn't see any need for that part of the code.

 

The problem that I am having is this: I get no input from the module. For instance the GetStatus function - I get the -GetStatus but not the actual status. The same goes for wifi scan. I never get the actual list of available SSIDs. I can actually disconnect and join the network though. If I enter my SSID, security mode and password then the module connects to the wifi network as expected. So apparently it is geting the data from the board. But I am not sure why I am not getting anything from the module.

  • Sign in to reply
  • Cancel

Top Replies

  • roli
    roli over 12 years ago in reply to roli +1 verified
    Got it. F*** IAR. It was their printf redirect that was making things not work as they should. I redirected that stream to a simple character array instead and what do you know... everything showed up…
Parents
  • dturcu91
    0 dturcu91 over 12 years ago

    Hello

    Can someone help me with an working project for IAR with spi comunication?
    I can not make it to work..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dturcu91

    The project was written in KEIL. Download an evaluation version of KEIL, you'll need the RTX libraries, so copy the the RV31 directory out of the install directory from KEIL and put it into your IAR project directory. Next you need to fix the rtl.h header file so IAR can use it.

     

    All the instances of __rev should be __REV for IAR.

    You'll also have to change the swi notation.

     

    So something like this

    #pragma swi_number=0x02

    extern int       _free_box (void *box_mem, void *box) __swi (2);

    #else

     

    should be like this for IAR

    #pragma swi_number=0x02

    __swi extern int       _free_box (void *box_mem, void *box);

    #else

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dturcu91

    The project was written in KEIL. Download an evaluation version of KEIL, you'll need the RTX libraries, so copy the the RV31 directory out of the install directory from KEIL and put it into your IAR project directory. Next you need to fix the rtl.h header file so IAR can use it.

     

    All the instances of __rev should be __REV for IAR.

    You'll also have to change the swi notation.

     

    So something like this

    #pragma swi_number=0x02

    extern int       _free_box (void *box_mem, void *box) __swi (2);

    #else

     

    should be like this for IAR

    #pragma swi_number=0x02

    __swi extern int       _free_box (void *box_mem, void *box);

    #else

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • hetcnc
    0 hetcnc over 11 years ago in reply to e14 Contributor

    What you need is: "MDK Cortex-M Legacy Device Support 5.12". It installs RV31 directory with the "rtl.h" file.