STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum STM32F4DIS-WIFI (SN8200) Firmware Updates?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 7 subscribers
  • Views 1726 views
  • Users 0 members are here
  • stm32f4dis-wifi
  • firmware
  • wifi
  • sn8200
  • smt32f4discovery
Related

STM32F4DIS-WIFI (SN8200) Firmware Updates?

mroussin
mroussin over 12 years ago

I have been working with the standard firmware package that comes with the STM32F4DIS-WIFI board.  Right now I am just using this through my STM32F4DISCOVERY board through the UART1.  I have had success with the sample code provided through the download package.  Now I am looking at making updates and trying some of the other firmware packages available (EWW) eventually leading me to create some custom pages for my application.  But I believe you need to have a JTAG to upload new firmware to the SN8200.

 

1) Am I understanding this correctly that you need a JTAG interface to upload new firmware to the SN8200? 

2) Is there any other interface that can be used to update the firmware?

 

Any help with this is appreciated.


Thanks,


Mike 

  • Sign in to reply
  • Cancel

Top Replies

  • mroussin
    mroussin over 12 years ago +1 verified
    I actually found my answer, which simple enough was in the manual for the WIFI board. You can use the STLINK SWD on the discovery board to update the firmware. See the attached picture for connections…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    Could you send me the image please ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    Could you send me the image please ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mroussin
    0 mroussin over 12 years ago in reply to e14 Contributor

    Omar,


    I will try to get this uploaded this weekend.


    Thanks,

     

    Mike