STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Discover WiFi - DNS Resolution
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 6 subscribers
  • Views 1040 views
  • Users 0 members are here
Related

Discover WiFi - DNS Resolution

andyw999
andyw999 over 12 years ago

In sn8200_core.h there is SNIC_RESOLVE_NAME_REQ which is referred to in page 72 of the SN8200 SNIC Serial Interface Specification.pdf

 

(Optional) SNIC_RESOLVE_NAME_REQ to resolve a host name to IP address

 

If you try to do a query with it then handleRxSNIC get returned 0x8A which is not a member of SNIC_subcmd_id_e in sn8200_core.h, in fact it has been deliberately left out :-

 

    SNIC_SEND_RSP = 0x82,

    SNIC_CLOSE_SOCKET_RSP,

    SNIC_GET_DHCP_INFO_RSP = 0x89,

    SNIC_IP_CONFIG_RSP = 0x8B,

 

Does anybody know how to make this work and if the SN8200 UART firmware even supports it?

 

I have asked Murata but do not know if I will get a response...

 

Edit - just had a response from Murata and the version 2.3 of the SNIC serial interface specification.pdf is a lot more up to date.

 

Thanks

 

Andy.

  • Sign in to reply
  • Cancel
  • andyw999
    0 andyw999 over 12 years ago

    Looking at the SNIC v2.3...

     

    In sn8200_core.h add in SNIC_subcmd_id_e :-

     

    SNIC_GET_DNS_INFO_RSP = 0x8A,

     

    In sn8200_api.c handleRxSNIC add :-

     

    case SNIC_GET_DNS_INFO_RSP:

    {

         if (SNIC_SUCCESS == buf[2])

         {

              printf("IP from DNS %i.%i.%i.%i \n\r", buf[3],buf[4],buf[5],buf[6]);

         }

         else

         {

              printf("IP not availabler\n\r");

         }

    }

    break;

     

    To get DNS info :-

    #define HOST "somesite.com"

     

    int getdns(int8u seq)

    {

        int8u buf[50];

        int16u len = sizeof(HOST);

        int16u mybufsize;

     

        buf[0] = SNIC_RESOLVE_NAME_REQ;

        buf[1] = seq;

        buf[2] = 0x00;

        buf[3] = len;

        memcpy(buf+4, HOST, len);

     

        serial_transmit(CMD_ID_SNIC, buf, 4+len, ACK_NOT_REQUIRED);

     

        return 0;

    }

     

    And it works!

     

    Andy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to andyw999

    Hi Andy,

     

    I found SN8200 SNIC Serial Interface Specification.pdf

    Version: 1.7

    October 17, 2012

     

    Where do I get version 2.3?

     

    Thank you!

    Werner

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andyw999
    0 andyw999 over 12 years ago in reply to e14 Contributor

    Hi Werner

     

    I got it from Murata UK support.

     

    If I knew where to upload it I would!

     

    I have, I think, uploaded it to you..

     

    Andy.