STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Discover Wi-Fi Module SPI Communication
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 58 replies
  • Subscribers 7 subscribers
  • Views 10185 views
  • Users 0 members are here
  • wifi
  • stm32f4
  • discovery
  • spi
  • discover
Related

Discover Wi-Fi Module SPI Communication

e14 Contributor
e14 Contributor over 11 years ago

I've been messing around for days and have been unable to get the SPI communication with the Wi-Fi module to work, it would never respond at all. I couldn't get the demo UART code to respond either, but I need SPI for the increased bandwidth anyways. Am I doing something wrong, like missing a setup step or something? I'm not even sure if I connected the correct pins on the board, as there are 2 sets of SPI pins (SPI and SPI3), and I'm not 100% sure of which pin is the "ALRT" pin. I couldn't even get that interrupt to fire, despite numerous attempts to send data to the module. Does anyone have some working SPI code and wiring? I'm kind of at a loss here. I've put the code is this gist and this gist (too many lines to paste here), it looks rather shoddy as I was trying various things to get the module to do anything at all. I tried both DMAs and straight up interrupts, though I'd prefer to use DMAs to save CPU cycles.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    Before you spend your money why not at least try to code it so that your waveforms look exactly like those on the data sheet ? And try clocking data out only when it's ready. These things might not make…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett +1
    Hi Michael, Thank you for your insight into SPI communication. I implemented that, driving a GPIO but with S/W and asserting prior to read/write and de-asserting when complete and it has improved communication…
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    I've configured more SPI links than I care to remember and I would never attempt it without  a scope. About half the time it just works and the other times you forget a clock enable or leave a pin in the wrong mode or whatever.

     

    Which development environment are you using ?

     

    I use Keil which allows you to look at the registers of all the peripherals to make sure that they are all set up right.

     

    If you are using Keil I can give you some detailed suggestions - if not you may get better help from someone familiar with the tools you are using.

     

    If all else fails (and it does quite often) - get the link working using code to bit bang the spi link on the uP side ( this is much easier to debug with primitive tools because you can single step everything and use a DMM or even an LED and a  resistor as your logic analyser).

    Once it bit bangs then try using the SPI peripheral on the uP

    And only once that works should you attempt using DMA.

     

    I very rarely find the problem by looking at the code - you need to step though it and see what actually happens on the pins.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Well I did fix one problem, but it still isn't working. I had the MISO pin set to no pull instead of pull down which was causing it to be floating when low, resulting in erratic behavior (random bits when even so much as touching the wire). I'm using Eclipse as my IDE and OpenOCD to communicate with the on-board ST-Link/V2. I don't see any reason why the SPI wouldn't be clocking out data, as I was able to get I2S working on the external DAC. I tried connecting the other set of SPI pins, and it seems that the MISO on that one is high, but it never goes low when I clock data in/out. All I'm receiving is logical ones. I connected the SPI outputs on the STM32F4 to an input setup with an interrupt to toggle an LED, and that seems to be working fine. I don't think bit-banging the Wi-Fi module will make a difference if the SPI output is working as it should. As I said I couldn't get the UART interface to work either. I'm starting to wonder if the module is somehow damaged. Scratch that, the UART wouldn't work because I messed up a clock enable call.

     

    EDIT: I'm starting to wonder if the SPI interface isn't enabled and I need to upload different firmware. I've been trying to do that but can't find the "boot" pin on the headers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    No matter what I try I can't seem to receive anything, unless I set the SPI speed fast enough, then it starts receiving garbage. I've uploaded the correct firmware to the SN8200. Pins 20, 18, 16 and 14 on J6 are the SPI pins, right? I tried 2, 4, 6 and 8 originally but that did nothing at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I'm using J6 12, 14, 16, 18 and 20 too. I thought I was having difficulty with NSS (20) so I just tied it to ground. On SPI4 (STM32F429I-Discovery) any baud rate prescaler from 4 through 128 works (don't recall if I tried 256.)

     

    At times the Murata stops sending replies. Some times that is resolved using the reset pin/button and at other times it may require a power cycle. It also doesn't like to be hammered by requests. I had to add a 50ms interval between exchanges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Well I think I'm getting actual responses now, but I can't verify the data, nor can I seem to clock the response out of the SPI. I have a circular DMA running with an empty buffer to keep the master clock going, but it doesn't seem to be doing anything. Can you check the code? I honestly don't think I know what I'm doing, pretty new to this thing...

     

    C file: https://gist.github.com/b987bbc998b0d27292af

    Header file: https://gist.github.com/579f9b3b8b42fb5adc7d

     

    There's a lot of commented out stuff, from various attempts to get the thing to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I'll try to take a look at it tonight. It is unlikely I'll see anything as I started working with example code which I modified to suit my needs. ASll of the SPI and other setup was already in place. (In other words, probably know less about it than you.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Can I see your current code? I could probably figure out what I'm doing wrong by looking at it myself. I can't find the example code you're speaking of.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Sorry - no can do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Why not exactly? And can you point me to where you got the example code you used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I started with C:\STM32Cube_FW_F4_V1.4.0\Projects\STM32F429I-Discovery\Examples\SPI\SPI_FullDuplex_ComDMA, part of the package downloaded from STM32CubeF4 Embedded software for STM32 F4 series (HAL low level drivers, USB, TCP/IP, File system, RTOS, Graphic - comi….

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    So it seems that by completing disabling the NSS pin on the STM32F4, it is actually working now. Next step is to ensure the data is correct. I'm also wondering if your "stops sending replies at times" has something to do with an oversight in sequence number. You said it won't reply to a previously used sequence number right? Maybe it overflows back to 0 and no longer works, effectively limiting you to 256 messages to the module before needing a reset. Only a theory though, haven't tested it yet.

     

    EDIT: Just tested it, it continues to reply even after the sequence number wraps around. Strange why it sometimes stops replying for no reason.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hmm... so I've run into another issue. The module is not replying reliably if I set the baudrate prescaler lower than 64. Not a grounding issue as I connected the grounds on the 2 boards. Shouldn't be a floating voltage issue either as I have the SPI pins in push/pull and pulldown mode. What else could it be?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hmm... so I've run into another issue. The module is not replying reliably if I set the baudrate prescaler lower than 64. Not a grounding issue as I connected the grounds on the 2 boards. Shouldn't be a floating voltage issue either as I have the SPI pins in push/pull and pulldown mode. What else could it be?