STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Discover Wi-Fi Module SPI Communication
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 58 replies
  • Subscribers 7 subscribers
  • Views 10169 views
  • Users 0 members are here
  • wifi
  • stm32f4
  • discovery
  • spi
  • discover
Related

Discover Wi-Fi Module SPI Communication

e14 Contributor
e14 Contributor over 11 years ago

I've been messing around for days and have been unable to get the SPI communication with the Wi-Fi module to work, it would never respond at all. I couldn't get the demo UART code to respond either, but I need SPI for the increased bandwidth anyways. Am I doing something wrong, like missing a setup step or something? I'm not even sure if I connected the correct pins on the board, as there are 2 sets of SPI pins (SPI and SPI3), and I'm not 100% sure of which pin is the "ALRT" pin. I couldn't even get that interrupt to fire, despite numerous attempts to send data to the module. Does anyone have some working SPI code and wiring? I'm kind of at a loss here. I've put the code is this gist and this gist (too many lines to paste here), it looks rather shoddy as I was trying various things to get the module to do anything at all. I tried both DMAs and straight up interrupts, though I'd prefer to use DMAs to save CPU cycles.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    Before you spend your money why not at least try to code it so that your waveforms look exactly like those on the data sheet ? And try clocking data out only when it's ready. These things might not make…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett +1
    Hi Michael, Thank you for your insight into SPI communication. I implemented that, driving a GPIO but with S/W and asserting prior to read/write and de-asserting when complete and it has improved communication…
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    I've configured more SPI links than I care to remember and I would never attempt it without  a scope. About half the time it just works and the other times you forget a clock enable or leave a pin in the wrong mode or whatever.

     

    Which development environment are you using ?

     

    I use Keil which allows you to look at the registers of all the peripherals to make sure that they are all set up right.

     

    If you are using Keil I can give you some detailed suggestions - if not you may get better help from someone familiar with the tools you are using.

     

    If all else fails (and it does quite often) - get the link working using code to bit bang the spi link on the uP side ( this is much easier to debug with primitive tools because you can single step everything and use a DMM or even an LED and a  resistor as your logic analyser).

    Once it bit bangs then try using the SPI peripheral on the uP

    And only once that works should you attempt using DMA.

     

    I very rarely find the problem by looking at the code - you need to step though it and see what actually happens on the pins.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Well I did fix one problem, but it still isn't working. I had the MISO pin set to no pull instead of pull down which was causing it to be floating when low, resulting in erratic behavior (random bits when even so much as touching the wire). I'm using Eclipse as my IDE and OpenOCD to communicate with the on-board ST-Link/V2. I don't see any reason why the SPI wouldn't be clocking out data, as I was able to get I2S working on the external DAC. I tried connecting the other set of SPI pins, and it seems that the MISO on that one is high, but it never goes low when I clock data in/out. All I'm receiving is logical ones. I connected the SPI outputs on the STM32F4 to an input setup with an interrupt to toggle an LED, and that seems to be working fine. I don't think bit-banging the Wi-Fi module will make a difference if the SPI output is working as it should. As I said I couldn't get the UART interface to work either. I'm starting to wonder if the module is somehow damaged. Scratch that, the UART wouldn't work because I messed up a clock enable call.

     

    EDIT: I'm starting to wonder if the SPI interface isn't enabled and I need to upload different firmware. I've been trying to do that but can't find the "boot" pin on the headers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Does your debug system allow you to see the STM32Fxxxx peripheral registers in some sort of organised way ?

     

    If not I suggest you use a different development system : the one I know is the Keil MDK (but there are many others) which is completely free to use for projects with up to 32k of code - it does support peripheral debugging.

     

    The point about using bit banging to debug is that you can trace and single step everything - this just isn't possible any other way (although a good logic analyser comes  close.)

     

    Is MISO supposed to be driven by the wIfI module ? From your description of things it looks as if it is not being driven at all. Are you doing all the things to the wifi to enable its SPI that you should ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    I'm currently trying to figure out how to configure the Wi-Fi module correctly for SPI, and yes MISO should be driven by it because it's the slave. I need to put the device in firmware upload mode by driving the "boot" pin high, but I cannot find said pin. Would you happen to have any idea where it is? I'll have to get back to you on the peripheral registers thing, I honestly haven't checked. But I don't think it's a configuration issue as I can get other peripherals to work just fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    I'm currently trying to figure out how to configure the Wi-Fi module correctly for SPI, and yes MISO should be driven by it because it's the slave. I need to put the device in firmware upload mode by driving the "boot" pin high, but I cannot find said pin. Would you happen to have any idea where it is? I'll have to get back to you on the peripheral registers thing, I honestly haven't checked. But I don't think it's a configuration issue as I can get other peripherals to work just fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    The boot pin on the Murata WiFi chip is referred to on the Murata docs but you can't tell if it is accessible on the Discover board because there is no schematic in the board User Manual - I suggest you moan, very loudly, to Farnell about this  - this kind of board should always be fully documented.

    It does (sort of) tell you how to do a firmware upgrade without using the boot pin on page 46 of the board user manual.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Yeah I just found that page and did the firmware upgrade using the SWD on the STM32F4 board. Going to try using the SPI now, will report back.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    So I've been mucking around with it for a bit, and I'm consistently receiving weird round values like 0xFF, 0x7F and 0x3F, but not any start-of-message (0x02) or end-of-message (0x04) bytes. It's clearly not just garbage because it's consistent every time I reset the microcontroller. The module also seems to realize it's receiving data because the ALRT pin goes high. However, I changed the baudrate prescaler to 256 and all of this behavior went away, so I'm honestly not sure. I might try the bit-banging, though that's going to take some time to mess around with. I really need to get a logic analyzer and oscilloscope, but can't afford either right now. That would really help with debugging this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    I connected MOSI to MISO on the STM32F4 so it's looping back to itself, and it's definitely sending the right data, so the Wi-Fi module just doesn't seem to be communicating over SPI. I configured it to use SPI and uploaded the edited firmware, so I'm honestly stumped. Using a BaudRatePrescaler lower than 64 still causes the STM32F4 to receive the consistent "garbage" from the module.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    This is  a bit of  a poser - at this stage I would connect the logic analyser image

     

    Are you able to borrow one ?

     

    There might be a  hackerspace or college resource you can access nearby.

     

    Or if you are in South West Scotland ..........

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    I actually live in the US, in Florida to be more specific. I'm don't know of any place nearby that will have a logic analyzer I can borrow. Got any other ideas?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Nothing nice,

     

    The software only SPI is debuggable but takes a lot of effort and without test gear it's difficult to be sure that it's all working the way it should.

     

    You can buy a  logic analyser for as little as £7.99 from Ebay (these look like Salea knock offs - so you have to consider the ethics and risks).

     

    You can buy a real Salea for $109,

     

    Or you can look for a Hackerpsace

     

    Florida - HackerspaceWiki

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    What about this logic analyzer? It looks pretty decent and is reasonably priced. I wasn't planning on buying a logic analyzer but I guess I don't have much of a choice. Going to a hackerspace is difficult in this case, since I won't have everything I need to work with the microcontroller.

     

    Prototype: Openbench Logic Sniffer logic analyzer | Dangerous Prototypes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    It looks OK and about as cheap as you can get legally.

     

    I've no experience of SUMP but it seems to supported by at least a few active people.

     

    I probably have  a different outlook on these things from you since I do this stuff for a living but I would worry that I might waste more time with the slightly DIY Logic Sniffer than I would doing in software.

    It shouldn't take more than a few hours to write  an instrumented bit banging SPI and then you can save your $50 for later.

    Another cheap approach would be to make a simple SPI debugger based on an ST nucleo board  (they are pretty cheap).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Ok, I'll try the bit banging. What would I do next after trying that? As I said I'm rather clueless here, I haven't messed with hardware much before as I primarily do software programming, so I'm still kind of learning about this stuff. Plus this is a really strange issue.