Technical Library
  • Products & Partners
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Documents PI-VIEW HDMI to VGA Adapter Cable for Raspberry Pi Computer Board
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: atomar
  • Date Created: 2 Aug 2012 7:07 AM Date Created
  • Last Updated Last Updated: 4 Mar 2016 10:12 PM
  • Views 5608 views
  • Likes 0 likes
  • Comments 11 comments
Related
Recommended

PI-VIEW HDMI to VGA Adapter Cable for Raspberry Pi Computer Board

BUY NOWBUY NOWTechnical DocumentsVideoFeaturesKit Contents

image

Pi-View is a high quality, high performance, convenient and compact electronic device which converts the digital HDMI video signals which are outputted from Raspberry Pi, into an analogue signal required by the widely used VGA based computer displays still widely used around the world.

 

Product Features:

  • Simple device design in the form of a small adaptor with integrated VGA socket output, with short cable complete with HDMI plug for connection to the HDMI socket on Raspberry Pi.
  • No external power supply is required, and in operation, the device is plug and play*
  • The device handles display resolutions of up to 720p/1080i/1080p (the maximum resolution is limited by the resolution supported by the connected display device).
  • Input: integrated Type-A HDMI plug, Output: standard female DE-15 connector.
  • Material: 99% high-purity oxygen-free copper wire core, 30µ gold-plated terminals for minimal signal loss, and gold-plated HDMI plug for high abrasion resistance.

 

* Note: It is recommended that Raspberry Pi is powered by an external, mains power supply when Pi-View is connected and in operating.

 

Key Applications:HDMI-VGA Converter

More Development Kits and Tools
imageRaspberry Pi - Single Board ComputerimageWI-PI - WLAN USB Module for Raspberry Pi
imageGertboard Kit - Add-on GPIO board for Raspberry Piimageelement14 Design Center

 

Technical Documents


Learning Center
TypeDescription
User GuidePI-VIEW: User Guide PI-VIEW (HDMI to VGA Adapter Cable for Raspberry Pi Computer Board)
DatasheetPi-View datasheet

 

Back to top

 

Interfacing


image

 

 

 

 

Back to top

 

Features


  • Simple device design in the form of a small adaptor with integrated VGA socket output, with short cable complete with HDMI plug for connection to the HDMI socket on Raspberry Pi.
  • No external power supply is required, and in operation, the device is plug and play*
  • The device handles display resolutions of up to 720p/1080i/1080p (the maximum resolution is limited by the resolution supported by the connected display device).
  • Input: integrated Type-A HDMI plug, Output: standard female DE-15 connector.
  • Material: 99% high-purity oxygen-free copper wire core, 30µ gold-plated terminals for minimal signal loss, and gold-plated HDMI plug for high abrasion resistance.

 

* Note: It is recommended that Raspberry Pi is powered by an external, mains power supply when Pi-View is connected and in operating.

 

 

Back to top

Kit Contents


  • PI-VIEW HDMI to VGA Adapter Cable
  • Product CD with Drivers and User Manual

 

Back to top


Attachments:
imagePI-VIEW.User_Guide.pdf
  • pi-view hdmi to vga adapter cable for raspberry pi comp
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    I have just got my adapter and the picture is stunning, only it vanishes and reappears randomly( 3 seconds), actually making the screen reset each time.I had been running my pi on vnc tightserver before that  and it did not behave in this annoying way.

     

    Could it be that the electrical power the adaptor receives is not sufficient? I got my adapter from Farnell, so there should not be any trouble.

    I'll sneak around the forums and will get back if I get the problem solved.Meanwhile, I'm happy if anyone wants to help.

    PS I am running a usb b/t keyboard and mouse, and it is not doing well either.....Maybe it is drawing on the power supply....

     

    I love it when things don't work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 13 years ago

    And both of mine work just fine....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I bought one of these through Amazon. waste of Money as they do not have enough power, apparently, and doesnt give a true HDMI signal. Ended up sending mine back as it gave no signal at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I just tried a Pi-View that I ordered from Newark with a new 512MB Pi.  I was shocked to see smoke coming from my Pi!  Looks like it toasted diode D1.  Hopefully that's all that was damaged.  The Pi-View is going back to Newark.  Beware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 13 years ago

    I did some "one off" measurements. On a different device (it's black (*)).

     

    It draws 128 mA, which causes a 0.94V voltage drop over D1.  This is whithin spec for the bat54. (wether the 3.84V on the HDMI line is "within spec" for the VGA adapter, remains to be seen. But as I said before: it works).

     

    (*) But otherwise identical as to size and shape.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • atomar
    atomar over 13 years ago in reply to rew

    Hi,

     

    Here are the SKU's for Newark & Farnell. "Buy Now" link also has been updated. Thanks

     

    Newark: 07W893707W8937

    Farnell: 21338992133899

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 13 years ago

    I was "invited" here by an Element14 tweet. Then about 10 hours later again by a tweet from Farnell.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustiniadmin
    fustiniadmin over 13 years ago in reply to rew

    I believe the "Buy Now" Product Link is blank because of your locale.  The product links can handle both Newark and Farnell SKUs and display appropriate one based on locale.  The Newark SKU is 07W8937.  However, as you noted, it doesn't seem there is a SKU for Pi View in the Farnell system.  CPC (part of Premier Farnell) does have the Pi View:

     

    http://cpc.farnell.com/element14/piview/adapter-raspberry-pi-hdmi-to-vga/dp/SC12760?Ntt=piview

     

    I'll check to see if the Pi View is something that will be stocked by Farnell, too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 13 years ago in reply to e14 Contributor

    I have two of these. Not from farnell. But they look identical. Both connect a pi to a 1280x1024 screen. It works. No complaints.

     

    The 'pi has a diode in series with the 5V for the HDMI port. The specs of that diode (bat54) say: "200mA". So as far as the 'pi is concerned, it depends on your powersupply (and the fuse).

     

    But.... what I wanted to ask is: How do I buy one from Farnell? The "buy now" header is not a link. And farnell gives zero hits on "pi-view".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    If that works and draws less than the 50mA from the HDMI as per HDMI spec. I'll eat my hat!

    I've had identical units work on a Pi at low resolution (800x600) and if a POWERED HDMI repeater used then at full 1920x1080.

    The powered repeater cost more than the HDMI-VGA Adaptor!

    The power in the signal of a chequerboard output of 1920x1080 is about 30mA then add circuitry power = >50mA

    Maybe Rev.2 Pi's alow more than 50mA?

    I'm surprised at Farnell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>