Technical Library
  • Products
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Documents Texas Instruments: CC2511/CC1111 USB Evaluation Module Kit
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: atomar
  • Date Created: 12 Oct 2012 4:54 AM Date Created
  • Last Updated Last Updated: 25 Jun 2014 12:53 AM
  • Views 2675 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Texas Instruments: CC2511/CC1111 USB Evaluation Module Kit

BUY NOWBUY NOWSoftware ToolsTechnical DocumentsVideoFeaturesKit Contents

image

The Texas Instruments CC2511EMKCC2511EMK evaluation module/USB dongle is designed to help the user to achieve his/hers objectives as quickly as possible. This is the same USB dongle which is included in the CC2510-CC2511DKCC2510-CC2511DK Development Kit.

 

  • Evaluate the CC2500/CC2550/CC2510 products. The CC2511CC2511 USB dongle can be used to test the communication between the CC2500/CC2550/CC2510 prototypes/development kits, and a PC, without having to wire up the CC2500/CC2550/CC2510 development kit to the PC.
  • Right out of the box, the user can do range testing (PER testing) and transfer data from one PC to another using the SmartRFRegistered04DK. This enables the user to quickly find out how well the SmartRFRegistered04 products fit the intended application. A number of demonstration applications serve to highlight the innovative features of the SmartRFRegistered04 ICs.
  • Perform RF measurements. Using SmartRFRegistered Studio, the user can configure the radio ICs with parameters that suit the intended application and easily measure sensitivity output power and other RF parameters.
  • Develop a prototype. The SmartRFRegistered04DK includes a Silicon Labs 8051-core MCU with 16 kB of program memory and 1 kB of data memory. By programming this MCU and utilizing the various peripherals included on the Evaluation Board, the user can easily make a prototype of the intended application. All signals are brought out on 0.1" pin-row connectors so easy connection of other required circuitry is possible. These connectors are also compatible with Agilent logic analyzer probes for easy debugging.
  • It is also possible to disconnect the Silicon Labs MCU from the EM board, and connect a MCU selected by the user to the I/O connectors.

 

The Texas Instruments CC1111EMK868-915CC1111EMK868-915 USB dongle makes it easy to have a direct connection between a PC and a sub-1 GHz network based on compatible radios, like the multiProductLinkCC1101, CC1120, CC1110, and CC430. The dongle is a complete reference design demonstrating how to use the USB and RF interfaces on the CC1111 system-on-chip.The dongle operates in the 868 MHz and 915 MHz frequency bands.

  • Use the USB firmware and examples (swrc088) as a basis to develop and test USB device software for the CC1111F32RSP.CC1111F32RSP.. If you have the complete CC1110-CC1110DK, you can run several examples:
    • Wireless serial port application (CDC)
    • Wireless mouse and keyboard (HID)
    • Any other USB class can also be implemented based on the generic USB firmware library. Refer to the USB firmware user guide for more information.
  • Use the dongle as a packet capture device for the SmartRF Packet Sniffer. Configured correctly, the dongle can capture packets over-the-air and the sniffer application can parse and display the contents.

 

Ordering Information:


MPNDescription
CC2511EMKCC2511EMKCC2511F32RSP.CC2511F32RSP. USB Evaluation Module Kit
CC1111EMK868-915CC1111EMK868-915CC1111F32RSP.CC1111F32RSP. USB Evaluation Module Kit 868/915 MHz

 

Note:

  • SmartRF04EB (included in the CC1110-CC1111DKCC1110-CC1111DK) or a CC-DebuggerCC-Debugger (sold separately) is needed to program the CC1111F32RSP.CC1111F32RSP. device.
  • Also that the CC1111F32RSP.CC1111F32RSP. USB Dongle has passed USB compliance tests. The USB TID is 10005584.

 

Key Applications: PER testing, Perform RF measurements, Develop a prototype.

More Development Kits and Tools
imageTexas Instruments Analog Development KitsimageTexas Instruments Embedded Development Kits
imageDevelopment Platforms & Kitsimageelement14 Knode

 

Software Tools


 

SmartRF Studio

 

SmartRFTm Studio is a Windows application that can be used to evaluate and configure Low Power RF-ICs from Texas Instruments. The application will help designers of RF systems to easily evaluate the RF-ICs at an early stage in the design process. It is especially useful for generation of configuration register values, for practical testing of the RF system and for finding optimized external component values. SmartRF Studio can be used both as a standalone application or together with applicable evaluation boards that are shipped in the RF-IC development kits.

 

  • Link tests. Send and Receive packets between nodes.
  • Antenna and radiation tests. Set the radio in continuous TX and RX states.
  • Easy Mode for packet testing and for getting basic register values.
  • A set of recommended/typical register settings for all devices.
  • Read and write individual RF registers.
  • Detailed information about the bit fields for each register.
  • Save/Load device configuration data from file.
  • Exports register settings to a user definable format.
  • Communication with evaluation boards through USB port or the parallel port.
  • Up to 32 evaluation boards are supported on a single computer.

Back to top

 

Technical Documents


Learning Center

 

TypeDescription
User GuideTI: User Guide for CC1111/CC2511 USB HW
User GuideTI: User Guide for CC USB Software Examples
DatasheetTI: Data Sheet for CC2510Fx / CC2511Fx -Low-Power SoC (System-on-Chip) with MCU, Memory 2.4 GHz RF Transceiver, and USB Controller
Revision NoteTI: Revision Note for CC2511Fx
Application NoteTI: AN101 - Application Note for Bootloader for CC2510, CC2511, CC1110 and CC1111 SoC (System-on-Chip) Transceivers
Application NoteTI: AN080 - LED Lighting with Remote Control using CC2510 and CC1110
Application NoteTI: AN064 - Application Note for Two Way Audio Communications Using the CC2510

 

Design Elements

 

TypeDescription
Application LibraryTI: Software Code for Bootloader for CC2510, CC2511, CC1110 and CC1111 SoC (System-on-Chip) Transceivers
Application LibraryTI: Software Code for LED Lighting with Remote Control using CC2510 and CC1110
Application LibraryTI: Software Code for Two Way Audio Communications Using the CC2510
Application Library

TI: Software code for CC USB Firmware Library and Examples (Rev. C)

 

Back to top

 

Video


image

Back to top

 

Kit Features


image

 

Key Features for CC2511Fx and CC1111Fx are as below:

  • Radio
    • High-performance RF transceiver based on the market-leading CC2500
    • High-performance RF transceiver based on the market-leading CC1101 (CC1101Fx)

    • Excellent receiver selectivity and blocking performance
    • High sensitivity (−103 dBm at 2.4 kBaud)
    • High sensitivity (−110 Bm at 1.2 kBaud) (CC1101Fx)
    • Programmable data rate up to 500 kBaud
    • Programmable output power up to 1 dBm for all supported frequencies
    • Programmable output power up to 10 dBm for all supported frequencies (CC1101Fx)

    • Frequency range: 2400 - 2483.5 MHz
    • Frequency range: 300 - 348 MHz, 391 - 464 MHz and 782 - 928 MHz (CC1101Fx)
    • Digital RSSI / LQI support

 

  • Current Consumption
    • Low current consumption (RX: 17.1 mA @ 2.4 kBaud, TX: 16 mA @ −6 dBm output power)
    • 0.3 μA in PM3 (the operating mode with the lowest power consumption)
    • Low power (CC1101Fx)
      • Low current consumption (RX: 16.2 mA @1.2 kBaud, TX: 15.2 mA @ −6 dBm output power)

      • 0.3 μA in PM3 (the operating mode with the lowest power consumption)

        image

      • 0.5 μA in PM2 (operating mode with the second lowest power consumption, timer or external interrupt wakeup)

 

  • MCU, Memory, and Peripherals
    • High performance and low power 8051 microcontroller core.
    • 8/16/32 kB in-system programmable flash, and 1/2/4 kB RAM
    • Full-Speed USB Controller with 1 kB USB FIFO
    • I2S interface
    • 7 - 12 bit ADC with up to eight inputs
    • 128-bit AES security coprocessor
    • Powerful DMA functionality
    • Two USARTs
    • 16-bit timer with DSM mode
    • Three 8-bit timers
    • Hardware debug support
    • 19  GPIO pins

 

  • General
    • Wide supply voltage range (2.0V - 3.6V)
    • RoHS compliant and no antimony or bromine, 6x6mm QFN 36

 

 

 

Back to top

Kit Contents


 

The Texas Instruments CC2511EMKCC2511EMK Evaluation Kit includes:

  • One CC2511F32RSP.CC2511F32RSP. USB dongle

 

The Texas Instruments CC1111EMK868-915CC1111EMK868-915 CC1111F32RSP.CC1111F32RSP. USB Evaluation Kit includes:

  • One CC1111F32RSP.CC1111F32RSP. USB dongle with chip antenna for 868 and 915 MHz operation

 

 

Back to top


  • cc1111emk868_915
  • cc2511emk
  • cc2511
  • cc1111emk868-915
  • texas_instruments
  • cc1111
  • Share
  • History