• Products and Partners
    Products and Partners
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
Autodesk EAGLE
  • Products and Partners
  • More
Autodesk EAGLE
Blog Resources for Early EAGLE Users
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: DaveYoung
  • Date Created: 18 Jul 2013 3:46 PM Date Created
  • Views 1179 views
  • Likes 1 like
  • Comments 3 comments
  • eagle
  • dyoung
  • resources
Related
Recommended

Resources for Early EAGLE Users

DaveYoung
DaveYoung
18 Jul 2013

Any schematic capture and layout CAD package will have a learning curve, which can leave a new user searching for resources that will help get the job done. CadSoft's EAGLE schematic and layout editors are widely acclaimed as an easy way to get into PCB design, through no small effort on the part of the designers.  However there are many resources beyond the widely ignored F1 help hotkey embedded in the program (yes, those still exist).image

 

To start, many attribute EAGLE's success to their remarkable community.  The active user base makes for high visibility to new questions, and CadSoft employees regularly respond to posts, infusing the forum with valuable expert knowledge.  Searching there is the go-to when facing a problem, especially one that seems like it should have an obvious solution.

 

After creating a blank schematic page, a new user will want to start by immediately adding parts.  There are a wealth of parts that can be added from the standard libraries that are included with the stock installation, but new users should be wary of simply adding unknown parts willy-nilly.  It is tempting to add a schematic component that doesn't have the right footprint or pinout as a 'placeholder,' but putting that much faith in one's memory is probably a mistake.  Instead, a new user can begin by searching out a part that has already been created.  Element14 has a collection of part libraries that is particularly nice thanks to the searchable pdf that lists all manufacturer part numbers for the contents of the library.  Always remember that any downloaded part is not to be trusted; spending 3 minutes verifying the pin connections and key footprint dimensions is well worth it!

 

If there are no decent parts that can be easily found in existing libraries, the designer can make the part themselves.  Many people dislike creating their own parts because of the feeling that 100 other people have probably already done the work, but it is easy to fall into the trap of spending more time searching for a part than it takes to make it from scratch.  In this case a manufacturer's datasheet, or perhaps an app note, will give all of the information required to create the required part.  Once the 'suggested pad layout' documentation is found, Sparkfun has a simple step-by-step part creation tutorial that is so simple and complete that I saved a copy of it onto my hard drive. Although it may seem tedious, after creating 5 or 10 parts will quickly make searching for downloadable libraries seem ridiculous.

 

Once the board design is complete, a new user can save the step of producing Gerber files thanks to OSHpark's service which allows direct uploading of the EAGLE *.brd file.  Their simple website and pricing scheme ($5 per sqin for 3 copies of the PCB) welcomes users to what is likely the easiest and cheapest way to get professional prototype boards made.

 

For those on a tighter time constraint and looking to save money by buying a PCB that only has copper on a bare board, BareBonesPCB by Advanced Circuits is another great place to go.  They produce the boards in 24 hours, usually for ~$0.84 per sqin.  However one should bear in mind that these simple PCBs lack solder mask, silkscreen, and many other attributes which will make assembling the boards more difficult.  They also require the design be submitted with Gerber files, an extra step that that even casual PCB designers should learn at least by their second or third order.

 

As software packages are constantly changing, a user that plans to get serious about EAGLE will want to keep up with the direction of the tool.  CadSoft does a great job updating their official facebook page by talking about new features, publishing resources, all without using it as a sales platform.

 

With these resources to start with, getting into EAGLE should be faster and easier, but there are many more that can help.  If you have any favorites that you'd like to add, please suggest them in the comments!

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    This is a great write up.  If you're working with SMT/SMD and have a reflow oven, there's a new service similar to OSHPark called OSH Stencils, www.oshstencils.com that works in a similar fashion.  They make low cost high quality stencils for solder paste/reflow applications.  They charge by the square inch as well, and their quality is great.  They also accept Eagle files directly so you can drop your board at OSHPark, then your same file at OSH Stencils and spend very little money to produce a quality prototype.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DaveYoung
    DaveYoung over 13 years ago in reply to shabaz

    Great points -- You can usually tell how long someone has been designing boards by how willing they are to accept downloaded parts.  Once bitte, twice shy I suppose.  And thanks for sharing the layers document!  Love it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 13 years ago

    EAGLE is one of the best tools to be productive with, and that is mainly due to the fact that new components can be created very rapidly - some other CAD systems seem to have a very long workflow for parts creation.

    I totally agree it is better not to trust other people's components, and create your own. It might initially seem a waste of time, but it's not if you just consider it to be part of the entire design process, which it is. So, I just factor that time in, and it's not a lot of time either. It gets you very familiar with the part, because you have to study the datasheet carefully; furthermore, you learn valuable information like advice on how to route certain signals or what supply rail decoupling is required, because this is contained in the datasheet. That means the design is more likely to work first time.

    Each manufacturer has subtly different recommendations on component land patterns, and also you may wish to modify some slightly to make for example protoyping easier (such as placing a hole for thermally-enhanced SMD IC packages), so it should be considered normal that most components in a design should be created from scratch in any CAD package; about the only components that I don't create from scratch are chip resistor and capacitors, but even they may need special land patterns created if (say) the design contains RF.

    Here are some notes I created a while back that are a bit old now (I don't have the latest EAGLE package) that I still refer to occasionally, to confirm what the layers mean.